edit

Bracket for Infrared Proximity Sensor

This is an aluminum infrared proximity sensor bracket kit for Infrared Proximity Sensor. With this kit,one RB-421 Servo and one Infrared Proximity Sensor you can build a 2 degrees freedom servo mount assembly. This kit is professional in steering the infrared proxinity sensor on a robot for 180° of rotation side to side and front to back. These parts also have holes at 20mm spacings so they can be attached to Seeed (http://www.seeedstudio.com/depot/starter-bundle-harness-p-906.html?cPath=178_184)Starter Bundle Harness which has 20mm spacings as well.

Application Ideas

  • Robot eyes
  • IR self controller

Mechanic Dimensions

Usage

Hardware Installation

For holding IR sensors while you can turn it with different angles

Bill of Materials (BOM) /parts list

Devic Value Manufacturer Details(size:mm)
IR sensor bracket(10034R0) 1
angle mounting bracket(10034R0) 1
Plastic rivet 2 HKWASI D3x5.5(diameter 3 length 5.5 ,black)
Plastic rivet 10 HKWASI D2X4.8(diameter 2 length 4.8 ,black)
selflocking plastic rope 2 2x56

Tech Support

Please submit any technical issue into our forum or drop mail to techsupport@seeed.cc.