Grove - 16x2 LCD

Grove - 16 x 2 LCD is a perfect I2C LCD display for Arduino and Raspberry Pi with high contrast and easy deployment. 16x2 means two lines and each line has 16 columns, 32 characters in total. With the help of Grove I2C connector, only 2 signal pins and 2 power pins are needed. You don't even need to care about how to connect these pins. Just plug it into the I2C interface on Seeeduino or Arduino/Raspberry Pi+baseshield via the Grove cable. There won't be complicated wiring, soldering, worrying about burning the LCD caused by the wrong current limiting resistor.
Versions
| Version | Order |
|---|---|
| The Grove - 16 x 2 LCD (Black on Yellow) | Buy Now |
| The Grove - 16 x 2 LCD (Black on Red) | Buy Now |
| The Grove - 16 x 2 LCD (White on Blue) | Buy Now |
The Grove - LCD RGB Backlight has been well received since its inception. Based on customer feedback, now, we bring more cost-effective monochrome backlight derivative for you.
Except for RGB backlights, these three products are almost identical to the the Grove - LCD RGB Backlight, they are all 16 characters wide, 2 rows with high brightness backlight.
Pre-reading
An introduction of What is a Grove - 16 x 2 LCD and How does it work is strongly recommended reading ahead if you are not familiar with it. Please visit our blog for detailed information.
Features
- Display construction: 16 Characters * 2 Lines
- Display mode: STN
- On board MCU
- I2C-bus interface
- Support English and Japanese fonts
Specification
| Item | Value |
|---|---|
| Operating Voltage | 3.3V / 5V |
| Operating temperature | 0 to 50℃ |
| Storage temperature | -10 to 60℃ |
| Driving method | 1/16 duty, 1/5 bias |
| Interface | I^2^C |
| I^2^C Address | 0X3E |
Typical Applications
- Temperature display
- Time display
- Any project that requires a simple display
Platforms Supported
| Arduino | Raspberry | ArduPy |
|---|---|---|
|
|
|
The platforms mentioned above as supported is/are an indication of the module's software or theoritical compatibility. We only provide software library or code examples for Arduino platform in most cases. It is not possible to provide software library / demo code for all possible MCU platforms. Hence, users have to write their own software library.
Getting Started
Play With Arduino
Materials required
| Seeeduino V4.2 | Base Shield | Grove - 16 x 2 LCD |
|---|---|---|
|
|
|
| Get One Now | Get One Now | Get One Now |
-
Please plug the USB cable gently, otherwise you may damage the port. Please use the USB cable with 4 wires inside, the 2 wires cable can't transfer data. If you are not sure about the wire you have, you can click here to buy.
-
Each Grove module comes with a Grove cable when you buy. In case you lose the Grove cable, you can click here to buy.
Hardware Overview
I2C Pull-Up Resistor
The first version of Grove - 16 x 2 LCD series does not have a built-in pull-up resistor, nor does it provide a pad to solder the optional pull-up resistor. We have redesigned the module, and the new version has built-in pull-up resistors.
If you have an older version on your hand, you can solder a 10kΩ DIP resistor yourself on the back pad of the Grove connector. Please follow the picture below, solder a 10kΩ DIP resistor between VCC and SCL pins and a 10kΩ DIP resistor between VCC and SDA pins.

Outline

Hardware Connection

| Seeeduino | Grove Cable | Grove - 16 x 2 LCD |
|---|---|---|
| GND | Black | GND |
| 5V or 3.3V | Red | VCC |
| SDA | White | SDA |
| SCL | Yellow | SCL |
-
Step 1. Connect the Grove - 16 x 2 LCD to port I^2^C of Grove-Base Shield.
-
Step 2. Plug Grove - Base Shield into Seeeduino and connect Seeeduino to PC via a USB cable.
Software
If this is the first time you work with Arduino, we strongly recommend you to see Getting Started with Arduino before the start.
- Step 1. Download the Grove-LCD RGB Backlight Library from Github.
The Grove - 16 x 2 LCD shares the same library with the Grove-LCD RGB Backlight. Their usage is almost the same, except that the Grove - 16 x 2 LCD does not support the RGB color API, such as setRGB().
-
Step 2. Refer to How to install library to install library for Arduino.
-
Step 3. Restart the Arduino IDE. Open the example, you can open it in the following three ways:
1). Open it directly in the Arduino IDE via the path: File --> Examples --> Grove - LCD RGB Backlight --> HelloWorld.

2). Open it in your computer by click the HelloWorld.ino which you can find in the folder XXXX\Arduino\libraries\Grove_LCD_RGB_Backlight-master\examples\HelloWorld, XXXX is the location you installed the Arduino IDE.

3). Or, you can just click the icon

in upper right corner of the code block to copy the following code into a new sketch in the Arduino IDE.
#include <Wire.h>
#include "rgb_lcd.h"
rgb_lcd lcd;
/*
const int colorR = 255;
const int colorG = 0;
const int colorB = 0;
*/
void setup()
{
// set up the LCD's number of columns and rows:
lcd.begin(16, 2);
//lcd.setRGB(colorR, colorG, colorB);
// Print a message to the LCD.
lcd.print("hello, world!");
delay(1000);
}
void loop()
{
// set the cursor to column 0, line 1
// (note: line 1 is the second row, since counting begins with 0):
lcd.setCursor(0, 1);
// print the number of seconds since reset:
lcd.print(millis()/1000);
delay(100);
}
-
The library file may be updated. This code may not be applicable to the updated library file, so we recommend that you use the first two methods.
-
Since the Grove - 16 x 2 LCD series are all monochrome backlight, you need to comment out the RGB color related code. In the demo code above, i.e., line 6 and line 17.
- Step 4. Upload the demo. If you do not know how to upload the code, please check How to upload code.
If every thing goes well, you will see the LCD shows the classic sentence: hello world.

If there's no Base Shield with you, Seeeduino VX Series with I2C interface do work as well.
Play With Raspberry Pi (With Grove Base Hat for Raspberry Pi)
Hardware
- Step 1. Things used in this project:
| Raspberry pi | Grove Base Hat for RasPi | Grove - 16x2 LCD |
|---|---|---|
![]() | ![]() | |
- Step 2. Plug the Grove Base Hat into Raspberry.
- Step 3. Connect the Grove - 16 x 2 LCD to I2C port of the Base Hat.
- Step 4. Connect the Raspberry Pi to PC through USB cable.
Software
- Step 1. Follow Setting Software to configure the development environment install the grove.py to your raspberry pi.
- Step 2. Excute below commands to run the code.
# virutalenv for Python3
virtualenv -p python3 env
source env/bin/activate
#enter commmand
grove_16x2_lcd
Following is the jhd1802.py code.
from grove.display.base import *
from grove.i2c import Bus
import time
import sys
# sphinx autoapi required
__all__ = ["JHD1802"]
class JHD1802(Display):
'''
Grove - 16 x 2 LCD, using chip JHD1802.
- Grove - 16 x 2 LCD (Black on Yellow)
- Grove - 16 x 2 LCD (Black on Red)
- Grove - 16 x 2 LCD (White on Blue)
Also, it's our class name,
which could drive the above three LCDs.
Args:
address(int): I2C device address, default to 0x3E.
'''
def __init__(self, address = 0x3E):
self._bus = Bus()
self._addr = address
if self._bus.write_byte(self._addr, 0):
print("Check if the LCD {} inserted, then try again"
.format(self.name))
sys.exit(1)
self.textCommand(0x02)
time.sleep(0.1)
self.textCommand(0x08 | 0x04) # display on, no cursor
self.textCommand(0x28)
@property
def name(self):
'''
Get device name
Returns:
string: JHD1802
'''
return "JHD1802"
def type(self):
'''
Get device type
Returns:
int: ``TYPE_CHAR``
'''
return TYPE_CHAR
def size(self):
'''
Get display size
Returns:
(Rows, Columns): the display size, in characters.
'''
# Charactor 16x2
# return (Rows, Columns)
return 2, 16
def clear(self):
'''
Clears the screen and positions the cursor in the upper-left corner.
'''
self.textCommand(0x01)
def draw(self, data, bytes):
'''
Not implement for char type display device.
'''
return False
def home(self):
'''
Positions the cursor in the upper-left of the LCD.
That is, use that location in outputting subsequent text to the display.
'''
self.textCommand(0x02)
time.sleep(0.2)
def setCursor(self, row, column):
'''
Position the LCD cursor; that is, set the location
at which subsequent text written to the LCD will be displayed.
Args:
row (int): the row at which to position cursor, with 0 being the first row
column(int): the column at which to position cursor, with 0 being the first column
Returns:
None
'''
# print("setCursor: row={}, column={}".format(row,column))
self.textCommand((0x40 * row) + (column % 0x10) + 0x80)
def write(self, msg):
'''
Write character(s) to the LCD.
Args:
msg (string): the character(s) to write to the display
Returns:
None
'''
for c in msg:
self._bus.write_byte_data(self._addr,0x40,ord(c))
def _cursor_on(self, enable):
if enable:
self.textCommand(0x0E)
else:
self.textCommand(0x0C)
def textCommand(self, cmd):
self._bus.write_byte_data(self._addr,0x80,cmd)
def main():
import time
lcd = JHD1802()
rows, cols = lcd.size()
print("LCD model: {}".format(lcd.name))
print("LCD type : {} x {}".format(cols, rows))
lcd.backlight(False)
time.sleep(1)
lcd.backlight(True)
lcd.setCursor(0, 0)
lcd.write("hello world!")
lcd.setCursor(0, cols - 1)
lcd.write('X')
lcd.setCursor(rows - 1, 0)
for i in range(cols):
lcd.write(chr(ord('A') + i))
time.sleep(3)
lcd.clear()
if __name__ == '__main__':
main()
(env)pi@raspberrypi:~ grove_16x2_lcd
If everything goes well, you will be able to see the following result
- The backlight will turn off for 1 second, then turn back on.
- LCD will display:
hello world! X
ABCDEFGHIJKLMNOP
- After 3 seconds, the entire display will be cleared, and the screen will be blank.
You can quit this program by simply press ctrl+c.
Play With Wio Terminal (ArduPy)
Hardware
- Step 1. Prepare the below stuffs:
| Wio Terminal | Grove - 16 x 2 LCD |
|---|---|
|
|
| Get One Now | Get One Now |
-
Step 2. Connect Grove - 16 x 2 LCD to I2C port of Wio Terminal.
-
Step 3. Connect the Wio Terminal to PC through USB Type-C cable.

Software
-
Step 1. Follow ArduPy Getting Started to configure the ArduPy development environment on Wio Terminal.
-
Step 2. Make sure that the ArduPy firmware contains the Grove - 16 x 2 LCD ArduPy library using the following commands. For more information, please follow here.
aip install Seeed-Studio/seeed-ardupy-lcd1602
aip build
aip flash
- Step 3. Copy the following code and save it as
ArduPy-LCD1602.py:
from arduino import grove_lcd1602
import time
lcd = grove_lcd1602()
def main():
lcd.print("hello, world!")
lcd.is_blink_cursor = True
i = 0
while True:
lcd.set_cursor(1, 2) #column 1, row 2
lcd.print(i)
time.sleep(1)
i = i + 1
if __name__ == "__main__":
main()
For more API reference, please refer to here.
- Step 4. Save the
ArduPy-LCD1602.pyin a location that you know. Run the following command and replace<YourPythonFilePath>with yourArduPy-LCD1602.pylocation.
aip shell -n -c "runfile <YourPythonFilePath>"
# Example:
# aip shell -n -c "runfile /Users/ansonhe/Desktop/ArduPy-LCD1602.py"
- Step 5. We will see the results on the Grove - 16 x 2 LCD.

Resources
- [PDF] JDH_1804_Datasheet
Project
This is the introduction Video of this product, simple demos, you can have a try.
Grove IR Universal Remote Project:Have multiple remotes? Have an Arduino? Operate multiple devices with a single press of a Keyes IR remote.
Range tests made easy with the RE-Mote and LCD:Reduce the number of equipment and preparations required for field testing (2.4GHz and 868MHz), pack everything you need in your hand.
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.