Skip to main content

Grove - 3-Axis Digital Accelerometer(±1.5g)

Grove - 3-Axis Digital Accelerometer v1.2

Grove - 3-Axis Digital Accelerometer v1.2b

3-Axis Digital Accelerometer is the key part in projects like orientation detection, gesture detection and Motion detection. This 3-Axis Digital Accelerometer(±1.5g) is based on Freescale's low power consumption module, MMA7660FC. It features up to 10,000g high shock survivability and configurable Samples per Second rate. For generous applications that don't require too large measurement range, this is a great choice because it's durable, energy saving and cost-efficient.

pir

Specifications

  • Working voltage: 3.0 - 5.5V
  • Off Mode Current: 0.4μA
  • Standby Mode Current: 2μA
  • Active Mode Current: 47 μA at 1 ODR
  • Test Range: ±1.5g
  • Sensitivity: 21LSB/g
  • Suli-compatible Library
tip

More details about Grove modules please refer to Grove System

Platforms Supported

ArduinoRaspberry Pi

pir

pir

caution

The platforms mentioned above as supported is/are an indication of the module's software or theoritical compatibility. We only provide software library or code examples for Arduino platform in most cases. It is not possible to provide software library / demo code for all possible MCU platforms. Hence, users have to write their own software library.

Demonstration

With Arduino

Here we are going to show you how to get raw data and data measured by "g" from this sensor.

Connect this module to the I2C port of Grove - Base Shield via a Grove cable.

Note

If you want to activate the Interrupt function of this module, you need to connect the INT soldering pad we broke out on the board with a pin of Arduino that's capable of Interrupt Service Routine.

pir

Install the library we provide in the resources section.

Open the code directly by the path:File -> Example ->DigitalAccelerometer_MMA7660FC ->MMA7660FC_Demo.

In this program, acceleration information are sent from the sensor to Seeeduino via I2C bus and then Seeeduino printed them onto the serial monitor. Open the serial monitor to check the result.

pir

The outputs of this sensor consist of two parts: raw data and 3-axis acceleration info converted into the unit of gravity, "g".

With Raspberry Pi

1.You should have got a raspberry pi and a grovepi or grovepi+.

2.You should have completed configuring the development enviroment, otherwise follow here.

3.Connection

  • Plug the sensor to grovepi socket i2c-x(1~3) by using a grove cable.

4.Navigate to the demos' directory:

cd yourpath/GrovePi/Software/Python/

  • To see the code
    nano grove_i2c_accelerometer.py   # "Ctrl+x" to exit #
    import time
import grovepi

# Connect the Grove Accelerometer (+/- 1.5g) to any I2C port eg. I2C-1
# Can be found at I2C address 0x4c
# SCL,SDA,VCC,GND

while True:
try:
print grovepi.acc_xyz()
time.sleep(.5)

except IOError:
print "Error"

5.Run the demo.

    sudo python grove_i2c_accelerometer.py

Reference

Below are two figures helping you understand the physical meaning of the result.

The first figure is about the direction of each axis:

pir

The second figure gives some examples:

pir

Schematic Online Viewer

Resources

Project

Tilt Activated Spinning Fan Light Stick Portable LED color stick reacts to your shaking motion. With extra fan and alarm.

Lean Green RC Sailing Machine An Internet connected device that controls servos and sends sensor (GPS/gyro/accel/compass) updates in real time over a GSM cell link.

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...