edit

Grove - 5-Way Switch

The Grove - 5-Way Switch can be used to detect the switch position and event like single click/double click/long press, etc. It can detect left/right/up/down/center 5 directions. The 5-way switch will be a great option for multifunction control.

With only one small switch to meet all your needs for switch control!

Version

Product Version Changes Released Date
Grove - 5-Way Switch Initial Jun 2018

Features

  • 5 way individual switch
  • Good heat resistance
  • Long operating Life
  • Grove compatible

Specification

Item Value
Operating voltage 3.3V / 5V
Interface I2C
Default I2C Address 0x03
Size L: 40mm W: 20mm H: 10mm
Weight 4.1g
Package size L: 140mm W: 90mm H: 10mm
Gross Weight 10g

Applications

  • Game control
  • Multifunction control

Hardware Overview

Pin Map

Platforms Supported

Arduino Raspberry Pi BeagleBone Wio LinkIt ONE

Caution

The platforms mentioned above as supported is/are an indication of the module's software or theoritical compatibility. We only provide software library or code examples for Arduino platform in most cases. It is not possible to provide software library / demo code for all possible MCU platforms. Hence, users have to write their own software library.

Getting Started

Play With Arduino

Hardware

Materials required

Seeeduino V4.2 Base Shield Grove - 5-Way Switch
enter image description here enter image description here enter image description here
Get One Now Get One Now Get One Now

Note

1 Please plug the USB cable gently, otherwise you may damage the port. Please use the USB cable with 4 wires inside, the 2 wires cable can't transfer data. If you are not sure about the wire you have, you can click here to buy

2 Each Grove module comes with a Grove cable when you buy. In case you lose the Grove cable, you can click here to buy.

  • Step 1. Connect the Grove - 5-Way Switch to the I2C port of the Base Shield.

  • Step 2. Plug Grove - Base Shield into Seeeduino.

  • Step 3. Connect Seeeduino to PC via a USB cable.

Note

If we don't have Grove Base Shield, We also can directly connect this module to Seeeduino as below.

Seeeduino Grove - 5-Way Switch
5V Red
GND Black
SDA White
SCL Yellow

Software

Attention

If this is the first time you work with Arduino, we strongly recommend you to see Getting Started with Arduino before the start.

  • Step 1. Download the Grove Multi Switch Library from Github.

  • Step 2. Refer to How to install library to install library for Arduino.

  • Step 3. Restart the Arduino IDE. Open example via the path: File → Examples → Grove Multi Switch Library → Grove_Switch_Events.

Or, you can just click the icon in upper right corner of the code block to copy the following code into a new sketch in the Arduino IDE.

  1
  2
  3
  4
  5
  6
  7
  8
  9
 10
 11
 12
 13
 14
 15
 16
 17
 18
 19
 20
 21
 22
 23
 24
 25
 26
 27
 28
 29
 30
 31
 32
 33
 34
 35
 36
 37
 38
 39
 40
 41
 42
 43
 44
 45
 46
 47
 48
 49
 50
 51
 52
 53
 54
 55
 56
 57
 58
 59
 60
 61
 62
 63
 64
 65
 66
 67
 68
 69
 70
 71
 72
 73
 74
 75
 76
 77
 78
 79
 80
 81
 82
 83
 84
 85
 86
 87
 88
 89
 90
 91
 92
 93
 94
 95
 96
 97
 98
 99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
#include "Grove_Multi_Switch.h"

GroveMultiSwitch mswitch[1];
const char* grove_5way_tactile_keys[] = {
    "KEY A",
    "KEY B",
    "KEY C",
    "KEY D",
    "KEY E",
};
const char* grove_6pos_dip_switch_keys[] = {
    "POS 1",
    "POS 2",
    "POS 3",
    "POS 4",
    "POS 5",
    "POS 6",
};

const char** key_names;

int deviceDetect(void) {
    if (!mswitch->begin()) {
        Serial.println("***** Device probe failed *****");
        return -1;
    }

    Serial.println("***** Device probe OK *****");
    if (PID_VAL(mswitch->getDevID()) == PID_5_WAY_TACTILE_SWITCH) {
        Serial.println("Grove 5-Way Tactile Switch Inserted!");
        key_names = grove_5way_tactile_keys;
    } else if (PID_VAL(mswitch->getDevID()) == PID_6_POS_DIP_SWITCH) {
        Serial.println("Grove 6-Position DIP Switch Inserted!");
        key_names = grove_6pos_dip_switch_keys;
    }

    // enable event detection
    mswitch->setEventMode(true);

    // report device model
    Serial.print("A ");
    Serial.print(mswitch->getSwitchCount());
    Serial.print(" Button/Switch Device ");
    Serial.println(mswitch->getDevVer());
    return 0;
}

void setup()
{
    Serial.begin(115200);
    Serial.println("Grove Multi Switch");

    // Initial device probe
    if (deviceDetect() < 0) {
        Serial.println("Insert Grove 5-Way Tactile");
        Serial.println("or Grove 6-Position DIP Switch");
        for (;;);
    }

    return;
}

void loop()
{
    GroveMultiSwitch::ButtonEvent_t* evt;

    delay(1);

    evt = mswitch->getEvent();
    if (!evt) {
        // dynamic device probe
        deviceDetect();
        delay(1000);
        return;
    }

    if (!(evt->event & GroveMultiSwitch::BTN_EV_HAS_EVENT)) {
        #if 0
        Serial.print("No event, errno = ");
        Serial.println(mswitch->errno);
        #endif
        return;
    }

    for (int i = 0; i < mswitch->getSwitchCount(); i++) {
        Serial.print(key_names[i]);
        Serial.print(": RAW - ");
        Serial.print((evt->button[i] & GroveMultiSwitch::BTN_EV_RAW_STATUS)?
                     "HIGH ": "LOW ");
        if (PID_VAL(mswitch->getDevID()) == PID_5_WAY_TACTILE_SWITCH) {
            Serial.print((evt->button[i] & GroveMultiSwitch::BTN_EV_RAW_STATUS)?
                         "RELEASED ": "PRESSED ");
        } else if (PID_VAL(mswitch->getDevID()) == PID_6_POS_DIP_SWITCH) {
            Serial.print((evt->button[i] & GroveMultiSwitch::BTN_EV_RAW_STATUS)?
                         "OFF ": "ON ");
        }
        Serial.println("");
    }

    for (int i = 0; i < mswitch->getSwitchCount(); i++) {
        if (evt->button[i] & ~GroveMultiSwitch::BTN_EV_RAW_STATUS) {
            Serial.println("");
            Serial.print(key_names[i]);
            Serial.print(": EVENT - ");
        }
        if (evt->button[i] & GroveMultiSwitch::BTN_EV_SINGLE_CLICK) {
            Serial.print("SINGLE-CLICK ");
        }
        if (evt->button[i] & GroveMultiSwitch::BTN_EV_DOUBLE_CLICK) {
            Serial.print("DOUBLE-CLICK ");
        }
        if (evt->button[i] & GroveMultiSwitch::BTN_EV_LONG_PRESS) {
            Serial.print("LONG-PRESS ");
        }
        if (evt->button[i] & GroveMultiSwitch::BTN_EV_LEVEL_CHANGED) {
            Serial.print("LEVEL-CHANGED ");
        }
    }
    Serial.println("");
}
  • Step 4. Upload the demo. If you do not know how to upload the code, please check How to upload code.

  • Step 5. Open the Serial Monitor of Arduino IDE by click Tool-> Serial Monitor. Or tap the Ctrl+Shift+M key at the same time. Set the baud rate to 115200.

Success

If every thing goes well, you will get the result. When you press the KEY E, it will trigger KEY E: RAW - LOW PRESSED

 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
Grove Multi Switch
***** Device probe  Device BN-5E-0.1
Grove Multi Switch
***** Device probe OK *****
Grove 5-Way Tactile Switch Inserted!
A 5 Button/Switch Device BN-5E-0.1
KEY A: RAW - HIGH RELEASED 
KEY B: RAW - HIGH RELEASED 
KEY C: RAW - HIGH RELEASED 
KEY D: RAW - HIGH RELEASED 
KEY E: RAW - LOW PRESSED 

KEY E: EVENT - LEVEL-CHANGED 
KEY A: RAW - HIGH RELEASED 
KEY B: RAW - HIGH RELEASED 
KEY C: RAW - HIGH RELEASED 
KEY D: RAW - HIGH RELEASED 
KEY E: RAW - HIGH RELEASED 

KEY E: EVENT - SINGLE-CLICK LEVEL-CHANGED 
KEY A: RAW - LOW PRESSED 
KEY B: RAW - HIGH RELEASED 
KEY C: RAW - HIGH RELEASED 
KEY D: RAW - HIGH RELEASED 
KEY E: RAW - HIGH RELEASED 

KEY A: EVENT - LEVEL-CHANGED 
KEY A: RAW - HIGH RELEASED 
KEY B: RAW - HIGH RELEASED 
KEY C: RAW - HIGH RELEASED 
KEY D: RAW - HIGH RELEASED 
KEY E: RAW - HIGH RELEASED 

Resources

Project

This is the introduction Video of this product, simple demos, you can have a try.

Tech Support

Please do not hesitate to submit the issue into our forum.