Grove - Barometer (High-Accuracy)

This Grove - Barometer (High-Accuracy) Sensor features a HP206F high-accuracy chip to detect barometric pressure, Altimeter, and temperature. It can widely measure pressure ranging from 300mbar~1200mbar, with a resolution of 0.02mbar during the measurement. The chip only accepts 1.8V to 3.6V input voltage. However, with outer circuit added, this module becomes compatible with 3.3V and 5V. Therefore, it can be used on Arduino/Seeeduino or Seeeduino Stalker without modification. It is designed to be connected directly to a micro-controller via the I2C bus.
Features
- Digital two wire (I2C) interface
- Command-based Reading, Compensated (Optional)
- Programmable Events and Interrupt Controls
- Full Data Compensation
- Wide barometric pressure range
- Flexible supply voltage range
- Ultra-low power consumption
- Altitude Resolution down to 0.01 meter
- Temperature measurement included
- I2C Address: 0x76
If you want to use multiplue I2C devices, please refer to Software I2C.
More details about Grove modules please refer to Grove System
Application Ideas
- High Precision Mobile Altimeter / Barometer
- Industrial Pressure and Temperature Sensor System
- Automotive Systems
- Personal Electronics Altimetry
- Adventure and Sports watches
- Medical Gas Control System
- Weather Station Equipment
- Indoor Navigation and Map Assist
- Heating, Ventilation, Air Conditioning
Specifications
| Parameter | Description |
|---|---|
| Supply Voltage | 1.8v~3.6v |
| Operation Temperature Range | -40℃~85℃ |
| Pressure Measurement Range | 300mbar~1200mbar |
| Pressure Resolution | 0.02mbar |
| Altitude Resolution | 0.2m |
| Dimension | 20.4 × 41.8 × 9.7 mm |
Platforms Supported
| Arduino | Raspberry Pi |
|---|---|
|
|
The platforms mentioned above as supported is/are an indication of the module's software or theoritical compatibility. We only provide software library or code examples for Arduino platform in most cases. It is not possible to provide software library / demo code for all possible MCU platforms. Hence, users have to write their own software library.
Hardware Overview

Getting started
Play with Arduino
Barometric condition is one of the criteria used to predict coming change in weather and altitude above sea level. Here is a demo to show you how to read the barometric data from this Grove - Barometer Sensor.
Hardware
- Step 1. Prepare the below stuffs:
| Seeeduino V4.2 | Base Shield | Grove-Barometer-High-Accuracy |
|---|---|---|
![]() | ![]() | ![]() |
- Step 2. Connect Grove-Barometer-High-Accuracy to port I2C of Grove-Base Shield.
- Step 3. Plug Grove - Base Shield into Seeeduino.
- Step 4. Connect Seeeduino to PC via a USB cable.

If we don't have Grove Base Shield, We also can directly connect this module to Seeeduino as below.
| seeeduino_v4 | Grove-Barometer-High-Accuracy |
|---|---|
| 5V | VCC |
| GND | GND |
| SDA | SDA |
| SCL | SCL |
Software
Step 1. Download the library from Github.
Step 2. Refer How to install library to install library for Arduino.
Step 3. Create a new Arduino sketch and paste the codes below to it or open the code directly by the path:File -> Example -> Grove barometer HP20x -> HP20x_demo.
Here is the code
/*
* Demo name : HP20x_dev demo
* Usage : I2C PRECISION BAROMETER AND ALTIMETER [HP206F hopeRF]
* Author : Oliver Wang from Seeed Studio
* Version : V0.2
* Change log : Add kalman filter 2014/04/04
Update the chip to HP206F 2025/04/07
*/
#include <HP20x_dev.h>
#include <KalmanFilter.h>
#include "Arduino.h"
#include "Wire.h"
unsigned char ret = 0;
/* Instance */
KalmanFilter t_filter; //temperature filter
KalmanFilter p_filter; //pressure filter
KalmanFilter a_filter; //altitude filter
void setup()
{
Serial.begin(9600); // start serial for output
Serial.println("****HP20x_dev demo by seeed studio****\n");
Serial.println("Calculation formula: H = [8.5(101325-P)]/100 \n");
/* Power up,delay 150ms,until voltage is stable*/
delay(150);
/* Reset HP20x_dev*/
HP20x.begin();
delay(100);
/* Determine HP20x_dev is available or not*/
ret = HP20x.isAvailable();
if(OK_HP20X_DEV == ret)
{
Serial.println("HP20x_dev is available.\n");
}
else
{
Serial.println("HP20x_dev isn't available.\n");
}
}
void loop()
{
char display[40];
if(OK_HP20X_DEV == ret)
{
Serial.println("------------------\n");
long Temper = HP20x.ReadTemperature();
Serial.println("Temper:");
float t = Temper/100.0;
Serial.print(t);
Serial.println("C.\n");
Serial.println("Filter:");
Serial.print(t_filter.Filter(t));
Serial.println("C.\n");
long Pressure = HP20x.ReadPressure();
Serial.println("Pressure:");
t = Pressure/100.0;
Serial.print(t);
Serial.println("hPa.\n");
Serial.println("Filter:");
Serial.print(p_filter.Filter(t));
Serial.println("hPa\n");
long Altitude = HP20x.ReadAltitude();
Serial.println("Altitude:");
t = Altitude/100.0;
Serial.print(t);
Serial.println("m.\n");
Serial.println("Filter:");
Serial.print(a_filter.Filter(t));
Serial.println("m.\n");
Serial.println("------------------\n");
delay(1000);
}
}
Step 4. Open the serial monitor to receive the sensor's data including temperature, barometric pressure value, relative atmosphere pressure and altitude.
Play With Raspberry Pi
Hardware
- Step 1. Prepare the below stuffs:
| SRaspberry pi | Grove Base Hat for Raspberry Pi | Grove-Barometer-High-Accuracy |
|---|---|---|
![]() | ![]() | ![]() |
- Step 2. Plug the Grove Base Hat for Raspberry Pi into Raspberry.
- Step 3. Connect Grove-Barometer-High-Accuracy to I2C port of Grove Base Hat for Raspberry Pi.
- Step 4. Connect the Raspberry to PC through USB cable.

Software
-
Step 1. Follow Setting Software to configure the development environment and install dependencies.
-
Step 2. Git clone the Github repository.
cd ~
git clone https://github.com/Seeed-Studio/grove.py
cd grove.py
sudo pip3 install .
- Step 3. Excute below commands to use this sensor
sudo apt install python3-virtualenv
virtualenv -p python3 env
source env/bin/activate
cd ./grove.py/grove
python3 grove_i2c_hp206f_driver.py
Here is the code :
#!/usr/bin/env python
#
# Library for interacting with Grove - HP20x sensor (used to measure temperature, pressure and altitude)
#
# This is the library for Grove Base Hat which used to connect grove sensors for raspberry pi.
#
'''
## License
The MIT License (MIT)
Grove Base Hat for the Raspberry Pi, used to connect grove sensors.
Copyright (C) [Your Company Name or Relevant Party]
Permission is hereby granted, free of charge, to any person obtaining a copy
of this software and associated documentation files (the "Software"), to deal
in the Software without restriction, including without limitation the rights
to use, copy, modify, merge, publish, distribute, sublicense, and/or sell
copies of the Software, and to permit persons to whom the Software is
furnished to do so, subject to the following conditions:
The above copyright notice and this permission notice shall be included in
all copies or substantial portions of the Software.
THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE
AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER
LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM,
OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN
THE SOFTWARE.
'''
import time
from grove.i2c import Bus
# Class for interacting with the HP20x sensor
class HP20x:
def __init__(self):
# Initialize the I2C bus on Raspberry Pi (bus 1)
self.bus = Bus()
# I2C address of the HP206F sensor, may need adjustment based on actual situation
self.address = 0x76
# I2C device ID when CSB PIN is at VDD level (address is 0x76)
self.HP20X_I2C_DEV_ID = (0xEC) >> 1
# I2C device ID when CSB PIN is at GND level (address is 0x77)
self.HP20X_I2C_DEV_ID2 = (0XEE) >> 1
# Soft reset command for the HP20x sensor
self.HP20X_SOFT_RST = 0x06
# Write conversion command for the HP20x sensor
self.HP20X_WR_CONVERT_CMD = 0x40
# Different oversampling rate (OSR) configurations for conversion
self.HP20X_CONVERT_OSR4096 = 0 << 2
self.HP20X_CONVERT_OSR2048 = 1 << 2
self.HP20X_CONVERT_OSR1024 = 2 << 2
self.HP20X_CONVERT_OSR512 = 3 << 2
self.HP20X_CONVERT_OSR256 = 4 << 2
self.HP20X_CONVERT_OSR128 = 5 << 2
# Commands for reading pressure, altitude, temperature, etc.
self.HP20X_READ_P = 0x30 # Read pressure command
self.HP20X_READ_A = 0x31 # Read altitude command
self.HP20X_READ_T = 0x32 # Read temperature command
self.HP20X_READ_PT = 0x10 # Read pressure and temperature command
self.HP20X_READ_AT = 0x11 # Read altitude and temperature command
self.HP20X_READ_CAL = 0X28 # RE-CAL ANALOG command
# Write register mode for the HP20x sensor
self.HP20X_WR_REG_MODE = 0xC0
# Read register mode for the HP20x sensor
self.HP20X_RD_REG_MODE = 0x80
# Set the oversampling rate configuration
self.OSR_CFG = self.HP20X_CONVERT_OSR1024
# Conversion time corresponding to the oversampling rate (in milliseconds)
self.OSR_ConvertTime = 25
def begin(self):
# Send a soft reset command to the HP20x sensor
self.HP20X_IIC_WriteCmd(self.HP20X_SOFT_RST)
# Wait for 0.1 seconds to ensure the reset operation is completed
time.sleep(0.1)
def isAvailable(self):
# Check if the HP20x sensor is available by reading the register at address 0x0F
return self.HP20X_IIC_ReadReg(0x0F)
def ReadTemperature(self):
# Send a conversion command with the specified oversampling rate configuration
self.HP20X_IIC_WriteCmd(self.HP20X_WR_CONVERT_CMD | self.OSR_CFG)
# Wait for the conversion time (converted to seconds)
time.sleep(self.OSR_ConvertTime / 1000.0)
# Read 3 bytes of raw temperature data from the sensor
t_raw = self.bus.read_i2c_block_data(self.address, self.HP20X_READ_T, 3)
# Combine the 3 bytes of data to form a single value
t = t_raw[0] << 16 | t_raw[1] << 8 | t_raw[2]
# Handle negative values using 2's complement
if t & 0x800000:
t |= 0xff000000
us = (1 << 32)
t = -1 * (us - t)
# Return the temperature value in degrees Celsius (divided by 100)
return t / 100.0
def ReadPressure(self):
# Send a conversion command with the specified oversampling rate configuration
self.HP20X_IIC_WriteCmd(self.HP20X_WR_CONVERT_CMD | self.OSR_CFG)
# Wait for the conversion time (converted to seconds)
time.sleep(self.OSR_ConvertTime / 1000.0)
# Read 3 bytes of raw pressure data from the sensor
p_raw = self.bus.read_i2c_block_data(self.address, self.HP20X_READ_P, 3)
# Combine the 3 bytes of data to form a single value
p = p_raw[0] << 16 | p_raw[1] << 8 | p_raw[2]
# Handle negative values using 2's complement
if p & 0x800000:
p |= 0xff000000
# Return the pressure value in hectopascals (divided by 100)
return p / 100.0
def ReadAltitude(self):
# Send a conversion command with the specified oversampling rate configuration
self.HP20X_IIC_WriteCmd(self.HP20X_WR_CONVERT_CMD | self.OSR_CFG)
# Wait for the conversion time (converted to seconds)
time.sleep(self.OSR_ConvertTime / 1000.0)
# Read 3 bytes of raw altitude data from the sensor
a_raw = self.bus.read_i2c_block_data(self.address, self.HP20X_READ_A, 3)
# Combine the 3 bytes of data to form a single value
a = a_raw[0] << 16 | a_raw[1] << 8 | a_raw[2]
# Handle negative values using 2's complement
if a & 0x800000:
a |= 0xff000000
us = (1 << 32)
a = -1 * (us - a)
# Return the altitude value in meters (divided by 100)
return a / 100.0
def HP20X_IIC_WriteCmd(self, uCmd):
# Write a command byte to the specified I2C address
self.bus.write_byte(self.address, uCmd)
def HP20X_IIC_ReadReg(self, bReg):
# Read a byte from the specified register address
return self.bus.read_byte_data(self.address, bReg | self.HP20X_RD_REG_MODE)
# Class representing the Kalman filter
class KalmanFilter:
def __init__(self):
# Process noise covariance
self.q = 0.01
# Measurement noise covariance
self.r = 0.1
# Initial estimated value
self.x = 0
# Initial estimated error covariance
self.p = 1
# Initial Kalman gain
self.k = 0
def Filter(self, measurement):
# Prediction step: Update the estimated error covariance
self.p = self.p + self.q
# Update step: Calculate the Kalman gain
self.k = self.p / (self.p + self.r)
# Update step: Update the estimated value based on the measurement
self.x = self.x + self.k * (measurement - self.x)
# Update step: Update the estimated error covariance
self.p = (1 - self.k) * self.p
# Return the filtered estimated value
return self.x
# Kalman filter for temperature data
t_filter = KalmanFilter()
# Kalman filter for pressure data
p_filter = KalmanFilter()
# Kalman filter for altitude data
a_filter = KalmanFilter()
# Create an instance of the HP20x sensor
hp20x = HP20x()
# Function to simulate the setup process
def setup():
print("****HP20x_dev demo by seeed studio****\n")
print("Calculation formula: H = [8.5(101325-P)]/100 \n")
# Wait for 0.15 seconds after power-on to stabilize the voltage
time.sleep(0.15)
# Initialize the HP20x sensor
hp20x.begin()
# Wait for 0.1 seconds
time.sleep(0.1)
# Check if the HP20x sensor is available
ret = hp20x.isAvailable()
if ret:
print("HP20x_dev is available.\n")
else:
print("HP20x_dev isn't available.\n")
return ret
# Function to simulate the loop process
def loop(ret):
if ret:
while True:
print("------------------\n")
# Read the temperature value from the HP20x sensor
temper = hp20x.ReadTemperature()
print("Temper:")
print(f"{temper}C.\n")
print("Filter:")
# Apply the Kalman filter to the temperature value
print(f"{t_filter.Filter(temper)}C.\n")
# Read the pressure value from the HP20x sensor
pressure = hp20x.ReadPressure()
print("Pressure:")
print(f"{pressure}hPa.\n")
print("Filter:")
# Apply the Kalman filter to the pressure value
print(f"{p_filter.Filter(pressure)}hPa\n")
# Read the altitude value from the HP20x sensor
altitude = hp20x.ReadAltitude()
print("Altitude:")
print(f"{altitude}m.\n")
print("Filter:")
# Apply the Kalman filter to the altitude value
print(f"{a_filter.Filter(altitude)}m.\n")
print("------------------\n")
# Wait for 1 second before the next reading
time.sleep(1)
if __name__ == "__main__":
# Perform the setup process
ret = setup()
# Start the loop process if the sensor is available
loop(ret)
Schematic Online Viewer
Resources
- [Eagle] [Grove_Barometer_High-Accuracy_v1.0_sch_pcb Eagle File](https://files.seeedstudio.com/wiki/Grove-Barometer-High-Accuracy/res/Grove_Barometer_High_Accuracy_ v1.0_sch_pcb.zip)
- [Datasheet] HP206F Datasheet
- [Library] Github repository for Grove_Barometer_HP20x with arduino
Projects
Smart Crops: Implementing IoT in Conventional Agriculture! Our mission with nature is to preserve it, designing and implementing technologies and monitoring methods with the help of IoT via Helium.
Tech Support & Product Discussion
Upgradable to Industrial Sensors
With the SenseCAP S2110 controller and S2100 data logger, you can easily turn the Grove into a LoRaWAN® sensor. Seeed not only helps you with prototyping but also offers you the possibility to expand your project with the SenseCAP series of robust industrial sensors.
The IP66 housing, Bluetooth configuration, compatibility with the global LoRaWAN® network, built-in 19 Ah battery, and powerful support from APP make the SenseCAP S210x the best choice for industrial applications. The series includes sensors for soil moisture, air temperature and humidity, light intensity, CO2, EC, and an 8-in-1 weather station. Try the latest SenseCAP S210x for your next successful industrial project.