edit

Grove - I2C FM Receiver

Grove - I2C FM Receiver is a wideband FM receiver module, this module is based on RDA5807M. The RDA5807M series are the latest generation single-chip broadcast FM stereo radio tuner with fully integrated synthesizer. The RDA5807M series have a powerful low-IF digital audio processor. The Grove - I2C FM Receiver has a headset jack, so it can connect to earphones or audio.

Version

Version Change Release date
Grove - I2C FM Receiver v1.0 Initial May 18, 2017
Grove - I2C FM Receiver v1.1 Change some components to make the board more stable April 17, 2018

Features

  • Grove interface
  • Supports worldwide frequency band: 50 - 115MHz
  • Support RDS/RBDS
  • Lower power consumption
  • Headset interface
  • Digital auto gain control
  • Input voltage: 3.3V - 5V

Tip

More details about Grove modules please refer to Grove System

Platforms Supported

Arduino Raspberry Pi BeagleBone Wio LinkIt ONE

Caution

The platforms mentioned above as supported is/are an indication of the module's software or theoritical compatibility. We only provide software library or code examples for Arduino platform in most cases. It is not possible to provide software library / demo code for all possible MCU platforms. Hence, users have to write their own software library.

Getting Started

Note

If this is the first time you work with Arduino, we strongly recommend you to see Getting Started with Arduino before the start.

Play With Arduino

Hardware

Materials required

Seeeduino V4.2 Base Shield Grove - I2C FM Receiver v1.1 Grove - Button x 2 Grove - Rotary Angle Sensor
enter image description here enter image description here enter image description here enter image description here enter image description here
Get One Now Get One Now Get One Now Get ONE Now Get ONE Now

Note

1 Please plug the USB cable gently, otherwise you may damage the port. Please use the USB cable with 4 wires inside, the 2 wires cable can't transfer data. If you are not sure about the wire you have, you can click here to buy

2 Each Grove module comes with a Grove cable when you buy. In case you lose the Grove cable, you can click here to buy

  • Step 1. Connect Grove - I2C FM Receiver to port IIC of Grove-Base Shield.

  • Step 2. Connect Grove - Button 1 to D2 port and connect Grove - Button 2 to D3 port.

  • Step 3. Plug Grove - Base Shield into Seeeduino.

  • Step 4. Connect Seeeduino to PC via a USB cable.

Note

If we don't have Grove Base Shield, We also can directly connect Grove - Temperature and Humidity Sensor Pro to Seeeduino as below.

Seeeduino Grove - I2C FM Receiver v1.1
5V Red
GND Black
SDA White
SCL Yellow
Seeeduino Grove - Button 1
5V Red
GND Black
Null White
D2 Yellow
Seeeduino Grove - Button 2
5V Red
GND Black
Null White
D3 Yellow
Seeeduino Grove - Rotary Angle Sensor
5V Red
GND Black
Null White
A0 Yellow

Software

  1
  2
  3
  4
  5
  6
  7
  8
  9
 10
 11
 12
 13
 14
 15
 16
 17
 18
 19
 20
 21
 22
 23
 24
 25
 26
 27
 28
 29
 30
 31
 32
 33
 34
 35
 36
 37
 38
 39
 40
 41
 42
 43
 44
 45
 46
 47
 48
 49
 50
 51
 52
 53
 54
 55
 56
 57
 58
 59
 60
 61
 62
 63
 64
 65
 66
 67
 68
 69
 70
 71
 72
 73
 74
 75
 76
 77
 78
 79
 80
 81
 82
 83
 84
 85
 86
 87
 88
 89
 90
 91
 92
 93
 94
 95
 96
 97
 98
 99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
588
589
590
591
592
593
594
595
596
597
598
599
600
601
602
603
604
605
/*
 * I2C_FM.ino
 * Demo code for the Grove-I2C_FM_Receiver module
 *
 * Copyright (c) 2012 seeed technology inc.
 * Author     : Jack Shao (jacky.shaoxg@gmail.com)
 * Create Time: Jul 2014
 * Change Log :
 *
 * The MIT License (MIT)
 *
 * Permission is hereby granted, free of charge, to any person obtaining a copy
 * of this software and associated documentation files (the "Software"), to deal
 * in the Software without restriction, including without limitation the rights
 * to use, copy, modify, merge, publish, distribute, sublicense, and/or sell
 * copies of the Software, and to permit persons to whom the Software is
 * furnished to do so, subject to the following conditions:
 *
 * The above copyright notice and this permission notice shall be included in
 * all copies or substantial portions of the Software.
 *
 * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
 * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
 * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE
 * AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER
 * LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM,
 * OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN
 * THE SOFTWARE.
 */
//
/*
 * Modifications to the I2C_FM.ino by Mel Patrick - Wabbit Wanch Design
 * Modified routines for scanning UP or DOWN through the FM band
 * Modified routine to test for signal strength of received station
 * Modified routines to support bass boost and MONO signal
 * RSSI, read it too soon after setting a station and you get a small value
 * so it's better to wait a bit (50ms) and try it. minSignalStrength will
 * skip locking on a station with a weak signal (you could set the MONO bit) to get
 * better reception on these stations.
 */
#include <Arduino.h>
#include <Wire.h>
#include <EEPROM.h>

#define BTNUP          2// used for seeking UP (normally CLOSED push button)
#define VOL_POT        A0// volume POT LOG taper 10K
#define BTNDN          3// used for seeking DOWN (normally CLOSED push button)

uint16_t gChipID = 0;
uint8_t RDA5807P_REGW[10];

#define I2C_ADDR       0x10

#define READ            1
#define WRITE           0

#define ADRW            0x20
#define ADRR            0x21
//

//#define                 _SHARE_CRYSTAL_24MHz_
//#define                 _SHARE_CRYSTAL_12MHz_
#define                 _SHARE_CRYSTAL_32KHz_
//#define                 _FM_STEP_50K_

//5807M,5807FP,5807NN,5807NP
uint8_t RDA5807N_initialization_reg[]={
#if defined(_SHARE_CRYSTAL_24MHz_)
  0xC4, 0x51, //02H:
#elif defined(_SHARE_CRYSTAL_12MHz_)
  0xC4, 0x11, //02H:
#elif defined(_SHARE_CRYSTAL_32KHz_)
  0xC4, 0x01,//change 01 to 05 enables the RDS/RBDS
#else
  0xC0, 0x01,
#endif
  0x00, 0x00,
  0x04, 0x00,
  0xC3, 0xad,  //05h
  0x60, 0x00,
  0x42, 0x12,
  0x00, 0x00,
  0x00, 0x00,
  0x00, 0x00,  //0x0ah
  0x00, 0x00,
  0x00, 0x00,
  0x00, 0x00,
  0x00, 0x00,
  0x00, 0x00,
  0x00, 0x00,  //0x10h
  0x00, 0x19,
  0x2a, 0x11,
  0xB0, 0x42,
  0x2A, 0x11,  //
  0xb8, 0x31,  //0x15h
  0xc0, 0x00,
  0x2a, 0x91,
  0x94, 0x00,
  0x00, 0xa8,
  0xc4, 0x00,  //0x1ah
  0xF7, 0xcF,
  0x12, 0x14,  //0x1ch
  0x80, 0x6F,
  0x46, 0x08,
  0x00, 0x86,  //10000110
  0x06, 0x61,  //0x20H
  0x00, 0x00,
  0x10, 0x9E,
  0x23, 0xC8,
  0x04, 0x06,
  0x0E, 0x1C,  //0x25H     //0x04 0x08
};

int16_t freq = 10110;
uint16_t vol = 1;
//
// added items - Mel
boolean bassBit = true;// bass boost
boolean monoBit = false;// force MONO not stereo
const boolean seekUP = true;
const boolean seekDN = false;
uint8_t minSignalStrength = 36;// anything below this probably set a MONO flag for better reception
uint8_t signalStrength;
long previousMillis = 0;// last time the function was called
long interval = 2000;// interval for the signal level function (2 seconds)
int8_t stationStep = 10;// kHz steps bewteen the stations (North America = 10)
boolean hasVolumePot = true;// flag if you have a POT attached or not
//
void setup()
{
  Wire.begin();
  loadDefaults();// load any defaults from previous radio settings
  Serial.begin(9600);
  Serial.println("Started");
  //=======================
  //rda5807 power on
  RDA5807P_PowerOnReset();
  RDA5807P_SetMute(false);

  //=======================
  pinMode(BTNUP, INPUT_PULLUP);
  pinMode(VOL_POT, INPUT);
  pinMode(BTNDN, INPUT_PULLUP);
  //=======================
  RDA5807P_SetVolumeLevel(vol);// use this if you don't have a POT for volume attached (0-15)
  RDA5807P_SetFreq( freq );
}

void loop()
{
  unsigned long currentMillis = millis();

  if(currentMillis - previousMillis > interval) {
    // save the last time you blinked the LED
    previousMillis = currentMillis;
    showSignalStrength();
  }
  //
  if (digitalRead(BTNUP) == 1)
  {
    delay(100);
    if (digitalRead(BTNUP) == 1)
      fmSeek(seekUP);
    while(digitalRead(BTNUP) == 1);
  }
  if (digitalRead(BTNDN) == 1)
  {
    delay(100);
    if (digitalRead(BTNDN) == 1)
      fmSeek(seekDN);
    while(digitalRead(BTNDN) == 1);
  }
  if (hasVolumePot == true) setVolume();// use this to read the POT
}
//
void setVolume() {
  unsigned int temp_vol;
  temp_vol = analogRead( VOL_POT );
  if (abs(temp_vol - vol)>5)
  {
    if (vol != temp_vol) {// don't bother changing the volume if unless the pot moves
      vol = temp_vol;
      unsigned char hex_vol = map(vol, 0, 1023, 0, 0xf);
      RDA5807P_SetVolumeLevel(hex_vol);
      saveDefaults();// save new volume to EEPROM
    }
  }
}
//
void fmSeek(boolean theDir) {
  int signalStrength;
  if (!theDir) {
    Serial.println("Start seeking down...");
  }
  else
  {
    Serial.println("Start seeking up...");
  }
  do {
    do{
      if (theDir == seekUP) {
        freq += stationStep;
      }
      else
      {
        freq -= stationStep;
      }
      if (freq > 10800) freq = 8800;
      if (freq < 8800) freq = 10800;
      //Serial.println(freq);
    }
    while(!RDA5807P_ValidStop(freq));
    delay(50);
    signalStrength = RDA5807P_GetSigLvl(freq);// max is 63 according to Data sheet, but I've seen more
  }
  while (signalStrength < minSignalStrength);// minimum signal strength, keep looking
  showRadioStation();
  saveDefaults();// save new station selection to EEPROM
}
//
void showRadioStation() {
  Serial.print("Stable Freq:");
  Serial.print(((float)freq)/100.0f);
  Serial.println("MHz");
}
//
void showSignalStrength() {
  signalStrength = RDA5807P_GetSigLvl(freq);// max is 63...as noted
  Serial.print("Signal Strength: ");
  Serial.println(signalStrength);
}

//===========================================================
// FM functions
//===========================================================
unsigned char OperationRDAFM_2w(unsigned char operation, unsigned char *data, int numBytes)
{
  if(operation == READ)
  {
    Wire.requestFrom(I2C_ADDR, numBytes);
    for(int i=0;i<numBytes;i++)
    {
      *data++ = Wire.read();
    }
  }
  else
  {
    Wire.beginTransmission(I2C_ADDR);
    for(int i=0;i<numBytes;i++)
    {
      Wire.write(*data++);
    }
    Wire.endTransmission();
  }
  return 0;
}


/**
 * @brief Reset RDA5807P while power on RDA5807P
 * @author RDA RDA Ri'an Zeng
 * @date 2008-11-05
 * @param void
 * @return void
 * @retval
 */
void  RDA5807P_PowerOnReset(void)
{
  RDA5807P_Intialization();
}

/**
 * @brief RDA5807P power off function
 * @author RDA Ri'an Zeng
 * @date 2008-11-05
 * @param void
 * @return void
 * @retval
 */
void  RDA5807P_PowerOffProc(void)
{
  RDA5807P_REGW[1] &= (~1);
  OperationRDAFM_2w(WRITE, &(RDA5807P_REGW[0]), 2);
}

/**
 * @brief Set RDA5807P into mute mode
 * @author RDA Ri'an Zeng
 * @date 2008-11-05
 * @param bool mute: if mute is true,then set mute; if mute is false,then set no mute
 * @return void
 * @retval
 */
void RDA5807P_SetMute(boolean mute)
{
  if(mute)
    RDA5807P_REGW[0] &=  ~(1<<6);
  else
    RDA5807P_REGW[0] |= 1<<6;
  RDA5807P_REGW[0] |= monoBit<<5;
  RDA5807P_REGW[0] |= bassBit<<4;
  OperationRDAFM_2w(WRITE, &(RDA5807P_REGW[0]), 2);//RDA5807M_REGW
  delay(50);    //Dealy 50 ms
}
//
/*************************************************
 * @brief Set frequency function
 * @author RDA Ri'an Zeng
 * @date 2008-11-05
 * @param int16_t curFreq:frequency value
 * @return void
 * @retval
 ***********************************************/
void RDA5807P_SetFreq(int16_t curFreq)
{
  uint16_t curChan;
  curChan=RDA5807P_FreqToChan(curFreq);

  if((curFreq >= 6500)&&(curFreq < 7600))
  {
    RDA5807P_REGW[3] = 0x0c;
  }
  else if((curFreq >= 7600)&&(curFreq < 10800))
  {
    RDA5807P_REGW[3] = 0x08;// sets the BAND bits (00xx = 87-108, 01xx=76-91, 10xx=76-108, 11xx=65-76
    // for north america this must be set to 10xx for some unknown reason
  }
  //SetNoMute
  RDA5807P_REGW[0] |= 1<<6;
  RDA5807P_REGW[0] |= monoBit<<5;
  RDA5807P_REGW[0] |= bassBit<<4;
  //handleBits();
  RDA5807P_REGW[2]=curChan>>2;
  RDA5807P_REGW[3]=(((curChan&0x0003)<<6)|0x10) | (RDA5807P_REGW[3]&0x0f);    //set tune bit

  OperationRDAFM_2w(WRITE, &(RDA5807P_REGW[0]), 4);
  delay(50);     //Delay five ms
  showRadioStation();
}
//
/**
 * @brief Station judge for auto search
 * @In auto search mode,uses this function to judge the frequency if has a station
 * @author RDA Ri'an Zeng
 * @date 2008-11-05
 * @param int16_t freq:frequency value
 * @return bool: if return true,the frequency has a true station;otherwise doesn't have a station
 * @retval
 */
boolean RDA5807P_ValidStop(int freq)
{
  uint8_t RDA5807P_reg_data[4]={
    0                                                  };
  uint8_t falseStation = 0;
  uint8_t i=0;
  uint16_t curChan;

  if((freq >= 6500)&&(freq < 7600))
  {
    RDA5807P_REGW[3] = 0x0c;
  }
  else if((freq >= 7600)&&(freq < 10800))
  {
    RDA5807P_REGW[3] = 0x08;// sets the BAND bits (00xx = 87-108, 01xx=76-91, 10xx=76-108, 11xx=65-76
    // for north america this must be set to 10xx for some unknown reason
  }
  curChan=RDA5807P_FreqToChan(freq);
  //SetNoMute bit 9 is seek direction (0=seek down, 1=seek up).
  //02H 14
  RDA5807P_REGW[0] |=   1<<6;// reg zero is bits 15 to bit 8 (this shifts to bit 14)
  RDA5807P_REGW[0] |= monoBit<<5;
  RDA5807P_REGW[0] |= bassBit<<4;
  //handleBits();
  RDA5807P_reg_data[0]=RDA5807P_REGW[0];
  RDA5807P_reg_data[1]=RDA5807P_REGW[1];
  RDA5807P_reg_data[2]=curChan>>2;//03H 15:8 CHAN
  RDA5807P_reg_data[3]=(((curChan&0x0003)<<6)|0x10) | (RDA5807P_REGW[3]&0x0f);//
  OperationRDAFM_2w(WRITE,&(RDA5807P_reg_data[0]), 4);

  delay(50);    //Dealy 25 ms

  if (0x5808 == gChipID)
    OperationRDAFM_2w(READ,&(RDA5807P_reg_data[0]), 4); //
  else
  {
    do
    {
      i++;
      if(i>5) return 0;

      delay(30);
      //read REG0A&0B
      OperationRDAFM_2w(READ,&(RDA5807P_reg_data[0]), 4);
    }
    while((RDA5807P_reg_data[0]&0x40)==0);
  }

  //check FM_TRUE
  if((RDA5807P_reg_data[2] &0x01)==0) falseStation=1;//0B 8  FM TRUE

  if(freq==9600) falseStation=1;// North America - if scanning DOWN, the radio will lock on 9600 for some reason!
  delay(50);
  if (falseStation==1)
    return 0;
  else
    return 1;
}

/**
 * @brief Get the signal level(RSSI) of the current frequency
 * @author RDA Ri'an Zeng
 * @date 2008-11-05
 * @param int16_t curf:frequency value
 * @return uint8_t: the signal level(RSSI)
 * @retval
 */
uint8_t RDA5807P_GetSigLvl( int16_t curf )
{
  uint8_t RDA5807P_reg_data[4]={
    0                                                  };
  OperationRDAFM_2w(READ,&(RDA5807P_reg_data[0]), 4);
  delay(50);    //Delay 50 ms
  return  (RDA5807P_reg_data[2]>>1);  /*??rssi*/
}

/**
 * @brief Set FM volume
 * @It has better use the system volume operation to replace this function
 * @author RDA Ri'an Zeng
 * @date 2008-11-05
 * @param uint8_t level: volume value
 * @return void
 * @retval
 */
void RDA5807P_SetVolumeLevel(uint8_t level)
{
  uint8_t RDA5807P_reg_data[8];
  uint8_t i = 0;

  for (i=0;i<8;i++)
    RDA5807P_reg_data[i] = RDA5807P_REGW[i];

  RDA5807P_reg_data[7]=(( RDA5807P_REGW[7] & 0xf0 ) | (level & 0x0f));

  RDA5807P_reg_data[3] &= (~(0x10));//disable tune

  OperationRDAFM_2w(WRITE, &(RDA5807P_reg_data[0]), 8);
  delay(50);    //Dealy 50 ms
}

/**
 * @brief Initialize RDA5807P
 * @author RDA Ri'an Zeng
 * @date 2008-11-05
 * @param void
 * @return bool:if true,the operation is successful;otherwise is failed
 * @retval
 **/
boolean  RDA5807P_Intialization(void)
{
  uint8_t error_ind = 0;
  uint8_t RDA5807P_REGR[10]={
    0x0                                                  };
  uint8_t i = 0;

  RDA5807P_REGW[0] = 0x00;
  RDA5807P_REGW[0] |= monoBit<<5;
  RDA5807P_REGW[0] |= bassBit<<4;
  RDA5807P_REGW[1] = 0x02;

  error_ind = OperationRDAFM_2w(WRITE, (uint8_t *)&RDA5807P_REGW[0], 2);//soft reset
  delay(50);

  error_ind = OperationRDAFM_2w(READ, (uint8_t *)&RDA5807P_REGR[0], 10);
  delay(50);

  gChipID = RDA5807P_REGR[8];
  gChipID = ((gChipID << 8) | RDA5807P_REGR[9]);

  Serial.print("Chip ID: 0x");
  Serial.println(gChipID, HEX);

  for (i=0;i<8;i++) {
    RDA5807P_REGW[i] = RDA5807N_initialization_reg[i];
  }

  error_ind = OperationRDAFM_2w(WRITE, (uint8_t *)&RDA5807N_initialization_reg[0], 2); //power up
  delay(600);
  //Serial.println(sizeof(RDA5807N_initialization_reg));
  error_ind = OperationRDAFM_2w(WRITE, (uint8_t *)&RDA5807N_initialization_reg[0], sizeof(RDA5807N_initialization_reg));

  delay(50);         //Dealy 50 ms

  if (error_ind )
    return 0;
  else
    return 1;
}
//
/**
 * @brief Cover the frequency to channel value
 * @author RDA Ri'an Zeng
 * @date 2008-11-05
 * @param uint16 frequency:covered frequency
 * @return uint16: channel value
 * @retval
 * In the United States, frequency-modulated broadcasting stations operate in a frequency band extending from 87.8 MHz to 108.0 MHz,
 * for a total of 20.2 MHz. It is divided into 101 channels, each 0.2 MHz wide, designated "channel 200" through "channel 300."
 * In actual practice, no one (except the FCC) uses these channel numbers; the frequencies are used instead.
 */
uint16_t RDA5807P_FreqToChan(uint16_t frequency) {
  uint8_t channelSpacing = 10;
  uint16_t channel = 0;

  if((frequency >= 6500)&&(frequency < 7600))
  {
    channel = (frequency - 6500)/channelSpacing;
  }
  else if((frequency >= 7600)&&(frequency < 10800))
  {
    channel = (frequency - 7600)/channelSpacing;
  }
  return (channel);
}
//
void loadDefaults() {
  char myCode[9] = "Grove_FM";
  char myInit[9] = "blank123";
  /*
  * byte map in EEPROM
   * 8, 9 the default frequency for a reboot
   * 10, 11 current preset volume of the radio (used if no pot is attached)
   */
  for (int i=0; i < 8; i++) {
    myInit[i] = EEPROM.read(i);// read out to see if the thing is INITIALIZED
  }
  if (strcmp(myCode, myInit) == 0) {// if this is ZERO (we previously wrote some), then read the values
    freq = epReadINT(8);// read back the INT for frequency from eeprom 8 and 9 (two bytes for an INT)
    if (!hasVolumePot) vol = epReadINT(10);// read back the volume setting but don't use it unless flag is false
  }
  else// we don't have any defaults, so we have to save some first
  {
    for (int i=0; i < 8; i++) {
      EEPROM.write(i, myCode[i]);// write this to EEPROM to show we have it saved
    }
    saveDefaults();// write the current default settings
  }
}
//
void saveDefaults() {
  epWriteINT(8, freq);// write the two bytes for INT for a reboot
  epWriteINT(10, vol);// write the current volume POT setting
}
//
void epWriteINT(int where, int theVal) {
  union uData
  {
    byte stuff[2];
    int f1;// 2 bytes of memory
  }
  u;
  u.f1 = theVal;// copy into the union
  for (int j=0; j < 2; j++) {// now we have to write out 2 bytes of memory
    EEPROM.write(where + j, u.stuff[j]);// write it to EEPROM
  }
}
//
long epReadINT(int where) {
  union uData
  {
    byte stuff[2];
    int f1;// 2 bytes of memory
  }
  u;
  for (int j=0; j < 2; j++) {
    u.stuff[j]=EEPROM.read(where + j);// read back the 2 bytes at this memory location
  }
  return u.f1;
}
//
void epWriteLong(int where, long theVal) {
  union uData
  {
    byte stuff[4];
    long f1;// 4 bytes of memory
  }
  u;
  u.f1 = theVal;// copy into the union
  for (int j=0; j < 4; j++) {// now we have to write out 4 bytes of memory
    EEPROM.write(where + j, u.stuff[j]);// write it to EEPROM
  }
}
//
long epReadLong(int where) {
  union uData
  {
    byte stuff[4];
    long f1;// 4 bytes of memory
  }
  u;
  for (int j=0; j < 4; j++) {
    u.stuff[j]=EEPROM.read(where + j);// read back the 4 bytes to this memory location
  }
  return u.f1;
}
  • Step 4. Upload the demo. If you do not know how to upload the code, please check How to upload code.

  • Step 5. Open the Serial Monitor of Arduino IDE by click Tool-> Serial Monitor. Or tap the Ctrl+Shift+M key at the same time. if every thing goes well, you will get the result.

The result should be like:

 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
Started
Chip ID: 0x5808
Stable Freq:102.60MHz
Signal Strength: 46
Signal Strength: 46
Signal Strength: 45
Signal Strength: 45
Signal Strength: 45
Signal Strength: 45
Start seeking down...
Stable Freq:94.00MHz
Signal Strength: 44
Signal Strength: 51
Signal Strength: 51
Signal Strength: 50
Signal Strength: 50
Signal Strength: 51

Now you can hear the FM station, and you can press the Grove- button 1 and Grove- button 2 to change the radio stations. And you can rotate the Grove - Rotary Angle Sensor to adjust the volume.

Have fun~

Resources

Tech Support

Please do not hesitate to contact techsupport@seeed.cc if you have any technical issue. Or submit the issue into our forum.