Grove - LED Socket Kit
Grove - LED is designed for the beginners of Arduino/Seeeduino to monitor controls from digital ports. It can be mounted to the surface of your box or desk easily and used as pilot lamp for power or signal. Its brightness can be adjust by potentiometer.
Features
-
Grove compatible interface
-
3.3V/5V Compatible
-
Adjustable LED orientation
-
Adjustable LED brightness
Specification
Item | Description |
LED Control Mode | Digital Pin of Arduino |
Working Voltage | 5V |
Supply Mode | Grove Interface |
Get Started with Aduino
Here we show how to use Arduino to control the state of the LED.
1.Connect the LED to Base Shield's digital port 2 with 4pin Grove Cable.Of course you can change to other valid digital ports if it's necessary and the definitions of the port should be changed too.
2.Plug it onto the Arduino/Seeeduino. Connect the board to PC using USB cable.
3.Copy the demo code to your sketch, then upload to Arduino or Seeeduino board. Please click here if you do not know how to upload.
You will see the LED blink every second.
/*************************************************************************
* File Name : GroveLEDDemoCode.ino
* Author : Seeedteam
* Version : V1.1
* Date : 18/2/2012
* Description : Demo code for Grove - LED
*************************************************************************/
#define LED 2 //connect LED to digital pin2
void setup() {
// initialize the digital pin2 as an output.
pinMode(LED, OUTPUT);
}
void loop() {
digitalWrite(LED, HIGH); // set the LED on
delay(500); // for 500ms
digitalWrite(LED, LOW); // set the LED off
delay(500);
}
Get Started with Raspberry Pi
Connect the LED to Port D4 and power on the Raspberry Pi, using the Grove wire connector. This is a test to make led blinking. You can connect to GrovePi+ with it as the picture below.
# GrovePi LED Blink example
import time
from grovepi import *
# Connect the Grove LED to digital port D4
led = 4
pinMode(led,"OUTPUT")
time.sleep(1)
while True:
try:
#Blink the LED
digitalWrite(led,1) # Send HIGH to switch on LED
time.sleep(1)
digitalWrite(led,0) # Send LOW to switch off LED
time.sleep(1)
except KeyboardInterrupt: # Turn LED off before stopping
digitalWrite(led,0)
break
except IOError: # Print "Error" if communication error encountered
print "Error"
Run The Program
- Find the path to the file(According to your own path)
cd GrovePi/Software/Python/
- Run Program
sudo python grove_led_blink.py
Grove - LED
Grove - LED v1.3
Resources
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.