M11 1.25 Water flow Sensor
Water flow sensor consists of a plastic valve body, a water rotor, and a hall-effect sensor. When water flows through the rotor, rotor rolls. Its speed changes with different rate of flow. The hall-effect sensor outputs the corresponding pulse Signal.
Specification
Mini. Wokring Voltage | DC 4.5V |
Max. Working Current | 15mA(DC 5V) |
Working Voltage | 5V~24V |
Flow Rate Range | 0.3~6L/min |
Load Capacity | ≤10mA(DC 5V) |
Operating Temperature | ≤80℃ |
Liquid Temperature | ≤120℃ |
Operating Humidity | 35%~90%RH |
Water Pressure | ≤0.8MPa |
Storage Temperature | -25℃~+80℃ |
Storage Humidity | 25%~95%RH |
Mechanic Dimensions
Thread size :M11*1.25
Sensor Components
No. | Name | Quantity | Material | Note |
---|---|---|---|---|
1 | Valve body | 1 | PA66+33%glass fiber | |
2 | Stainless steel bead | 1 | Stainless steel SUS304 | |
3 | Axis | 1 | Stainless steel SUS304 | |
4 | Impeller | 1 | POM | |
5 | Ring magnet | 1 | Ferrite | |
6 | Middle ring | 1 | PA66+33%glass fiber | |
7 | O-seal ring | 1 | Rubber | |
8 | Electronic seal ring | 1 | Rubber | |
9 | Cover | 1 | PA66+33%glass fiber | |
10 | Screw | 4 | Stainless steel SUS304 | |
11 | Cable | 1 | 1007 24AWG |
Usage Example
Note: This example is abstracted from the forum, which was done by Charles Gantt. Thanks for his contribution.Let's see how it works.
Reading Water Flow rate with Water Flow Sensor
This is part of a project I have been working on and I thought I would share it here since there have been a few threads on how to read water flow rate in liters per hour using the Water Flow Sensor found in the Seeed Studio Depo. It uses a simple rotating wheel that pulses a hall effect sensor. By reading these pulses and implementing a little math, we can read the liquids flow rate accurate to within 3%. The threads are simple G3/4 so finding barbed ends will not be that hard.
Hardware Installation
You will need Seeeduino / Arduino ,Water Flow Sensor,10K resistor,a breadboard and some jumper wires.
Wiring up the Water Flow Sensor is pretty simple. There are 3 wires: Black, Red, and Yellow. Black to the Seeeduino's ground pin Red to Seeeduino's 5v pin The yellow wire will need to be connected to a 10k pull up resistor.and then to pin 2 on the Seeeduino.
Here is a fritzing diagram I made to show you how to wire it all up.
Once you have it wired up you will need to upload the following code to your Seeeduino. Once it is uploaded and you have some fluid flowing through the Water Flow Sensor, you can open the serial monitor and it will display the flow rate, refreshing every second.
Programming
// reading liquid flow rate using Seeeduino and Water Flow Sensor from Seeedstudio.com
// Code adapted by Charles Gantt from PC Fan RPM code written by Crenn @thebestcasescenario.com
// http:/themakersworkbench.com http://thebestcasescenario.com https://www.seeedstudio.com
volatile int NbTopsFan; //measuring the rising edges of the signal
int Calc;
int hallsensor = 2; //The pin location of the sensor
void rpm () //This is the function that the interupt calls
{
NbTopsFan++; //This function measures the rising and falling edge of the
hall effect sensors signal
}
// The setup() method runs once, when the sketch starts
void setup() //
{
pinMode(hallsensor, INPUT); //initializes digital pin 2 as an input
Serial.begin(9600); //This is the setup function where the serial port is
initialised,
attachInterrupt(0, rpm, RISING); //and the interrupt is attached
}
// the loop() method runs over and over again,
// as long as the Arduino has power
void loop ()
{
NbTopsFan = 0; //Set NbTops to 0 ready for calculations
sei(); //Enables interrupts
delay (1000); //Wait 1 second
cli(); //Disable interrupts
Calc = (NbTopsFan * 60 / 73); //(Pulse frequency x 60) / 73Q, = flow rate
in L/hour
Serial.print (Calc, DEC); //Prints the number calculated above
Serial.print (" L/hour\r\n"); //Prints "L/hour" and returns a new line
}
You can refer our forum for more details about Reading Water Flow rate with Water Flow Sensor.
Wiring Diagram
The external diameter of thread the connections use is 1.4mm.
Output Table
Output pulse high level | Signal voltage >4.5 V( input DC 5 V) |
Output pulse low level | Signal voltage <0.5V( input DC 5V) |
Precision | 3% (Flow rate from 1L/min to 10L/min) |
Output signal duty cycle | 40%~60% |
FAQ
What materials is water flow sensor made of?
Nylon with fiber, avoiding strong acid and strong base.
Is the water flow sensor safe for drinking water?
Yeah, it has been used on drinking machine.
What thread type does this sensor have? British or NPT?
It has BSP thread. We have two kinds of water sensors. The black is standard(Thread major diameter) and the white one is smaller(Thread minor diameter). You can refer to BSP details.
Resource
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.