Skip to main content

Mini GSM/GPRS GPS Breakout SIM808

Overview

This board based on the latest SIMCOM SIM808 GSM/GPS module, it offers cellular GSM and GPRS data along with GPS technology for satellite navigation.

The board features ultra-low power consumption in sleep mode, giving the project incredibly long standby times. Furthermore there's an onboard battery charging circuit that can be used with LiPo batteries.

The GPS receiver is incredibly sensitive with 22 tracking and 66 acquisition channels, and also supports assisted-GPS (A-GPS) for indoor localisation. The board is controlled by AT command via UART and supports 3.3V and 5V logical level. It comes with a mini GPS and GSM antenna, however a battery is optional.

The board uses the 2G (not 3G or LTE) GSM networks.

Features

  • Quad-band 850/900/1800/1900MHz

  • GPRS multi-slot class12 connectivity: max. 85.6kbps(down-load/up-load)

  • GPRS mobile station class B

  • Controlled by AT Command (3GPP TS 27.007, 27.005 and SIMCOM enhanced AT Commands)

  • Supports charging control for Li-Ion battery

  • Supports Real Time Clock

  • Supply voltage range 3.4V ~ 4.4V

  • Integrated GPS/CNSS and supports A-GPS

  • Supports 3.0V to 5.0V logic level

  • Low power consumption, 1mA in sleep mode

  • Supports GPS NMEA protocol

  • Compact size 27mm x 46mm x 10mm

  • Standard SIM Card

GPS Specifications

  • Receiver channels: 22 tracking / 66 acquisition

  • Coarse/Acquisition code: GPS L1

  • Tracking sensitivity: -165dBm

  • Cold start time: 30s (typ.)

  • Hot start time: 1s (typ.)

  • Warm start time: 28s (typ.)

  • Horizontal position accuracy: < 2.5m CEP

  • Power consumption - Acquisition: 42mA

  • Power consumption - Continuous tracking: 24mA

  • Update rate: 5Hz

Functional Block

  • GPS Antenna: this is an uFL GPS antenna connector. You can connect either passive or active GPS antenna to it. Active GPS antenna runs at 2.8V voltage.

  • MicroUSB: the charging interface for Li-Ion battery, of input voltage range from 5V to 7V.

  • Power Button: this is the hard power switch for the module. When the module is power up, you can turn on or turn off the module by pressing the button for 2s.

  • Net Indicator: Red LED, it will tell the what status is about the module linking to network. It can be turned off by LEDs_EN jumper pad.

  • Status Indicator: Green LED, it will tell whether the module is on, light when the module is running. It can be turned off by LEDs_EN jumper pad.

  • Li-ion Battery: this is power supply for the module, input voltage is from 3.4V to 4.4V. It uses the JST-2.0mm connector, that make it convenient to connect to 3.7V Li-Po Battery.

  • GSM Antenna: this is an uFL GSM antenna connector, just connect it to a GSM antenna for receiving GSM signal.

  • SIM - Card Holder: SIM card holder for standard SIM card

Pin Definitions

NameI/ODescriptionNote
BATPower input / output3.4V - 4.4V DC
GNDPower ground / logic ground
VIOILogic level reference3.0V - 5.0V DC
DTRIWake up pin for module in sleep mode
PWROPower switchLow level pulse
RIOEvent/ message pin
TXDOTransmit dataUART output from SIM808
RXDIReceive dataUART Input to SIM808
RSTIModule rest

Indicator LEDs

Indicator LEDsStatusBehavior
Operating Status (Green)OffSIM808 is not running
OnSIM808 is running
Network Status (Red)OffSIM808 is not running
64ms on/ 800ms OffSIM808 not registered to the network
64ms On/ 3000ms OffSIM808 registered to the network
64ms On/ 300ms OffPPP GPRS communication is established

Usage

The module comes with a mini GPS and GSM antenna, but not includes Li-Po battery. In addition, to use this module, you still need a unlock SIM-Card that supports GPRS service.

  • 3.7 V Li-ion Battery
  • SIM-Card
  • USB to UART Tool

Reference Circuit

Getting Started with AT Command

The module is controlled by AT command via serial port, here we use Arduino as USB to serial tool. Upload the following code to Arduino and open the serial monitor. If you use other USB to serial tools, you can use AT Command Tester or SSCOM32 to test AT commands.

// this sketch is used for testing LoNet with Arduino

// Connect VIO to +5V
// Connect GND to Ground
// Connect RX (data into SIM808) to Digital 11
// Connect TX (data out from SIM808) to Digital 10

#include <SoftwareSerial.h>

SoftwareSerial mySerial(10, 11); // RX, TX

void setup()
{
// Open serial communications and wait for port to open:
Serial.begin(9600);
mySerial.begin(9600);

}

void loop() // run over and over
{
if (mySerial.available())
Serial.write(mySerial.read());

if (Serial.available())
{
while(Serial.available())
{
mySerial.write(Serial.read());
}
mySerial.println();
}
}

Set Baud and Enable Charging Function

It is recommended to execute this process when first time to use the module. In the Serial Monitor columns of following tables, input of AT commands are in back, module returns values are in orange.

Serial Monitor Description
AT OK Send command "AT" to synchronize baud rate. Serial port of module is by default set at auto-baud mode, and in this mode, it will not output any indications when the module is on.
AT+IPR=9600 OK Set baud rate at 9600bps, supports baud rate from 1200bps to 115200bps.
AT+ECHARGE=1 OK Send command "AT+ECHARGE=1" to enable battery charging function. By default the charging function is closed.
AT&W OK Save parameter setting.
AT+CPOWD=1 NORMAL POWER DOWNPower down the module.
RDY +CFUN: 1 GPS Ready +CPIN: READY Call Ready SMS ReadyTurn on the module again by the power button, it will response status about GPS and GSM.
AT+CBC +CBC: 1,96,4175 OKInquire charging status and remaining battery capacity.
AT+CSQ +CSQ: 14,0 OKInquire GSM signal quality.

Get location with GPS

Serial Monitor Description
AT+CGPSPWR=1 OK Open GPS
AT+CGPSSTATUS? +CGPSSTATUS: Location Not FixOK Read GPS fix status, "Location Not Fix" means that positioning is not successful. For the first time to start, it will take at least 30s. GPS must be tested by the window or outdoor.
AT+CGPSSTATUS? +CGPSSTATUS: Location 3D Fix OK GPS has fixed with 3D status.
AT+CGPSINF=0 +CGPSINF: 0,2234.931817,11357.122485,92.461185,20141031041141.000,88,12,0.000000,0.000000 Get the current GPS location information. Parameters formate: <mode>, <altitude>, <longitude>, <UTC time>, <TTFF>, <num>, <speed>, <course>

AT+CGPSOUT=32 OK $GPRMC,043326.000,A, 2234.9414,N,11357.1187,E, 0.000,143.69,311014,,,A*50

Read NMEA $GPRMC data, of which, "2234.9414 N, 11357.1187 E" is the location coordinates. For more details about NMEA sentences, check this site.

AT+CGPSRST=0 OK

Reset GPS in Cold Start Mode.
AT+CGPSRST=1 OKReset GPS in Hot Start Mode.
AT+CGPSPWR=0 OKClose GPS.

Resource

It's a pity that we don't have any demo about LoNet-GSM/GPRS/GPS Breakout in the Recipe yet.

Post your awesome project about LoNet-GSM/GPRS/GPS Breakout to win $100 Coupon!. Please feel free to contact us: [email protected]

Here we introduce some projects about GPRS Shield as a reference.

What is GPRS shield

Features:

  • Compatible with standard Arduino and Arduino Mega

  • Quad band support: 850/900/1800/1900MHz

  • Full control via AT commands set: Standard - GSM 07.07 & 07.05 and Enhanced - SIMCOM AT Commands

  • Support TCP/UDP protocols

SMS Remote Control

This project describes how to turn your hot water heater on and off via SMS and check if it is on or off.

It is reliable, secure, easy and flexible because of the reasons below:

  • Commands are always responded to and lost messages are re-requested

  • It uses 128 bit password protection

  • The pfodDesigner generates all the code, and you can use it to create you own custom menu.

  • All the pfod screens are available via SMS, like sub-menus, multi and single selection list, text input, data logging and plotting.

I want to make it.

Arduino Phone

Arduino phone is a cell phone made by ourselves via combining Arduino and other shield modules.

This project tells us what you need to do when Arduino Phone apps can't fit your needs.

This Arduino Phone contains the following main functions.

  • receive & send message, letter input

  • dial & answer calls

  • real time clock display

  • A convenient and concise UI

I want to make it.

More Awesome Projects by GPRS

Share Your Awesome Projects with Us

Born with the spirit of making and sharing, that is what we believe makes a maker.

And only because of this, the open source community can be as prosperous as it is today.

It does not matter what you are and what you have made, hacker, maker, artist or engineers.

As long as you start sharing your works with others, you are being part of the open source community and you are making your contributions.

Now share your awesome projects with us on Recipe, and win a chance to become the Core User of Seeed.

  • Core Users, are those who show high interests in Seeed products and make significant contributions on Recipe.
  • We cooperate with our Core Users in the development of our new product, this, in another word, the Core Users will have the chance to experience any new products of Seeed before its official launch, and in return we expect valuable feedback from them to help us improve the product performance and user experience. And in most cases when our Core Users have some good ideas of making things, we'll offer hardware pieces, PCBA services as well as technical support. Besides, further commercial cooperation with the Core Users is highly possible.

Get more information about Core User, please email to: [email protected]

Support

Any tech support, please contact [email protected]

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...