edit

ODYSSEY X86J4105

The ODYSSEY - X86J4105, is based on Intel Celeron J4105, a Quad-Core 1.5GHz CPU that bursts up to 2.5GHz. It has all the great features that a standard Computer needs, including an 8GB LPDDR4 RAM, 64GB eMMC Storage(optional), onboard Wi-Fi/BLE, Dual Gigabyte Ethernet Ports, Audio Input and Output, USB Ports, HDMI, SATA Connectors, PCIe, etc.

Key Features:

  • Intel® Celeron® J4105, Quad-Core 1.5-2.5GHZ
  • Dual-Band Frequency 2.5GHz/5GHz WiFi/ Bluetooth 5.0
  • Intel® UHD Graphics 600
  • Dual Gigabit Ethernet
  • Integrated Arduino Coprocessor ATSAMD21 ARM® Cortex®-M0+
  • Raspberry Pi 40-Pin Compatible
  • 2 x M.2 PCIe (B Key and M Key)
  • Pre-installed with Windows 10 Enterprise
  • Compatible with Grove Ecosystem

Hardware Specifications

Components ODYSSEY - X86J4105
Processor Intel® Celeron® J4105 (Frequency: 1.5 - 2.5GHz)
Coprocessor Microchip® ATSAMD21G18 32-Bit ARM® Cortex® M0+
Graphics Intel® UHD Graphics 600 (Frequency: 250 – 750MHz)
Memory LPDDR4 8GB
Storage 64GB eMMC V5.1
Wireless Wi-Fi 802.11 a/b/g/n/ac @ 2.⅘ GHz HT160 & Bluetooth® 5.0
Networking Intel® I211AT PCIe Gigabit LAN
Audio Microphone + headphone Combo Connector
Headers 28-pin header from SAMD21G18 & 40-pin header compatible with Raspberry Pi
USB USB 2.0 Type-A x2, USB 3.1 Type-A x1, USB 3.1 Type-C x1
Video Interfaces HDMI2.0a: Up to 4096x2160 @ 60Hz 24bpp / DP1.2a: Up to 4096x2160 @60Hz 24bpp
Expansion Slots M.2(Key B, 2242/2280): SATA III, USB2.0, UIM; M.2 (Key M, 2242/2280): PCIe 2.0 ×4; Micro SD card Socket; SIM Card Socket; SATA III
RTC JST 1.0 CR2032 3V
TPM Built-in TPM (2.0)
Power DC Jack 5.5/2.1mm or Type-C PD; DC Jack input: 12-19V DC; Type-C input: 12V DC
Dimensions 110x110mm
Certifications FCC, CE

Hardware Overview

Pinout Diagram

Quick Start with ODYSSEY - X86J4105

Hardware Required

  1. ODYSSEY - X86J4105

  2. Power Adapter(provided)

  3. External monitor

  4. HDMI cable

  5. Keyboard and Mouse

Attaching External Storage

For 64 GB EMMC storage version of the ODYSSEY - X86J4105, you can skip this step. However, if you need more storage for your needs, feel free to follow this step.

There are 4 methods of adding storage for ODYSSEY - X86J4105, but only 3 methods support installing the operating system(M.2 SATA, M.2 PCIE and SATA), and the Micro SD card slot can only be used as external storage.

  • Method 1 - M.2 PCIE Connector

  • Method 2 - M.2 SATA Connector

  • Method 3 - SATA Connector

  • Method 4 - Micro SD Card Slot

Installing the Operating System

ODYSSEY - X86J4105 supports both Windows and Linux operating system.

  • For Non-EMMC version, attach extenal storage following previous steps, and install your desired operating system through a bootable USB drive.

  • For EMMC version, Windows 10 Enterprise is pre-installed.

Step 1

Connect bootable USB drive into one of the USB ports on ODYSSEY - X86J4105.

Note: please visit Creating Bootable USB and Installing OS for more information about creating a bootable USB Drive.

Step 2

Press the power button and keep pressing the F7 key on the keyboard until the Boot Manager screen appears.

Step 3

Select the connected USB Drive as the 1st boot drive and press Enter.

Step 4

Follow the instructions on the installation to complete installing the operating system.

Note: To access the BIOS setup, keep pressing F7 key when booting up.

Connecting Antennas

Connect two antennas into the two sockets on the board.

Note: One Antenna is for Wi-Fi and Bluetooth, and the other is for strong 5G Connectivity.

Adding 4G Cellular Connectivity

For 4G Cellular connectivity, insert a standard SIM card into the SIM card slot of the board.

Insert a PCIE 4G Module

Note: This module is a must have if you want to use the connected SIM Card.

Connecting to Display

There are 2 methods for display:

Method 1 - HDMI Port

Method 2 - DP over USB-C Port

Connecting to Keyboard and Mouse

Connect Keyboard and Mouse through USB ports

Powering up

There are two ways to power up the ODYSSEY - X86J4105:

Method 1

The simplest way is to use the 12V/2A power adaptor included in the package, and connect to the DC jack of ODYSSEY - X86J4105.

Method 2

You can also power the ODYSSEY - X86J4105 through the USB-C port with 12V input. Furthermore, if your Monitor supports USB-PD, you are able to power and display ODYSSEY - X86J4105 using only 1 cable!

Performance Stats

Wi-Fi Connecitivity

Bluetooth Connecitivity

Operating as Computer

  • Browsing and watch videos on Youtube

  • Playing Google T-Rex!

Using the Arduino Core (ATSAMD21G18) in Windows

The ODYSSEY - X86J4105 is built with Arduino Core(ATSAMD21G18) which provides more functionality to the board, and to use it, simply download the Arduino IDE, and Install the Windows version.

  1. Click File->Preferences->Additional Boards Manager URL: and Copy the following link into it https://raw.githubusercontent.com/Seeed-Studio/Seeed_Platform/master/package_seeeduino_boards_index.json.

  2. Click Tools->Board:->Boards Manager..., and Boards Manager will appear. Search and install the Seeeduino SAMD Zero board library.

  1. Select the right Port and Board before uploading.

  2. Port -> COM4(Seeeduno Cortex M0+)

  3. Board -> Seeeduino Cortex M0+

  1. Feel free to explore your creativity with ODYSSEY - X86J4105!

Using the Arduino Core (ATSAMD21G18) in Linux OS

If you have installed Linux OS, Download the Linux verison of Arduino IDE and install the IDE as follow:

Installing Arduino IDE

  1. Open terminal and goto Downloads
1
cd ~/Downloads
  1. Use tar command to unzip the downloaded file
1
tar -xvf arduino -1.8.10-linux64.tar.xz
  1. Move the file to opt
1
sudo mv arduino-1.8.10 /opt
  1. Install Arduino IDE and make a Desktop shortcut
1
cd /opt/arduino-1.8.10/ && chmod +x install.sh && ./install.sh
  1. Allow permissions for Arduino to upload
1
cd /opt/arduino-1.8.10 && ./arduino-linux-setup.sh

Installing Board Libraries

  1. Click File->Preferences->Additional Boards Manager URL: and Copy the following link into it https://raw.githubusercontent.com/Seeed-Studio/Seeed_Platform/master/package_seeeduino_boards_index.json.

  2. Click Tools->Board:->Boards Manager..., and Boards Manager will appear. Search and install the Seeeduino SAMD Zero board library.

  1. Select the right Port and Board before uploading.

  2. Port -> ttyACM0(Seeeduno Cortex M0+)

  3. Board -> Seeeduino Cortex M0+

FAQs

How can I access the BIOS setup

Press the Power Button and keep pressing DEL key until you see the BIOS Setup.

Arduino IDE doesn't recognize the onboard microcontroller

Add a jumoer wire between pin 3 and pin 4 of UART pins on the 28-pin header to reset the AMSAMDG21

I cannot connect Wi-Fi and Bluetooth

Check BIOS settings and enable Wi-Fi and Bluetooth from BIOS

ODYSSEY - X86J4105 doesn't power up

Maker sure you use the 12V/2A power adapter provided in the bopx and check connection.

Different status of Power button of ODYSSEY - X86J4105

It has the same power button state as other computers:

  • Short Press(While it's off) -> Turn on

  • Short Press(While it's on) -> Sleep

  • Long Press(While it's on) -> Force shutdown

Is the built-in fan controllable

Currently the fan is controlled by BIOS, and not controlled by user. The fan speed is set according to the CPU temperature. Check Chipset -> FAN Contorl in the BIOS setup screen for more information.

How to upgrade BIOS

For the instrucitons of upgrading BIOS, please check the Installing OS section.

Resources

Tech Support

Please submit any technical issue into our forum