Skip to main content

reSpeaker USB 4-Mic Array XVF3000 v2.0

We are excited to formally introduce the reSpeaker XVF3800 — a comprehensive upgrade to the reSpeaker XVF 3000. Building upon its predecessor's foundation of 4-microphone array architecture, universal compatibility (Windows / macOS / Linux), and dual-firmware (I2S / USB) plug-and-play convenience, the XVF3800 delivers a significant leap in both audio fidelity and algorithmic performance.

Key Upgrade Highlights

  • AI-Powered Audio Algorithms: Integrated suite featuring AEC (Acoustic Echo Cancellation), AGC (Automatic Gain Control), DoA (Direction of Arrival) detection, beamforming, VAD (Voice Activity Detection), noise suppression, and dereverberation — laying robust groundwork for advanced voice applications.
  • 360° Far-Field Voice Capture: Precision voice pickup within a 5-meter radius, effortlessly accommodating conferencing systems, intelligent interaction, and voice-controlled scenarios.
  • Dual Operating Modes: Flexible USB/I2S firmware switching to meet diverse development and deployment requirements.
  • Product Details & Specifications: ReSpeaker XVF3800 4-Mic Array Store Page
  • Quick Start & Wiki Guide: reSpeaker XVF3800 Getting Started Guide | Seeed Studio Wiki

The ReSpeaker Mic Array v2.0 is an upgrade to the original ReSpeaker Mic Array v1.0. This upgraded version is based on XMOS’s XVF-3000, a significantly higher performing chipset than the previously used XVSM-2000. This new chipset includes many voice recognition algorithms to assist in performance. The array can be stacked (connected) right onto the top of the original ReSpeaker Core to significantly improve the voice interaction performance.The microphones have also been improved in this version allowing significant performance improvements over the first generation mic array with only 4 microphones.

The ReSpeaker Mic Array v2.0 supports USB Audio Class 1.0 (UAC 1.0) directly. All major Operating System, including Windows,macOS, and Linux are compatible with UAC 1.0, allowing the mic array to function as a sound card without the ReSpeaker Core,while also retaining voice algorithms, such as DoA, BF, and AEC on those systems.

The ReSpeaker Mic Array v2.0 is a great solution for those who wish to add voice interface into their existing products or future products. It also works well as an entry point to higher level voice interface evaluation. The board allows some flexibility for customization upon request.

The ReSpeaker Mic Array v2.0 has two firmware versions available, one including speech algorithms and a second for raw voice data.

Version​

Product VersionChangesReleased Date
ReSpeaker Mic Array v1.0InitialAug 15, 2016
ReSpeaker Mic Array v2.0XVSM-2000 is EOL,change MCU to XVF-3000 and reduce the Mics from 7 to 4.Jan 25, 2018

Features​

  • Far-field voice capture
  • Support USB Audio Class 1.0 (UAC 1.0)
  • Four microphones array
  • 12 programmable RGB LED indicators
  • Speech algorithms and features
    • Voice Activity Detection
    • Direction of Arrival
    • Beamforming
    • Noise Suppression
    • De-reverberation
    • Acoustic Echo Cancellation

Specification​

  • XVF-3000 from XMOS
  • 4 high performance digital microphones
  • Supports Far-field Voice Capture
  • Speech algorithm on-chip
  • 12 programmable RGB LED indicators
  • Microphones: ST MP34DT01TR-M
  • Sensitivity: -26 dBFS (Omnidirectional)
  • Acoustic overload point: 120 dBSPL
  • SNR: 61 dB
  • Power Supply: 5V DC from Micro USB or expansion header
  • Dimensions: 70mm (Diameter)
  • 3.5mm Audio jack output socket
  • Power consumption: 5V, 180mA with led on and 170mA with led off
  • Max Sample Rate:16Khz

Hardware Overview​

  • ① XMOS XVF-3000: It integrates advanced DSP algorithms that include Acoustic Echo Cancellation (AEC), beamforming, dereverberation, noise suppression and gain control.

  • ② Digital Microphone: The MP34DT01-M is an ultra-compact, lowpower, omnidirectional, digital MEMS microphone built with a capacitive sensing element and an IC interface.

  • ③ RGB LED: Three-color RGB LED.

  • ④ USB Port: Provide the power and control the mic array.

  • ⑤ 3.5mm Headphone jack: Output audio, We can plug active speakers or Headphones into this port.

  • ⑥ WM8960: The WM8960 is a low power stereo codec featuring Class D speaker drivers to provide 1 W per channel into 8 W loads.

System Diagram

Pin Map

Dimensions

Applications​

  • USB Voice Capture
  • Smart Speaker
  • Intelligent Voice Assistant Systems
  • Voice Recorders
  • Voice Conferencing System
  • Meeting Communicating Equipment
  • Voice Interacting Robot
  • Car Voice Assistant
  • Other Voice Interface Scenarios

Getting Started​

note

ReSpeaker Mic Array v2.0 is compatiable with Windows, Mac, Linux systems andriod. The below scripts are tested on Python2.7.

For andriod, we tested it with emteria.OS(andriod 7.1) on Raspberry. We plug the mic array v2.0 to raspberry pi USB port and select the ReSpeaker mic array v2.0 as audio device. Here is the audio recording screen.

Here is the audio playing screen. We plug speaker to ReSpeaker mic array v2.0 3.5mm audio jack and hear what we record.

Update Firmware​

There are 2 firmwares. One includes 1 channel data, while the other inlcudes 6 channels data (factory firmware). Here is the table for the differences.

FirmwareChannelsNote
1_channel_firmware.bin1Processed audio for ASR
6_channels_firmware.bin6Channel 0: processed audio for ASR
Channel 1: mic1 raw data
Channel 2: mic2 raw data
Channel 3: mic3 raw data
Channel 4: mic4 raw data
Channel 5: merged playback

For Linux: The Mic array supports the USB DFU. We develop a python script dfu.py to update the firmware through USB.

sudo apt-get update
sudo pip install pyusb click
git clone https://github.com/respeaker/usb_4_mic_array.git
cd usb_4_mic_array
sudo python dfu.py --download 6_channels_firmware.bin # The 6 channels version

# if you want to use 1 channel,then the command should be like:

sudo python dfu.py --download 1_channel_firmware.bin

Here is the firmware downloading result.

For Windows/Mac: We do not suggest use Windows/Mac and Linux vitual machine to update the firmware.

Out of Box Demo​

Here is the Acoustic Echo Cancellation example with 6 channels firmware.

  • Step 1. Connect the USB cable to PC and audio jack to speaker.

  • Step 2. Select the mic array v2.0 as output device in PC side.
  • Step 3. Start the audacity to record.
  • Step 4. Play music at PC side first and then we talk.
  • Step 5. We will see the audacity screen as below, Please click Solo to hear each channel audio.

Channel0 Audio(processed by algorithms):

Channel1 Audio(Mic1 raw data):

Channel5 Audio(Playback data):

Here is the video about the DOA and AEC.

Install DFU and LED Control Driver​

  • Windows: Audio recording and playback works well by default. Libusb-win32 driver is only required to control LEDs an DSP parameters on Windows. We use a handy tool - Zadig to install the libusb-win32 driver for both SEEED DFU and SEEED Control (ReSpeaker Mic Array has 2 devices on Windows Device Manager).

caution

Please make sure that libusb-win32 is selected, not WinUSB or libusbK.

  • MAC: No driver is required.
  • Linux: No driver is required.

Tuning​

For Linux/Mac/Windows: We can configure some parameters of built-in algorithms.

  • Get the full list parameters, for more info, please refer to FAQ.
git clone https://github.com/respeaker/usb_4_mic_array.git
cd usb_4_mic_array
python tuning.py -p
  • Example#1, we can turn off Automatic Gain Control (AGC):
python tuning.py AGCONOFF 0
  • Example#2, We can check the DOA angle.
pi@raspberrypi:~/usb_4_mic_array $ sudo python tuning.py DOAANGLE
DOAANGLE: 180

Control the LEDs​

We can control the ReSpeaker Mic Array V2's LEDs through USB. The USB device has a Vendor Specific Class Interface which can be used to send data through USB Control Transfer. We refer pyusb python library and come out the usb_pixel_ring python library.

The LED control command is sent by pyusb's usb.core.Device.ctrl_transfer(), its parameters as below:

ctrl_transfer(usb.util.CTRL_OUT | usb.util.CTRL_TYPE_VENDOR | usb.util.CTRL_RECIPIENT_DEVICE, 0, command, 0x1C, data, TIMEOUT)

Here are the usb_pixel_ring APIs.

CommandDataAPINote
0[0]pixel_ring.trace()trace mode, LEDs changing depends on VADand DOA
1[red, green, blue, 0]pixel_ring.mono()mono mode, set all RGB LED to a single color, for example Red(0xFF0000), Green(0x00FF00), Blue(0x0000FF)
2[0]pixel_ring.listen()listen mode, similar with trace mode, but not turn LEDs off
3[0]pixel_ring.speak()wait mode
4[0]pixel_ring.think()speak mode
5[0]pixel_ring.spin()spin mode
6[r, g, b, 0] * 12pixel_ring.custimize()custom mode, set each LED to its own color
0x20[brightness]pixel_ring.set_brightness()set brightness, range: 0x00~0x1F
0x21[r1, g1, b1, 0, r2, g2, b2, 0]pixel_ring.set_color_palette()set color palette, for example, pixel_ring.set_color_palette(0xff0000, 0x00ff00) together with pixel_ring.think()
0x22[vad_led]pixel_ring.set_vad_led()set center LED: 0 - off, 1 - on, else - depends on VAD
0x23[volume]pixel_ring.set_volume()show volume, range: 0 ~ 12
0x24[pattern]pixel_ring.change_pattern()set pattern, 0 - Google Home pattern, others - Echo pattern

For Linux: Here is the example to control the leds. Please follow below commands to run the demo.

git clone https://github.com/respeaker/pixel_ring.git
cd pixel_ring
sudo python setup.py install
sudo python examples/usb_mic_array.py

Here is the code of the usb_mic_array.py.

import time
from pixel_ring import pixel_ring


if __name__ == '__main__':
pixel_ring.change_pattern('echo')
while True:

try:
pixel_ring.wakeup()
time.sleep(3)
pixel_ring.think()
time.sleep(3)
pixel_ring.speak()
time.sleep(6)
pixel_ring.off()
time.sleep(3)
except KeyboardInterrupt:
break


pixel_ring.off()
time.sleep(1)

For Windows/Mac: Here is the example to control the leds.

  • Step 1. Download pixel_ring.
git clone https://github.com/respeaker/pixel_ring.git
cd pixel_ring/pixel_ring
  • Step 2. Create a led_control.py with below code and run 'python led_control.py'
from usb_pixel_ring_v2 import PixelRing
import usb.core
import usb.util
import time

dev = usb.core.find(idVendor=0x2886, idProduct=0x0018)
print dev
if dev:
pixel_ring = PixelRing(dev)

while True:
try:
pixel_ring.wakeup(180)
time.sleep(3)
pixel_ring.listen()
time.sleep(3)
pixel_ring.think()
time.sleep(3)
pixel_ring.set_volume(8)
time.sleep(3)
pixel_ring.off()
time.sleep(3)
except KeyboardInterrupt:
break

pixel_ring.off()
note

If you see "None" printed on screen, please reinstall the libusb-win32 driver.

DOA (Direction of Arrival)​

For Windows/Mac/Linux: Here is the example to view the DOA. The Green LED is the indicator of the voice direction. For the angle, please refer to hardware overview.

  • Step 1. Download the usb_4_mic_array.
git clone https://github.com/respeaker/usb_4_mic_array.git
cd usb_4_mic_array
  • Step 2. Create a DOA.py with below code under usb_4_mic_array folder and run 'python DOA.py'
from tuning import Tuning
import usb.core
import usb.util
import time

dev = usb.core.find(idVendor=0x2886, idProduct=0x0018)

if dev:
Mic_tuning = Tuning(dev)
print Mic_tuning.direction
while True:
try:
print Mic_tuning.direction
time.sleep(1)
except KeyboardInterrupt:
break
  • Step 3. We will see the DOA as below.
pi@raspberrypi:~/usb_4_mic_array $ sudo python doa.py 
184
183
175
105
104
104
103

VAD (Voice Activity Detection)​

For Windows/Mac/Linux: Here is the example to view the VAD. The Red LED is the indicator of the VAD.

  • Step 1. Download the usb_4_mic_array.
git clone https://github.com/respeaker/usb_4_mic_array.git
cd usb_4_mic_array
  • Step 2. Create a VAD.py with below code under usb_4_mic_array folder and run 'python VAD.py'
from tuning import Tuning
import usb.core
import usb.util
import time

dev = usb.core.find(idVendor=0x2886, idProduct=0x0018)
#print dev
if dev:
Mic_tuning = Tuning(dev)
print Mic_tuning.is_voice()
while True:
try:
print Mic_tuning.is_voice()
time.sleep(1)
except KeyboardInterrupt:
break
  • Step 3. We will see the DOA as below.
pi@raspberrypi:~/usb_4_mic_array $ sudo python VAD.py 
0
0
0
1
0
1
0
note

For the threshold of VAD, we also can use the GAMMAVAD_SR to set. Please refer to Tuning for more detail.

Extract Voice​

We use PyAudio python library to extract voice through USB.

For Linux: We can use below commands to record or play the voice.

arecord -D plughw:1,0 -f cd test.wav # record, please use the arecord -l to check the card and hardware first
aplay -D plughw:1,0 -f cd test.wav # play, please use the aplay -l to check the card and hardware first
arecord -D plughw:1,0 -f cd |aplay -D plughw:1,0 -f cd # record and play at the same time

We also can use python script to extract voice.

  • Step 1, We need to run the following script to get the device index number of Mic Array:
sudo pip install pyaudio
cd ~
nano get_index.py
import pyaudio

p = pyaudio.PyAudio()
info = p.get_host_api_info_by_index(0)
numdevices = info.get('deviceCount')

for i in range(0, numdevices):
if (p.get_device_info_by_host_api_device_index(0, i).get('maxInputChannels')) > 0:
print "Input Device id ", i, " - ", p.get_device_info_by_host_api_device_index(0, i).get('name')
  • Step 3, press Ctrl + X to exit and press Y to save.

  • Step 4, run 'sudo python get_index.py' and we will see the device ID as below.

Input Device id  2  -  ReSpeaker 4 Mic Array (UAC1.0): USB Audio (hw:1,0)
  • Step 5, change RESPEAKER_INDEX = 2 to index number. Run python script record.py to record a speech.
import pyaudio
import wave

RESPEAKER_RATE = 16000
RESPEAKER_CHANNELS = 6 # change base on firmwares, 1_channel_firmware.bin as 1 or 6_channels_firmware.bin as 6
RESPEAKER_WIDTH = 2
# run getDeviceInfo.py to get index
RESPEAKER_INDEX = 2 # refer to input device id
CHUNK = 1024
RECORD_SECONDS = 5
WAVE_OUTPUT_FILENAME = "output.wav"

p = pyaudio.PyAudio()

stream = p.open(
rate=RESPEAKER_RATE,
format=p.get_format_from_width(RESPEAKER_WIDTH),
channels=RESPEAKER_CHANNELS,
input=True,
input_device_index=RESPEAKER_INDEX,)

print("* recording")

frames = []

for i in range(0, int(RESPEAKER_RATE / CHUNK * RECORD_SECONDS)):
data = stream.read(CHUNK)
frames.append(data)

print("* done recording")

stream.stop_stream()
stream.close()
p.terminate()

wf = wave.open(WAVE_OUTPUT_FILENAME, 'wb')
wf.setnchannels(RESPEAKER_CHANNELS)
wf.setsampwidth(p.get_sample_size(p.get_format_from_width(RESPEAKER_WIDTH)))
wf.setframerate(RESPEAKER_RATE)
wf.writeframes(b''.join(frames))
wf.close()
  • Step 6. If you want to extract channel 0 data from 6 channels, please follow below code. For other channel X, please change [0::6] to [X::6].
import pyaudio
import wave
import numpy as np

RESPEAKER_RATE = 16000
RESPEAKER_CHANNELS = 6 # change base on firmwares, 1_channel_firmware.bin as 1 or 6_channels_firmware.bin as 6
RESPEAKER_WIDTH = 2
# run getDeviceInfo.py to get index
RESPEAKER_INDEX = 3 # refer to input device id
CHUNK = 1024
RECORD_SECONDS = 3
WAVE_OUTPUT_FILENAME = "output.wav"

p = pyaudio.PyAudio()

stream = p.open(
rate=RESPEAKER_RATE,
format=p.get_format_from_width(RESPEAKER_WIDTH),
channels=RESPEAKER_CHANNELS,
input=True,
input_device_index=RESPEAKER_INDEX,)

print("* recording")

frames = []

for i in range(0, int(RESPEAKER_RATE / CHUNK * RECORD_SECONDS)):
data = stream.read(CHUNK)
# extract channel 0 data from 6 channels, if you want to extract channel 1, please change to [1::6]
a = np.fromstring(data,dtype=np.int16)[0::6]
frames.append(a.tostring())

print("* done recording")

stream.stop_stream()
stream.close()
p.terminate()

wf = wave.open(WAVE_OUTPUT_FILENAME, 'wb')
wf.setnchannels(1)
wf.setsampwidth(p.get_sample_size(p.get_format_from_width(RESPEAKER_WIDTH)))
wf.setframerate(RESPEAKER_RATE)
wf.writeframes(b''.join(frames))
wf.close()

For Windows:

  • Step 1. We run below command to install pyaudio.
 pip install pyaudio
C:\Users\XXX\Desktop>python get_index.py
Input Device id 0 - Microsoft Sound Mapper - Input
Input Device id 1 - ReSpeaker 4 Mic Array (UAC1.0)
Input Device id 2 - Internal Microphone (Conexant I)
  • Step 3. Modify the device index and channels of record.py and then extract voice.
C:\Users\XXX\Desktop>python record.py
* recording
* done recording
caution

If we see "Error: %1 is not a valid Win32 application.", please install Python Win32 version.

For MAC:

  • Step 1. We run below command to install pyaudio.
 pip install pyaudio
MacBook-Air:Desktop XXX$ python get_index.py 
Input Device id 0 - Built-in Microphone
Input Device id 2 - ReSpeaker 4 Mic Array (UAC1.0)
  • Step 3. Modify the device index and channels of record.py and then extract voice.
MacBook-Air:Desktop XXX$ python record.py 
2018-03-24 14:53:02.400 Python[2360:16629] 14:53:02.399 WARNING: 140: This application, or a library it uses, is using the deprecated Carbon Component Manager for hosting Audio Units. Support for this will be removed in a future release. Also, this makes the host incompatible with version 3 audio units. Please transition to the API's in AudioComponent.h.
* recording
* done recording

FAQ​

Q1: Parameters of built-in algorithms

pi@raspberrypi:~/usb_4_mic_array $ python tuning.py -p
name type max min r/w info
-------------------------------
AECFREEZEONOFF int 1 0 rw Adaptive Echo Canceler updates inhibit.
0 = Adaptation enabled
1 = Freeze adaptation, filter only
AECNORM float 16 0.25 rw Limit on norm of AEC filter coefficients
AECPATHCHANGE int 1 0 ro AEC Path Change Detection.
0 = false (no path change detected)
1 = true (path change detected)
AECSILENCELEVEL float 1 1e-09 rw Threshold for signal detection in AEC [-inf .. 0] dBov (Default: -80dBov = 10log10(1x10-8))
AECSILENCEMODE int 1 0 ro AEC far-end silence detection status.
0 = false (signal detected)
1 = true (silence detected)
AGCDESIREDLEVEL float 0.99 1e-08 rw Target power level of the output signal.
[−inf .. 0] dBov (default: −23dBov = 10log10(0.005))
AGCGAIN float 1000 1 rw Current AGC gain factor.
[0 .. 60] dB (default: 0.0dB = 20log10(1.0))
AGCMAXGAIN float 1000 1 rw Maximum AGC gain factor.
[0 .. 60] dB (default 30dB = 20log10(31.6))
AGCONOFF int 1 0 rw Automatic Gain Control.
0 = OFF
1 = ON
AGCTIME float 1 0.1 rw Ramps-up / down time-constant in seconds.
CNIONOFF int 1 0 rw Comfort Noise Insertion.
0 = OFF
1 = ON
DOAANGLE int 359 0 ro DOA angle. Current value. Orientation depends on build configuration.
ECHOONOFF int 1 0 rw Echo suppression.
0 = OFF
1 = ON
FREEZEONOFF int 1 0 rw Adaptive beamformer updates.
0 = Adaptation enabled
1 = Freeze adaptation, filter only
FSBPATHCHANGE int 1 0 ro FSB Path Change Detection.
0 = false (no path change detected)
1 = true (path change detected)
FSBUPDATED int 1 0 ro FSB Update Decision.
0 = false (FSB was not updated)
1 = true (FSB was updated)
GAMMAVAD_SR float 1000 0 rw Set the threshold for voice activity detection.
[−inf .. 60] dB (default: 3.5dB 20log10(1.5))
GAMMA_E float 3 0 rw Over-subtraction factor of echo (direct and early components). min .. max attenuation
GAMMA_ENL float 5 0 rw Over-subtraction factor of non-linear echo. min .. max attenuation
GAMMA_ETAIL float 3 0 rw Over-subtraction factor of echo (tail components). min .. max attenuation
GAMMA_NN float 3 0 rw Over-subtraction factor of non- stationary noise. min .. max attenuation
GAMMA_NN_SR float 3 0 rw Over-subtraction factor of non-stationary noise for ASR.
[0.0 .. 3.0] (default: 1.1)
GAMMA_NS float 3 0 rw Over-subtraction factor of stationary noise. min .. max attenuation
GAMMA_NS_SR float 3 0 rw Over-subtraction factor of stationary noise for ASR.
[0.0 .. 3.0] (default: 1.0)
HPFONOFF int 3 0 rw High-pass Filter on microphone signals.
0 = OFF
1 = ON - 70 Hz cut-off
2 = ON - 125 Hz cut-off
3 = ON - 180 Hz cut-off
MIN_NN float 1 0 rw Gain-floor for non-stationary noise suppression.
[−inf .. 0] dB (default: −10dB = 20log10(0.3))
MIN_NN_SR float 1 0 rw Gain-floor for non-stationary noise suppression for ASR.
[−inf .. 0] dB (default: −10dB = 20log10(0.3))
MIN_NS float 1 0 rw Gain-floor for stationary noise suppression.
[−inf .. 0] dB (default: −16dB = 20log10(0.15))
MIN_NS_SR float 1 0 rw Gain-floor for stationary noise suppression for ASR.
[−inf .. 0] dB (default: −16dB = 20log10(0.15))
NLAEC_MODE int 2 0 rw Non-Linear AEC training mode.
0 = OFF
1 = ON - phase 1
2 = ON - phase 2
NLATTENONOFF int 1 0 rw Non-Linear echo attenuation.
0 = OFF
1 = ON
NONSTATNOISEONOFF int 1 0 rw Non-stationary noise suppression.
0 = OFF
1 = ON
NONSTATNOISEONOFF_SR int 1 0 rw Non-stationary noise suppression for ASR.
0 = OFF
1 = ON
RT60 float 0.9 0.25 ro Current RT60 estimate in seconds
RT60ONOFF int 1 0 rw RT60 Estimation for AES. 0 = OFF 1 = ON
SPEECHDETECTED int 1 0 ro Speech detection status.
0 = false (no speech detected)
1 = true (speech detected)
STATNOISEONOFF int 1 0 rw Stationary noise suppression.
0 = OFF
1 = ON
STATNOISEONOFF_SR int 1 0 rw Stationary noise suppression for ASR.
0 = OFF
1 = ON
TRANSIENTONOFF int 1 0 rw Transient echo suppression.
0 = OFF
1 = ON
VOICEACTIVITY int 1 0 ro VAD voice activity status.
0 = false (no voice activity)
1 = true (voice activity)

Q2: ImportError: No module named usb.core

A2: Run sudo pip install pyusb to install the pyusb.

pi@raspberrypi:~/usb_4_mic_array $ sudo python tuning.py DOAANGLE
Traceback (most recent call last):
File "tuning.py", line 5, in <module>
import usb.core
ImportError: No module named usb.core
pi@raspberrypi:~/usb_4_mic_array $ sudo pip install pyusb
Collecting pyusb
Downloading pyusb-1.0.2.tar.gz (54kB)
100% |████████████████████████████████| 61kB 101kB/s
Building wheels for collected packages: pyusb
Running setup.py bdist_wheel for pyusb ... done
Stored in directory: /root/.cache/pip/wheels/8b/7f/fe/baf08bc0dac02ba17f3c9120f5dd1cf74aec4c54463bc85cf9
Successfully built pyusb
Installing collected packages: pyusb
Successfully installed pyusb-1.0.2
pi@raspberrypi:~/usb_4_mic_array $ sudo python tuning.py DOAANGLE
DOAANGLE: 180

Q3: Do you have the example for Raspberry alexa application?

A3: Yes, we can connect the mic array v2.0 to raspberry usb port and follow Raspberry Pi Quick Start Guide with Script to do the voice interaction with alexa.

Q4: Do you have the example for Mic array v2.0 with ROS system?

A4: Yes, thanks for Yuki sharing the package for integrating ReSpeaker Mic Array v2 with ROS (Robot Operating System) Middleware.

Q5: How to enable 3.5mm audio port to receive the signal as well as usb port?

A5: Please download the new firmware and burn the XMOS by following How to update firmware.

Resource​

Tech Support & Product Discussion​

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...