W600 Module
The W600 Module is a cost-effective 2.4GHz WiFi module support 802.11b/g/n. Seeed W600 Module is based on the W600 chip which features ARM Cortex-M3 with 1MB on-chip flash and freeRTOS kernel.
We take the pins of the W600 chip out and put them on the back of the board, including I2S/I2C/SPI/GPIO/PWM/UART/SDIO. In addition, this module has an on-board PCB Antenna, no need to design the antenna separately, so you can quickly deploy the module to your own board. We also have made CE/FCC certification for this module and you can use it directly for business projects.
Features
• Integrated 32bit Embedded Cortex-M3 CPU, operating frequency 80MHz
• Integrated 288KB RAM
• Integrated 1MB FLASH
Interface
• Integrated GPIO device controller
• Integrated 2 UART interface, support RTS/CTS, baud rate: 1200bps~2Mbps
• Integrated one high speed SPI controller, operating frequency: 0~50MHz;
Wireless
• Support IEEE802.11 b/g/e/i/d/k/r/s/w/n
• Support 2.4~2.4835 GHz
• Support Wi-Fi WMM/WMM-PS/WPA/WPA2/WPS
• Support Wi-Fi Direct
• STBC、GreenField、Short-GI
• Support multiple network protocols: TCP/UDP/ICMP/DHCP/DNS/HTTP
Others
• Supports AT+ instruction protocol based on ASCII encoding (UART interface)
• Support for user‐programmable GPIO control
• On-board Antenna
Specification
Category | Item | Parameter |
---|---|---|
Wireless | Support Wi‐Fi Mode | IEEE802.11b/g/n |
RF system impedance | 50Ω | |
Frequency Range | 2.4~2.4835 GHz | |
Receiving sensitivity | 20MHz MCS7@‐71dBm; 40MHz MCS7@‐68dBm; 54Mbps@‐73dBm; 11Mbps@‐86dBm; 1Mbps@‐95dBm; | |
Physical layer data rate | 802.11n MCS 0~7 150Mbps | |
Modulation | DSSS、OFDM、DBPSK、DQPSK、CCK、QAM16/64 | |
Output Power | IEEE802.11b, DSSS 1Mbps, POUT = +17dBm; IEEE802.11g, OFDM 54Mbps, POUT = +10dBm; IEEE802.11n, OFDM MCS7, POUT = +10dBm | |
Hardware | Interface Type | UART/SPI/GPIO |
Interface rate | 2Mbps@UART (Max) 50Mbps@SPI (Max) | |
Operating Voltage | 3.3V(Module)/5V(Development Board) | |
Operating humidity | 5%~90% (No condensation) | |
storage temperature | ‐40~+125 ℃ | |
Operating temperature | ‐40~+85℃ | |
Software | Network Type | STA/AP/AP+STA/Wi‐Fi Direct |
Verification | WEP/WPA‐PSK/WPA2‐PSK | |
Encryption | WEP64/WEP128/TKIP/CCMP(AES) | |
WPS Function | WPS | |
Energy saving | PS‐POLL/Standby | |
Network protocol | TCP/UDP/ARP/ICMP/DHCP/DNS/HTTP | |
Interface Protocol | AT+ instruction set |
For more detail about specifications, please check the W600 Specification V1.0.0_EN.pdf and W600 HardwareDesignGuide_v1.0.1.pdf
Typical Applications
- intelligent home appliances
- smart home
- wireless audio and video
- smart toys
- medical monitoring
- industrial control
- other Internet of Things applications
Hardware Overview
Block Diagram
Pinout
Getting Started
To use the W600 Module, you need to use USB-to-Serial Tools to connect the RX/TX pins to your computer, also you need to power this module with the 3.3v and GND pins.
For mac, we found that some version of mac system can not recognize the on-board USB-to-Serial chip CH330N, please check here for solution Mac os driver issue
We use the serial port tool sscom to send the AT command. You can use your favorite serial port tool, in case you want to use sscom, you can download it Here.
What ever, please make sure you have checked the option AddCrLf, and set the baud rate to 115200
Tap AT+ then click SEND or press ++enter++ key to to check if the connection was successfully established.
AT+
When it returns +OK, you can use the AT command to control this module.
Create a SoftAP process
- 1- WPRT sets the wireless network card working mode to SoftAP:
AT+WPRT=2
- 2- APSSID Set the AP SSID for the STA, e.g.MyAP:
AT+APSSID=MyAp
- 3- APENCRY Set the wireless network card security mode to WEP64:
AT+APENCRY=1
Parameter:
open:0,WEP64:1,WEP128:2
- 4- APKEY Set the wireless network card key to 12345
AT+APKEY=1,1,12345
Parameter 1:Key format, 0 means HEX, 1 means ASCII
Parameter 2:index: Key index number, 1 to 4 are used for WEP encryption keys, and other encryption methods are fixed to 0.
Parameter 3:wireless key, e.g.:12345
- 5- APNIP Set the ip address and subnet mask
AT+APNIP=1,192.168.1.1,255.255.255.0,192.168.1.1,192.168.1.1
Parameter 1:address type: 0 means dynamic allocation using DHCP, 1 means static address
parameter 2:ip:192.168.1.1
parameter 3:netmask:255.255.255.0
parameter 4:gateway:192.168.1.1
parameter 5:dns:192.168.1.1
- 6- PMTF saves the above parameters to spi flash, just start from step 7 with the next boot.
AT+PMTF
- 7- WJOIN Create wireless network MyAp
AT+WJOIN
- 8- SLIST Query the STA information which connected to your SoftAP.
AT+SLIST
Scan AP Process
Wireless network card scanning AP's AT command is :
AT+WSCAN
The last paremeter is the signal strength, unit db
STA joins the AP process
- 1- WPRT Set the working mode to STA
AT+WPRT=0
- 2- SSID Set the AP name to join. e.g. TEST_AP
AT+SSID=TEST_AP
- 3- KEY Set the wireless key of the AP you want to join. e.g. 12345678
AT+KEY=1,0,12345678
parameter 1:0 means HEX, 1 means ASCII
parameter 2:index: The key index number, 1 to 4 is used for the WEP encryption key. The other encryption methods are fixed to 0.
parameter 3: Wireless key e.g.:12345678
- 4- NIP Enable DHCP
AT+NIP=0
- 5- PMTF Save the above parameters to spi flash, Just start from step 6 with the next boot
AT+PMTF
- 6- WJOIN Join the wireless network TEST_AP
AT+WJOIN
Create an APSTA process
- 1- WPRT Set the working mode to APSTA
AT+WPRT=3
- 2- SSID Set the AP name to be joined, such as TEST_AP
AT+SSID=TEST_AP
- 3- KEY Set the wireless key of the AP you want to join. e.g. 12345678
AT+KEY=1,0,12345678
parameter 1:0 means HEX, 1 means ASCII
parameter 2:index: The key index number, 1 to 4 is used for the WEP encryption key. The other encryption methods are fixed to 0.
parameter 3: Wireless key e.g.:12345678
- 4- APSSID Set the network name of the created SOFTAP
AT+APSSID=”MYSoftAP”
- 5- APENCRY Set the encryption type of SoftAP (such as WPA2-TKIP)
AT+APENCRY=5
- 6- APKEY Set the password for SoftAP (e.g. ASCII code 87654321)
AT+APKEY=1,0,87654321
- 7- APNIP Set the IP address and subnet mask
AT+APNIP=1,192.168.1.1,255.255.255.0,192.168.1.1,192.168.1.1
- 8- PMTF Save the above parameters to spi flash, just start from step 9
AT+PMTF
- 9- WJOIN Join the wireless network TEST_AP
AT+WJOIN
For more detail about AT command, please check the WM_W60X_SDK_AT Command_V1.0.2.pdf
Firmware Programming
For the firmware programming please check here:
WM_W60X_SDK_User Manual_V1.0.0.pdf and WM_W60X_Firmware Generation Guide_V1.1.pdf
FAQ
Q1.How the STA disconnects the AP
A: The wireless network card disconnects the AP's AT command:
AT+WLEAV
Q2.SoftAP disconnected
A: The AT command of SoftAP disconnected network is:
AT+WLEAV=2
Q3.How STA view current status
A: The AT command for the wireless network card to view the status of the current network card is:
AT+LKSTT
Q4. How to View current SoftAP status
A: The AT command to view the current SoftAP status is:
AT+APLKSTT
Schematic Online Viewer
Resouce
[ZIP] sscom
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.