Skip to main content

Displaying Anti-aliased Fonts

This repo demonstrates how to use Anti-aliased fonts in Wio Terminal (i.e. Displaying Japanese characters, Greek characters and other UCS-2 glyphs)! Further, smooth fonts can also be used to display Normal English characters with your favorite font in your computer.

Libraries Installation

Installing the SD Card library for Wio Terminal

Installing the TFT LCD Library For Wio Terminal

Generate vlw Font file

Here demonstrates how to generate a vlw font file that can be used for smooth font in Wio Terminal.

Step 1

Download the Processing software and download according to your operating system.

Step 2

Open Processing, and navigate to Tools -> Create Font...

Step 3

A Create Font Window will appear. You are able to choose the font available from your computer. Change the font size, and click Characters.... You can also change the Filename of the vlw file.

Step 4

A Character Selector window will appear, and you are able to choose the specific language Unicode Characters Blocks(i.e Basic Latin in this case). For Asian characters, CJK Compatibility or CJK category unicode Blocks are recommended to use. Click OK to save font settings.

Step 5

Navigate to File -> Save and save the sketch file into your local drive in your computer. Now, we have generated the vlw font file!

Storing into SD Card

Once generated the vlw font file, you can find the vlw file inside data folder inside the sketch file you saved in the previous step.

Now, copy the vlw font file into the SD card and put the SD card back in Wio Terminal.

Configuring the LCD Library

By default, the smooth font option for LCD Library is turned off to save resources on Wio Terminal. So it needs to be configured to enable smooth font in Wio Terminal.

Navigate to the Arduino Library folders(libraries) -> Seeed_Arduino_LCD and open User_Setup.h with editor. Search #define SMOOTH_FONT and uncomment the line as followed:

Now you have enabled smooth font in Wio Terminal, you can display any fonts or characters that you like!

Displaying

  • To load font from SD card to Wio Terminal:
void loadFont(String fontName);

where fontName is the name of the vlw font file.

  • To show all the characters inside vlw on screen:
void showFont(uint32_t td);

where td is the delay time between screens while showing all the characters.

  • To unload fonts:
void unloadFont();

To display characters in screen, you can use the functions just like in the tft libraries using tft.println(). Further, you can use other functions like tft.setCursor() and tft.setTextColor to change the position and color of character displaying.

Note: Please check the User_Setup.h in the LCD library and make sure that #define SMOOTH_FONT is uncommented.

Complete Code

Please download the complete code and the example vlw files here.

#include<SPI.h>
#include "Seeed_FS.h"
#include "SD/Seeed_SD.h"
#include"TFT_eSPI.h"

TFT_eSPI tft;

void setup() {
tft.begin();
Serial.begin(115200);
tft.setRotation(3);
tft.fillScreen(TFT_BLACK); //Black background

while(!SD.begin(SDCARD_SS_PIN, SDCARD_SPI)){
Serial.println("SD card error!\n");
while(1);
}
delay(1000);

tft.loadFont("Apple-Chancery-24");
// Show all characters on screen with 2 second (2000ms) delay between screens
tft.showFont(2000); // Note: This function moves the cursor position!

tft.setTextColor(TFT_RED,TFT_BLACK);
tft.setCursor(0,0);

tft.println("Konnichiwa");
tft.println("Sayonara");
tft.println();
tft.unloadFont();

tft.loadFont("Latin-Hiragana-24");
tft.setTextColor(TFT_GREEN,TFT_BLACK);
tft.println("こんにちは");
tft.println("さようなら");
tft.unloadFont();

}
void loop(){}

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...