Skip to main content

Getting Started with Light Sensor

This repo demonstrates how to use the built-in light sensor as a component in Wio Terminal. The light sensor uses Analog interface and you can simply read the surrounding Light sensor values via reading its pin.

Example Code

Note: WIO_LIGHT is the pin for builtin Light Sensor. The Light sensor is connected to A13.

void setup() {
pinMode(WIO_LIGHT, INPUT);
Serial.begin(115200);

}

void loop() {
int light = analogRead(WIO_LIGHT);
Serial.print("Light value: ");
Serial.println(light);
delay(200);
}

Note: The light sensor is at the back of the Wio Terminal, just above the microSD card slot.

Loading Comments...