Skip to main content

Xadow - RGB OLED 96*64

RBG OLED is a 16 bit 9664 dot matrix OLED display module with RGB color. It is based on SSD1331 module which is a single chip CMOS OLED/PLED driver with 288 segments and 64 common output, supporting up to 96 RGB 64 dot matrix display. It use SPI for communication.

Specifications​


  • Power Voltage (VCC):3.3V
  • Display Color: RGB
  • Dot Matrix: 96*64
  • Operating temperature: -20~70 ℃
  • Dimensions: 25.43mm x 20.35mm

Pin Definition​


We only need CS, DC, MOSI, SCLK 4 pins for communication. and

CS <==> A5

DC <==> 3

MOSI <==> 16

SCLK <==> 15

caution

Please notice: heavy impact or stress on OLED will cause the breakdown of screen.

Getting Started​


RGB OLED can display all kinds of graphics and characters. We offered lots of example sketches for you to play with it.

The hardware installation

Note: When connecting Xadow RGB OLED to Xadow Main Board, you should concern about the connection direction. The connection method is that the unfilled corner of one Xadow module need to connect to the right angle of another module(see four corners of each Xadow module).

Draw Line

Download RGB OLED Library and SGL Library, then install them to your Arduino Library. Open the DrawLine example sketch by the path: Files->Examples->RGB_OLED_96_64->examples->drawLine.

<pre>
/*
draw rectangle

This sketch is used to test Seeed's Xadow - RGB OLED,
it will draw several line with different color

create on 2014/06/24, version: 0.1
by lawliet.zou(lawliet.zou@gmail.com)
*/

#include <SGL.h>
#include <SSD1331.h>
#include <SPI.h>

#define cs A5
#define dc 3
#define mosi 16
#define sclk 15

SSD1331 oled = SSD1331(cs, dc, mosi, sclk);

void setup(){
Serial.begin(9600);
Serial.println("Start to draw");
oled.init();
oled.fillScreen(COLOR_BLACK);
delay(2000);
oled.drawLine(5,7,65,48,COLOR_BLUE);
delay(1000);
oled.drawLine(5,40,48,7,COLOR_RED);
delay(1000);
oled.drawLine(65,5,47,50,COLOR_GREEN);
delay(1000);
oled.drawLine(3,10,80,21,COLOR_YELLOW);
}

void loop(){
//nothing to do
}
</pre>

Select the correct port number and the board type should be Seeeduino Xadow, then upload the code, you can see four line with different color will be drew on the screen of RGB OLED just as follow.

Draw Circle

Open the DrawCircle example sketch by the path: Files->Examples->RGB_OLED_96_64->examples->drawCircle.


/*
draw circle

This sketch is used to test Seeed's Xadow - RGB OLED,
it will draw a circle

create on 2014/06/24, version: 0.1
by lawliet.zou(lawliet.zou@gmail.com)
*/

#include <SGL.h>
#include <SSD1331.h>
#include <SPI.h>

#define cs A5
#define dc 3
#define mosi 16
#define sclk 15

SSD1331 oled = SSD1331(cs, dc, mosi, sclk);

void setup(){
Serial.begin(9600);
Serial.println("Start to draw");
oled.init();
oled.fillScreen(COLOR_BLACK);
delay(2000);
}

void loop(){
for(int i = 30; i > 0; i--){
oled.drawCircle(48,32,i,COLOR_CYAN);
delay(50);
}
for(int i = 1; i <= 30; i++){
oled.drawCircle(48,32,i,COLOR_RED);
delay(50);
}
for(int i = 30; i > 0; i--){
oled.drawCircle(48,32,i,COLOR_PURPLE);
delay(50);
}
for(int i = 1; i <= 30; i++){
oled.drawCircle(48,32,i,COLOR_GOLDEN);
delay(50);
}
}

It is used to draw concentric circles with different color. Select the correct port number and the board type should be Seeeduino Xadow, then upload the code, you can see many circles with different colors will be drew on the screen of RGB OLED just as follow.

Draw Rectangle

Open the DrawRectangle example sketch by the path: Files->Examples->RGB_OLED_96_64->examples->drawRectangle.


/*
draw rectangle

This sketch is used to test Seeed's Xadow - RGB OLED,
it will draw a rectangle with blue color

create on 2014/06/24, version: 0.1
by lawliet.zou(lawliet.zou@gmail.com)
*/

#include <SGL.h>
#include <SSD1331.h>
#include <SPI.h>

#define cs A5
#define dc 3
#define mosi 16
#define sclk 15

SSD1331 oled = SSD1331(cs, dc, mosi, sclk);

void setup(){
Serial.begin(9600);
Serial.println("Start to draw");
oled.init();
oled.fillScreen(COLOR_BLACK);
delay(2000);
}

void loop(){
for(int i = 1; i < 16; i++){
oled.drawRectangle(3*i,2*i,95-6*i,63-4*i,COLOR_YELLOW);
delay(50);
}
delay(2000);
for(int i = 15; i > 0; i--){
oled.drawRectangle(3*i,2*i,95-6*i,63-4*i,COLOR_BLUE);
delay(50);
}
delay(2000);
}

Select the correct port number and the board type should be Seeeduino Xadow, then upload the code, you can see many rectangle will be drew on the screen of RGB OLED just as follow.

Draw Triangle

Open the DrawTriangle example sketch by the path: Files->Examples->RGB_OLED_96_64->examples->drawTriangle.


/*
draw triangle

This sketch is used to test Seeed's Xadow - RGB OLED,
it will draw a triangle

create on 2014/06/24, version: 0.1
by lawliet.zou(lawliet.zou@gmail.com)
*/

#include <SGL.h>
#include <SSD1331.h>
#include <SPI.h>

#define cs A5
#define dc 3
#define mosi 16
#define sclk 15

SSD1331 oled = SSD1331(cs, dc, mosi, sclk);

void setup(){
Serial.begin(9600);
Serial.println("Start to draw");
oled.init();
oled.fillScreen(COLOR_BLACK);
delay(2000);

}

void loop(){
//nothing to do
uint8_t x0 = random(0,96);
uint8_t y0 = random(0,64);
uint8_t x1 = random(0,96);
uint8_t y1 = random(0,64);
uint8_t x2 = random(0,96);
uint8_t y2 = random(0,64);
oled.drawTraingle(x0,y0,x1,y1,x2,y2,random(0,65536));
delay(3000);
oled.fillScreen(COLOR_BLACK);
}

Upload the code, you can see triangles with random location and shape will be drew on the screen of RGB OLED just as follow.

Draw String

Open the DrawString example sketch by the path: Files->Examples->RGB_OLED_96_64->examples->drawString.


/*
draw string

This sketch is used to test Seeed's Xadow - RGB OLED,
it will draw a string

create on 2014/06/24, version: 0.1
by lawliet.zou(lawliet.zou@gmail.com)
*/

#include <SGL.h>
#include <SSD1331.h>
#include <SPI.h>

#define cs A5
#define dc 3
#define mosi 16
#define sclk 15

SSD1331 oled = SSD1331(cs, dc, mosi, sclk);

char* str = "Seeed";

void setup(){
Serial.begin(9600);
Serial.println("Start to draw");
oled.init();
oled.fillScreen(COLOR_BLACK);
delay(2000);
oled.drawString(str,15,25,2,COLOR_GREEN);
delay(2000);
oled.setScolling(Horizontal,0,64,1);
}

void loop(){
//nothing to do
}

Upload the code, you can see the string "seeed" will be drew on the screen of RGB OLED just as follow.

Draw BitMap

Open the DrawBitMap example sketch by the path: Files->Examples->RGB_OLED_96_64->examples->drawBitMap.


/*
draw bitmap

This sketch is used to test Seeed's Xadow - RGB OLED,
it will draw a bitmap

create on 2014/06/24, version: 0.1
by lawliet.zou(lawliet.zou@gmail.com)
*/

#include <SGL.h>
#include <SSD1331.h>
#include <SPI.h>

#define cs A5
#define dc 3
#define mosi 16
#define sclk 15

SSD1331 oled = SSD1331(cs, dc, mosi, sclk);

static unsigned char SeeedLogo[] PROGMEM ={
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x80, 0x04, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x01, 0x80, 0x06, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x03, 0x80, 0x07, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x07, 0x00, 0x03, 0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x0F, 0x00, 0x03, 0xC0, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x1E, 0x00, 0x01, 0xE0,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x1E, 0x00, 0x01, 0xE0, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x3E, 0x00, 0x01, 0xF0, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x3E, 0x00, 0x01, 0xF8, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x7C, 0x00, 0x00, 0xF8,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x18, 0x00, 0x7C, 0x00, 0x00, 0xF8, 0x00, 0x60, 0x00, 0x00,
0x00, 0x00, 0x18, 0x00, 0xFC, 0x00, 0x00, 0xFC, 0x00, 0x60, 0x00, 0x00, 0x00, 0x00, 0x18, 0x00,
0xFC, 0x00, 0x00, 0xFC, 0x00, 0x60, 0x00, 0x00, 0x00, 0x00, 0x1C, 0x00, 0xFC, 0x00, 0x00, 0xFC,
0x00, 0x60, 0x00, 0x00, 0x00, 0x00, 0x1C, 0x00, 0xFC, 0x00, 0x00, 0xFC, 0x00, 0xE0, 0x00, 0x00,
0x00, 0x00, 0x1C, 0x00, 0xFC, 0x00, 0x00, 0xFC, 0x00, 0xF0, 0x00, 0x00, 0x00, 0x00, 0x1E, 0x00,
0xFC, 0x00, 0x00, 0xFC, 0x01, 0xF0, 0x00, 0x00, 0x00, 0x00, 0x1E, 0x00, 0xFC, 0x00, 0x00, 0xFC,
0x01, 0xE0, 0x00, 0x00, 0x00, 0x00, 0x1E, 0x00, 0xFC, 0x00, 0x00, 0xFC, 0x01, 0xE0, 0x00, 0x00,
0x00, 0x00, 0x1F, 0x00, 0xFC, 0x00, 0x00, 0xFC, 0x03, 0xE0, 0x00, 0x00, 0x00, 0x00, 0x1F, 0x80,
0xFC, 0x00, 0x00, 0xFC, 0x03, 0xE0, 0x00, 0x00, 0x00, 0x00, 0x1F, 0x80, 0xFE, 0x00, 0x00, 0xFC,
0x07, 0xE0, 0x00, 0x00, 0x00, 0x00, 0x0F, 0xC0, 0x7E, 0x00, 0x01, 0xFC, 0x0F, 0xE0, 0x00, 0x00,
0x00, 0x00, 0x0F, 0xC0, 0x7E, 0x00, 0x01, 0xF8, 0x0F, 0xC0, 0x00, 0x00, 0x00, 0x00, 0x0F, 0xE0,
0x7E, 0x00, 0x01, 0xF8, 0x1F, 0xC0, 0x00, 0x00, 0x00, 0x00, 0x07, 0xF0, 0x3F, 0x00, 0x01, 0xF0,
0x3F, 0x80, 0x00, 0x00, 0x00, 0x00, 0x07, 0xF0, 0x3F, 0x00, 0x03, 0xF0, 0x3F, 0x80, 0x00, 0x00,
0x00, 0x00, 0x03, 0xF8, 0x1F, 0x00, 0x03, 0xE0, 0x7F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x01, 0xFC,
0x1F, 0x80, 0x07, 0xE0, 0xFE, 0x00, 0x00, 0x00, 0x00, 0x00, 0x01, 0xFE, 0x0F, 0x80, 0x07, 0xC1,
0xFE, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0xFF, 0x07, 0xC0, 0x07, 0x83, 0xFC, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x7F, 0x83, 0xC0, 0x0F, 0x07, 0xF8, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x3F,
0xC1, 0xE0, 0x0E, 0x0F, 0xF0, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x1F, 0xF0, 0xE0, 0x1C, 0x1F,
0xE0, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x07, 0xF8, 0x70, 0x38, 0x7F, 0x80, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x03, 0xFC, 0x38, 0x30, 0xFF, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0xFF, 0x00, 0x03, 0xFC, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x3F, 0x80, 0x07, 0xF0,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x0F, 0xF0, 0x3F, 0xC0, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x01, 0xF8, 0x7E, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x08, 0x40, 0x00, 0x00, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x3C, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x3C, 0x00,
0x00, 0x03, 0xF0, 0x0F, 0xC0, 0x0F, 0xC0, 0x0F, 0x80, 0x1F, 0xBC, 0x00, 0x00, 0x0F, 0xF8, 0x3F,
0xF0, 0x3F, 0xF0, 0x3F, 0xE0, 0x7F, 0xFC, 0x00, 0x00, 0x1F, 0xFC, 0x7F, 0xF8, 0x7F, 0xF8, 0x7F,
0xF8, 0xFF, 0xFC, 0x00, 0x00, 0x1F, 0x7E, 0xFE, 0xFC, 0xFD, 0xFC, 0xFD, 0xFD, 0xFD, 0xFC, 0x00,
0x00, 0x1E, 0x1E, 0xF0, 0x3F, 0xF0, 0x3D, 0xE0, 0x3D, 0xE0, 0x7C, 0x00, 0x00, 0x1F, 0xF1, 0xFF,
0xFF, 0xFF, 0xFF, 0xFF, 0xFD, 0xE0, 0x3C, 0x00, 0x00, 0x0F, 0xFD, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF,
0xFD, 0xC0, 0x3C, 0x00, 0x00, 0x03, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFD, 0xC0, 0x3C, 0x00,
0x00, 0x3C, 0x1E, 0xF0, 0x31, 0xF0, 0x21, 0xE0, 0x21, 0xE0, 0x7C, 0x00, 0x00, 0x3F, 0x3E, 0xFE,
0xFC, 0xFC, 0xF8, 0xFD, 0xF9, 0xFD, 0xFC, 0x00, 0x00, 0x1F, 0xFE, 0x7F, 0xFC, 0x7F, 0xF8, 0x7F,
0xF8, 0xFF, 0xFC, 0x00, 0x00, 0x0F, 0xFC, 0x3F, 0xF0, 0x3F, 0xF0, 0x3F, 0xE0, 0x7F, 0xFC, 0x00,
0x00, 0x03, 0xF0, 0x0F, 0xC0, 0x0F, 0xC0, 0x0F, 0x80, 0x1F, 0xBC, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x1F, 0x64, 0xCD, 0xF6, 0xE1, 0xC9, 0x3F,
0x3F, 0xFB, 0xA6, 0x00, 0x00, 0x1F, 0xFF, 0xEF, 0xFF, 0xFF, 0xFF, 0xBF, 0xFF, 0xFF, 0xFE, 0x00,
0x00, 0x1F, 0xFF, 0xEF, 0xFF, 0xFF, 0xFF, 0xBF, 0xFF, 0xFF, 0xFC, 0x00, 0x00, 0x1F, 0xFF, 0xED,
0xFF, 0xFF, 0xFF, 0xB7, 0xFF, 0xFF, 0xFC, 0x00, 0x00, 0x00, 0xC0, 0x00, 0x20, 0x00, 0x01, 0x00,
0x00, 0x08, 0x00, 0x00, 0x00, 0x00, 0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
};

void setup(){
Serial.begin(9600);
Serial.println("Start to draw");
oled.init();
oled.fillScreen(COLOR_BLACK);
delay(2000);
oled.drawBitMap(0,0,SeeedLogo,96,64,COLOR_YELLOW);
delay(5000);
Serial.println("start to scoll ...");
oled.setScolling(Vertical,0,64,0);
}

void loop(){
//nothing to do
}

Upload the code, you can see Seeed's logo with yellow color will be drew on the screen of RGB OLED just as follow.

Schematic Online Viewer​

Resources​


Tech Support & Product Discussion​

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...