Skip to main content

Home Assistant Local Voice Control — Selection, Deployment and Measured Data

Before you use it

Voice commands in Chinese and English. The official Xiaomi Home integration for Home Assistant is licensed for non-commercial use only and is not pre-installed; do not use it in commercial projects.

What this solution does​

Bring the lights, curtains, air conditioning and Zigbee sensors in a home into Home Assistant and control them with one sentence. Say "turn on the living room light" and Home Assistant carries it out locally and answers that the light is on. Speech recognition and speech synthesis run on a local reComputer J40, so spoken audio is not uploaded to a cloud speech service. It fits living rooms and bedrooms, and smart-home integrators delivering systems in customers' homes.

  • No audio to the cloud

    Understanding the command and speaking the reply both happen on the reComputer J40; Home Assistant executes locally.

  • Text 0.12 s after speech

    Median over 5 Chinese and English commands; see "Performance and measured data".

  • Native Home Assistant integration

    The voice service joins the Home Assistant voice assistant through the Wyoming Protocol integration, with no changes to Home Assistant.

  • Zigbee devices directly

    Plug in a Connect ZBT-2 and Zigbee sensors and switches join Home Assistant without brand gateways.

On a real device​

One exchange in the Home Assistant voice assistant: the spoken "turn on the living room light" (in Chinese) is recognised by the local voice service, Home Assistant carries it out and replies that the light is on, and the living-room light card on the right turns on.

Home Assistant voice assistant: turn on the living room light, the light is on
Home Assistant dashboard: living room light, curtains, temperature, humidity, air conditioning; bedroom light and humidifier

The lights, curtains, air conditioning and sensors in the screenshots are simulated demo devices; the voice input was synthesised by the same reComputer J40, not recorded from a person.

Hardware you need​

Four things on site: the Home Assistant host, the voice host, a Zigbee coordinator and a voice terminal.

DeviceRoleNotes
ARM64 Linux host (64-bit OS, 8 GB RAM)Runs Home AssistantOne per home
reComputer Super J4012 reComputer Super J4012 (Orin NX 16GB)Local speech recognition and synthesisDownloads the voice models on first start; keep at least 30 GB of disk free
Home Assistant Connect ZBT-2Brings in Zigbee devicesPlugs into a USB port of the Home Assistant host
Home Assistant Voice Preview EditionVoice terminal in the room: listens and plays repliesOne per room
SONOFF SNZB Zigbee sensors (optional)Temperature, humidity and other statesJoin through the ZBT-2

The Home Assistant host, reComputer J40 and voice terminals share one LAN. For the Apple Home app, the iPhone must be on the same LAN as the Home Assistant host.

Deploying on site​

1. Place the devices​

Keep the voice host separate from Home Assistant

The reComputer J40 only runs the voice service, so it can sit in a cabinet or network enclosure and talk to Home Assistant over the LAN; put a voice terminal in each room where people speak.

2. Install the software: three steps​

Device-by-device steps are on the reference design page; this is the outline.


  1. Home Assistant host: deploy Home Assistant with the bundled Chinese, English and Japanese command sentences and the room/device template.
  2. Voice host: deploy the voice service on the reComputer J40; it downloads the models on first start, then recognition and synthesis run on the device.
  3. Connect and check: add the Wyoming Protocol integration in Home Assistant pointing at the two ports of the reComputer J40, select it as the assistant's speech-to-text and text-to-speech, then say "turn on the living room light" to a voice terminal and confirm the light turns on.

Interfaces​

The voice service is offered to Home Assistant over the Wyoming Protocol; all other automation stays in Home Assistant.

  • Home Assistant: add the Wyoming Protocol integration; seeed-local-voice appears as speech-to-text and text-to-speech in the voice assistant.
  • Apple Home / Siri: Home Assistant's HomeKit bridge syncs the devices to the iPhone.
  • Your own system: read and write device states through Home Assistant's own API.
PortMachineContent
HTTP 8123Home Assistant hostHome Assistant web UI and API
TCP 10300reComputer J40Speech-to-text service (Wyoming)
TCP 10200reComputer J40Text-to-speech service (Wyoming)

Performance and measured data​

End to end: speech to action​

Home Assistant ran on an ARM64 Linux host with 8 GB of RAM and the voice service on a reComputer J40 Series (Orin NX 16GB); input was synthesised speech fed to the Home Assistant voice assistant.

MetricResult
Chinese and English light commands5/5 carried out, all handled locally by Home Assistant (measured)
End of speech to recognised textmedian 0.12 s, range 0.11–0.95 s (measured)

Reproduce: sensecraft-solutions/solutions/home_assistant_whole_home (deployment package)

Voice service on its own​

Same reComputer J40 Series, voice service called directly, 16 kHz mono synthesised speech as input.

TextFirst reply audioRecognisedTranscription after end of speech
打开客厅灯 (turn on the living room light)0.122 s (measured)打开客厅灯。0.383 s (measured)
关闭卧室的灯 (turn off the bedroom light)0.049 s (measured)关闭卧室的灯。0.421 s (measured)
Turn on the living room light0.115 s (measured)Turn on the living room light.0.579 s (measured)

Through the Wyoming path, two samples were transcribed in 0.13 s (measured).

Reproduce: sensecraft-solutions/solutions/home_assistant_whole_home/assets/docker/docker-compose.jetson-voice.yml

Models and runtimes​

DeviceSpeech recognitionSpeech synthesisRuntime
reComputer J40 SeriesQwen3-ASRMatcha-TTSTensorRT-Edge-LLM / TensorRT

Settings that affect results:

  • Assistant language: Chinese or English, each with its bundled command sentences.
  • Device and room names: commands match names in Home Assistant, so "living room light" must match the entity name.

Known degradation​

  • Entity alias and phrasing divergence: Intent matching relies on entity names and aliases. If a spoken phrase diverges significantly from the configured Home Assistant entity alias, the text may be transcribed correctly without firing an automation.
  • Compound and sequential intents: The pipeline is tuned for single-intent home control; compound requests (e.g. "turn on AC and close the blinds halfway") should be issued as separate commands.
  • Multi-client voice concurrency: A single J4012 host comfortably serves 1–3 voice satellite endpoints; simultaneous long speech inputs from multiple rooms may cause a slight increase in time-to-first-token.

Data and asset sources​

  • Screenshots come from Home Assistant 2026.9.3 (Apache License 2.0, home-assistant.io) with simulated devices.
  • Voice input was generated by the same reComputer J40's speech synthesis; no human recordings or third-party audio were used.
Loading Comments...