Setting Up a Hotspot with Raspberry Pi 4G LTE Hat on Raspberry Pi OS
Introduction
This guide will walk you through the process of setting up a 4G LTE hotspot on your Raspberry Pi using the 4G LTE Hat. We'll cover the necessary hardware and software components, including the Raspberry Pi, the 4G LTE Hat, with Raspberry Pi OS (Bookworm). You'll learn how to configure the 4G module, establish a Wi-Fi network, and securely share your internet connection with other devices.
Prerequisites
Hardware Requirements
| Raspberry Pi 5 | Raspberry Pi 4G LTE CAT4 HAT |
|---|---|
![]() | ![]() |
Software Requirements
-
A Raspberry Pi with Bookworm OS installed is required.
-
A Quectel LTE 4G module configured for internet access. Ensure LTE connectivity is properly set up using RNIDS or similar configurations. Link
Steps to Enable the Hotspot
Connect to the LTE Network
Ensure your Quectel LTE module is connected and providing internet access. Confirm connectivity using:
ping -c 4 google.com
Create a Hotspot
To broadcast a hotspot network using the built-in Wi-Fi module:
- Open the terminal.
- Run the following command, replacing
hotspot nameandhotspot passwordwith your desired SSID and password:
sudo nmcli device wifi hotspot ssid <hotspot name> password <hotspot password> ifname wlan0
- ssid: Sets the name of your hotspot network.
- password: Sets the password to access the hotspot.
- ifname wlan0: Specifies the Wi-Fi interface to use.
Manage the Hotspot
Disable the Hotspot
To stop the hotspot and restore the Wi-Fi interface to client mode:
sudo nmcli device disconnect wlan0
Reconnect to Another Wi-Fi Network
To connect to a different Wi-Fi network after disabling the hotspot:
sudo nmcli device up wlan0
Additional Notes
- You can now use your Raspberry Pi as a portable router or Wi-Fi access point.
- Ensure your Raspberry Pi's power source is stable when broadcasting a hotspot for long durations.
- You can refer this document for futher
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.