Connect Wio Terminal to Google Cloud IoT Core¶
Introduction¶
In this tutorial, we will walk you through the process of connecting the Wio Terminal to Google Cloud IoT Core and send telemetry data from the Wio Terminal to the Google Cloud IoT core. This will be divided into two sections where the first section will talk about how to use the exciting libraries to send telemtry data preconfigured in the code, whereas the second section will talk about how to add your own sensors to the Wio Terminal to send the telemtry data to Google Cloud IoT Core. Google Cloud IoT Core supports both HTTP and MQTT protocols for communication, but however we will be using the MQTT protocol in this tutorial.
What is Google Cloud?¶
Google Cloud consists of a set of physical assets, such as computers and hard disk drives, and virtual resources, such as virtual machines (VMs), that are contained in Google's data centers around the globe. This distribution of resources provides several benefits, including redundancy in case of failure and reduced latency by locating resources closer to clients.
In cloud computing, what you might be used to thinking of as software and hardware products, become services. These services provide access to the underlying resources. The list of available Google Cloud services is long, and it keeps growing. When you develop your website or application on Google Cloud, you mix and match these services into combinations that provide the infrastructure you need, and then add your code to enable the scenarios you want to build.
What is Google Cloud Platform?¶
Google Cloud Platform (GCP) is a collection of cloud computing services. With a set of management tools, it provides a series of modular cloud services including computing, data storage, data analytics and machine learning. It provides infrastructure as a service, platform as a service, and serverless computing environments.
What is Google Cloud IoT Core?¶
Google Cloud Internet of Things (IoT) Core is a fully managed service for securely connecting and managing IoT devices, from a few to millions. Ingest data from connected devices and build rich applications that integrate with the other big data services of Google Cloud Platform.
What is Google Cloud Console?¶
Google Cloud Console provides a web-based, graphical user interface that you can use to manage Google Cloud Platform resources. When you use the Cloud Console, you create a new project, or choose an existing project, and use the resources that you create in the context of that project. You can create multiple projects, so you can use projects to separate your work in whatever way makes sense for you. For example, you might start a new project if you want to make sure only certain team members can access the resources in that project, while all team members can continue to access resources in another project.
Connecting Wio Terminal to Google Cloud IoT Core via MQTT¶
As explained before, we will be using the availble MQTT bridge for the communication between the Wio Terminal and the Google Cloud IoT Core. However, you may use the HTTP bridge as well, if that is your requirement.
Google Cloud Console Set Up¶
First we need to visit the Google Cloud Console, create a Cloud IoT Core device registry and register a device.
Intial Setup¶
- STEP 1: Visit here to create a new project
Note: Log in to your Google account if prompted
-
STEP 2: Click Select a project menu
-
STEP 3: Click NEW PROJECT and enter a project name
-
STEP 4: Click CREATE
-
STEP 5: Enable billing for your Cloud project. This is required to make sure you are not a robot and you will not be charged. Choose "Billing" under the navigation menu and go through the set up.
- STEP 6: Visit here to enable the Cloud IoT Core and Cloud Pub/Sub APIs
Note: Choose the project that you created before from the drop-down menu
Create a Device Registry¶
-
STEP 1: Visit Google Cloud IoT Core page in Cloud Console
-
STEP 2: Click Create Registry
-
STEP 3: Enter a registry ID
Note: This is the name of your registry
- STEP 4: Select a Region
Note: If you're in the US, select us-central1 for the Region. If you're outside the US, select your preferred region.
-
STEP 5: In the Select a Cloud Pub/Sub topic dropdown list, select Create a topic and type your preferred Topic ID
-
STEP 6: Click CREATE TOPIC
-
STEP 7: Click on SHOW ADVANCED OPTIONS
-
STEP 8: The Device state topic and Certificate value fields are optional, so leave them blank
-
STEP 9: Select MQTT for the Protocol
-
STEP 10: Click Create on the Cloud IoT Core page
Now we have created a device registry with a Cloud Pub/Sub topic for publishing device telemetry events
Generate a Device Key Pair (EC Keys)¶
Cloud IoT Core uses public key (or asymmetric) authentication
- The device uses a private key to sign a JSON Web Token (JWT). The token is passed to Cloud IoT Core as proof of the device's identity.
- The service uses the device public key (uploaded before the JWT is sent) to verify the device's identity.
Cloud IoT Core supports the RSA and Elliptic Curve algorithms, and we will be using Elliptic Curve keys in this tutorial.
-
STEP 1: Create a new folder on your PC
-
STEP 2: Navigate to the folder from a terminal window and type the following to generate a P-256 Elliptic Curve key pair
openssl ecparam -genkey -name prime256v1 -noout -out ec_private.pem
openssl ec -in ec_private.pem -pubout -out ec_public.pem
Note: Make sure to install openssl by following this link and adding the directory location to PATH.
The above commands create the following public/private key pair:
- ec_private.pem: The private key that must be securely stored on the device and used to sign the authentication JWT.
- ec_public.pem: The public key that must be stored in Cloud IoT Core and used to verify the signature of the authentication JWT.
Extract the Private Key¶
We need to extract the private key bytes and copy them into the private key string in the Arduino project that we will create later in this tutorial. Save these keys for now to use later.
-
STEP 1: Open a terminal window and navigate to the folder containing the Elliptic Curve key pair that we generated before.
-
STEP 2: Type the following command
openssl ec -in ec_private.pem -noout -text
- STEP 3: Copy and paste the generated private key bytes under priv: into a notepad and save for later use.
Add a Device to the Registry¶
-
STEP 1: Visit the Registries page and select the registry that you created before
-
STEP 2: Select the Devices tab and click CREATE A DEVICE
-
STEP 3: Enter a Device ID
-
STEP 4: The Device metadata field is optional, so leave it blank
-
STEP 5: Click on the COMMUNICATION, CLOUD LOGGING, AUTHENTICATION drop-down menu
-
STEP 6: Select Allow for Device communication
-
STEP 7: Inside the Authentication field, under Input method, select Upload
-
STEP 8: Select ES256 from the Public key format drop-down menu
-
STEP 9: Under Public key value, press the BROWSE button ,navigate to the Elliptic Curve key pair folder that we created before and select ec_public.pem
-
STEP 10: Click Create
You have now added a device to your registry. The ES256 key appears on the Device details page for your device.
Set up a Subscriber¶
Now that we have created a device registry, created a topic and added a device to that registry, let's move on to creating a subscriber to subcribe to the topic we have created, in order to grab the telemetry data from the Wio Terminal.
- STEP 1: Type Pub on the search bar of Google Cloud Console and select Pub/Sub from the results
-
STEP 2: Click Subscriptions on the navigation menu
-
STEP 3: Click CREATE SUBSCRIPTION
-
STEP 4: Enter a Subscription ID of your choice
-
STEP 5: Select the Pub/Sub topic that we previously created from the Select a Cloud Pub/Sub topic drop-down menu
-
STEP 6: Select Pull as the Delivery type
-
STEP 7: Click Create
Now we have finished setting up the Google Cloud IoT Core. Next, we will move on to setting up the Wio Terminal along with the Arduino IDE.
Arduino Set Up with Wio Terminal¶
Needed Libraries¶
We need two libraries for this tutorial. 1. lwMQTT MQTT Arduino Library 2. Google Cloud IoT Arduino Library
To download these libaries:
- STEP 1: Open Arduino IDE
- STEP 2: Navigate to
Sketch > Include Library > Manage Libraries
- STEP 3: Type lwMQTT and Google Cloud IoT in the search box and install the libraries
Credentials and Account Information Configuration¶
Now we need to set the Wi-Fi credentials and Google Cloud IoT Core information in the ciotc_config.h file.
-
STEP 1: Inside Arduino IDE,
File > Examples > Google Cloud IoT JWT > Esp32-lwmqtt
-
STEP 2: Navigate to ciotc_config.h
-
STEP 3: Change the Wifi network details
const char *ssid = "Enter_SSID";
const char *password = "Enter_Password";
- STEP 4: Change the Google Cloud IoT details
const char *project_id = "Enter_Project_ID";
const char *location = "Enter_location";
const char *registry_id = "Enter_Registry_ID";
const char *device_id = "Enter_Device_ID";
- STEP 5: Copy the private key bytes that we obtained from ec_private.pem and saved into notepad before
const char *private_key_str =
"6e:b8:17:35:c7:fc:6b:d7:a9:cb:cb:49:7f:a0:67:"
"63:38:b0:90:57:57:e0:c0:9a:e8:6f:06:0c:d9:ee:"
"31:41";
Note: The key length should be 32 pairs of hex digits
Change NTP Time Methods¶
Open esp32-mqtt.h and replace the entire file with the following codes. Here we have replaced configTime function with the implementation of obtaining NTP time via UDP.
#include <Client.h>
#include <rpcWiFi.h>
#include <WiFiClientSecure.h>
#include <MQTT.h>
#include <CloudIoTCore.h>
#include <CloudIoTCoreMqtt.h>
#include "ciotc_config.h" // Update this file with your configuration
// !!REPLACEME!!
// The MQTT callback function for commands and configuration updates
// Place your message handler code here.
void messageReceived(String &topic, String &payload){
Serial.println("incoming: " + topic + " - " + payload);
}
///////////////////////////////
// Initialize WiFi and MQTT for this board
//Client *netClient;
CloudIoTCoreDevice *device;
CloudIoTCoreMqtt *mqtt;
MQTTClient *mqttClient;
unsigned long iat = 0;
String jwt;
WiFiUDP udp;
unsigned int localPort = 2390;
unsigned long devicetime;
const int NTP_PACKET_SIZE = 48; // NTP time stamp is in the first 48 bytes of the message
byte packetBuffer[NTP_PACKET_SIZE]; //buffer to hold incoming and outgoing packets
// send an NTP request to the time server at the given address
unsigned long sendNTPpacket(const char* address) {
// set all bytes in the buffer to 0
for (int i = 0; i < NTP_PACKET_SIZE; ++i) {
packetBuffer[i] = 0;
}
// Initialize values needed to form NTP request
// (see URL above for details on the packets)
packetBuffer[0] = 0b11100011; // LI, Version, Mode
packetBuffer[1] = 0; // Stratum, or type of clock
packetBuffer[2] = 6; // Polling Interval
packetBuffer[3] = 0xEC; // Peer Clock Precision
// 8 bytes of zero for Root Delay & Root Dispersion
packetBuffer[12] = 49;
packetBuffer[13] = 0x4E;
packetBuffer[14] = 49;
packetBuffer[15] = 52;
// all NTP fields have been given values, now
// you can send a packet requesting a timestamp:
udp.beginPacket(address, 123); //NTP requests are to port 123
udp.write(packetBuffer, NTP_PACKET_SIZE);
udp.endPacket();
}
unsigned long getNTPtime() {
// module returns a unsigned long time valus as secs since Jan 1, 1970
// unix time or 0 if a problem encounted
//only send data when connected
if (WiFi.status() == WL_CONNECTED) {
//initializes the UDP state
//This initializes the transfer buffer
udp.begin(WiFi.localIP(), localPort);
sendNTPpacket(ntp_primary); // send an NTP packet to a time server
// wait to see if a reply is available
delay(1000);
if (udp.parsePacket()) {
// Serial.println("udp packet received");
// Serial.println("");
// We've received a packet, read the data from it
udp.read(packetBuffer, NTP_PACKET_SIZE); // read the packet into the buffer
//the timestamp starts at byte 40 of the received packet and is four bytes,
// or two words, long. First, extract the two words:
unsigned long highWord = word(packetBuffer[40], packetBuffer[41]);
unsigned long lowWord = word(packetBuffer[42], packetBuffer[43]);
// combine the four bytes (two words) into a long integer
// this is NTP time (seconds since Jan 1 1900):
unsigned long secsSince1900 = highWord << 16 | lowWord;
// Unix time starts on Jan 1 1970. In seconds, that's 2208988800:
const unsigned long seventyYears = 2208988800UL;
// subtract seventy years:
unsigned long epoch = secsSince1900 - seventyYears;
// adjust time for timezone offset in secs +/- from UTC
// WA time offset from UTC is +8 hours (28,800 secs)
// + East of GMT
// - West of GMT
// long tzOffset = 28800UL;
long tzOffset = 0UL;
// WA local time
unsigned long adjustedTime;
return adjustedTime = epoch + tzOffset;
}
else {
// were not able to parse the udp packet successfully
// clear down the udp connection
udp.stop();
return 0; // zero indicates a failure
}
// not calling ntp time frequently, stop releases resources
udp.stop();
}
else {
// network not connected
return 0;
}
}
///////////////////////////////
// Helpers specific to this board
///////////////////////////////
String getDefaultSensor(){
return "Wifi: " + String(WiFi.RSSI()) + "db";
}
String getJwt(){
Serial.println("Refreshing JWT");
iat = getNTPtime();
Serial.println(iat);
jwt = device->createJWT(iat, jwt_exp_secs);
Serial.println(jwt);
return jwt;
}
void setupWifi(){
Serial.println("Starting wifi");
WiFi.mode(WIFI_STA);
// WiFi.setSleep(false); // May help with disconnect? Seems to have been removed from WiFi
WiFi.begin(ssid, password);
Serial.println("Connecting to WiFi");
while (WiFi.status() != WL_CONNECTED){
delay(100);
}
// configTime(0, 0, ntp_primary, ntp_secondary);
Serial.println("Waiting on time sync...");
// Serial.println(getNTPtime());
while (getNTPtime() < 1510644967){
delay(10);
}
}
void connectWifi(){
Serial.print("checking wifi...");
while (WiFi.status() != WL_CONNECTED){
Serial.print(".");
delay(1000);
}
}
///////////////////////////////
// Orchestrates various methods from preceeding code.
///////////////////////////////
bool publishTelemetry(String data){
return mqtt->publishTelemetry(data);
}
bool publishTelemetry(const char *data, int length){
return mqtt->publishTelemetry(data, length);
}
bool publishTelemetry(String subfolder, String data){
return mqtt->publishTelemetry(subfolder, data);
}
bool publishTelemetry(String subfolder, const char *data, int length){
return mqtt->publishTelemetry(subfolder, data, length);
}
void connect(){
connectWifi();
mqtt->mqttConnect();
}
WiFiClientSecure netClient;
void setupCloudIoT(){
device = new CloudIoTCoreDevice(
project_id, location, registry_id, device_id,
private_key_str);
setupWifi();
// netClient = new WiFiClientSecure();
mqttClient = new MQTTClient(512);
mqttClient->setOptions(180, true, 1000); // keepAlive, cleanSession, timeout
mqtt = new CloudIoTCoreMqtt(mqttClient, &netClient, device);
mqtt->setUseLts(true);
mqtt->startMQTT();
}
Add Macro Definition to Esp32-lwmqtt.ino¶
Add Wio Terminal board to macro definitions inside Esp32-lwmqtt.ino
#if defined(ESP32) || defined(WIO_TERMINAL)
#define __ESP32_MQTT_H__
#endif
Now we have finished setting up Arduino IDE. Finally you need to Upload this code to Wio Terminal. Open Serial Monitor and you will see the following displayed.
Display Telemetry Data¶
Now we need to display the incoming telemetry data from the Wio Terminal. Here in this example code, the Wi-Fi signal strength will be sent as telemetry data.
- STEP 1: Visit Pub/Sub in Google Cloud Console
Note: You can search Pub in the search bar within Google Cloud Console
-
STEP 2: Navigate to Subscriptions inside Navigation Menu
-
STEP 3: Select the subscription ID that we created before
-
STEP 4: Click on VIEW MESSAGES
-
STEP 5: Click on PULL and you will see the incoming telemetry data as follows.
How to Add Other Sensors?¶
You can add any sensor to the Wio Terminal and send telemetry data to Google Cloud IoT Core. For simplicity, we will use the built-in light sensor on the Wio Terminal to send light intensity levels to Google Cloud IoT Core.
Google Cloud IoT Set Up¶
- STEP 1: Visit IoT Core in Google Cloud Console
Note: You can search IoT Core in the search bar within Google Cloud Console
-
STEP 2: Select the registry that we created before
-
STEP 3: Under Cloud Pub/Sub topics select Add or edit topics
-
STEP 4: Click ADD ADDITIONAL TOPIC
-
STEP 5: Click CREATE A TOPIC from the drop-down menu of Select a Cloud Pub/Sub topic
-
STEP 6: Enter a Topic ID and click CREATE TOPIC
-
STEP 7: Enter a Subfolder name inside the Subfolder column
Note: Subfolder name will be used to relate to the topic in the Arduino code
-
STEP 8: Click UPDATE
-
STEP 9: Create a new subscription as explained before
Arduino Set Up¶
Navigate to Esp32-lwmqtt.ino and add the following
- STEP 1: After the loop, add the following for the built-in light sensor
void loop() {
int light = analogRead(WIO_LIGHT); //assign variable to store light sensor values
light = map(light,0,1023,0,100); //Map sensor values
- STEP 2: Add the topic with the Subfolder name
publishTelemetry(getDefaultSensor());
publishTelemetry("/light",String(light));
Note: If a subfolder name is not added, telemetry data will be sent to the default topic. In this case, the telemetry data for Wi-Fi signal strength as explained before will be sent to the first topic that we crated before which is the default topic.
After you upload the code to the Wio Terminal, pull from the newly created topic as a subscriber and you will see the following result.
Tech Support¶
Please submit any technical issue into our forum