Skip to main content

YOLO11n Model Conversion for reCamera: Complete Guide

Table of Contents

  1. Introduction
  2. Understanding the Hardware Constraints
  3. Prerequisites
  4. Cloud Provider Setup Options
  5. Step-by-Step Conversion Process
  6. Common Issues and Troubleshooting
  7. Deployment to reCamera
  8. Frequently Asked Questions

Introduction

Why Model Conversion is Necessary

The reCamera series devices are edge AI cameras powered by the Sophgo CV181x chip, which uses a specialized Tensor Processing Unit (TPU) for machine learning inference. Unlike general-purpose CPUs or GPUs, TPUs require models to be in a specific format optimized for their architecture.

Key Reasons for Conversion:

  1. Hardware Optimization: The CV181x chip uses INT8 quantization instead of FP32, reducing model size by ~75% and increasing inference speed by 4-8x
  2. Memory Constraints: reCamera devices have limited RAM (256MB-512MB), requiring compressed models
  3. Power Efficiency: TPU-optimized models consume significantly less power than CPU/GPU alternatives
  4. Real-time Performance: Edge devices need sub-100ms inference times for practical applications

About reCamera Hardware

The reCamera family includes several variants, all built around the Sophgo CV181x SoC:

  • reCamera Default: Basic model with 2MP sensor, USB-C connectivity
  • reCamera Microscope: Specialized for close-up imaging with interchangeable lenses
  • reCamera HD POE: Higher resolution with Power-over-Ethernet support
  • reCamera Gimbal: Motorized gimbal with object tracking capabilities

Technical Specifications:

  • Processor: Sophgo CV181x (RISC-V + TPU)
  • AI Performance: 0.5 TOPS INT8
  • Memory: 256MB DDR3
  • Storage: 16MB SPI Flash + microSD
  • Supported Formats: CVI models (Sophgo's proprietary format)

The Conversion Challenge

YOLO11n models are typically trained in PyTorch and exported to ONNX format. However, the reCamera's CV181x chip cannot directly run ONNX models. The conversion process involves:

  1. Model Architecture Translation: Converting ONNX to MLIR (Multi-Level Intermediate Representation)
  2. Quantization: Converting FP32 weights to INT8 while maintaining accuracy
  3. Hardware Optimization: Adapting layer operations for TPU acceleration
  4. Format Conversion: Creating the final CVI model format

Understanding the Hardware Constraints

Memory Limitations

  • Model Size Limit: Typically 8-16MB for practical deployment
  • Input Resolution: Usually 640x640 for YOLO11n to balance accuracy and performance
  • Batch Size: Limited to 1 due to memory constraints

Processing Constraints

  • Supported Operations: Not all ONNX operations have TPU equivalents
  • Precision Loss: INT8 quantization may reduce accuracy by 1-3%
  • Inference Speed: Target is 10-30 FPS depending on model complexity

Why Standard ML Frameworks Don't Work

  • TensorFlow/PyTorch: Designed for x86/ARM CPUs and NVIDIA GPUs
  • ONNX Runtime: Lacks CV181x backend support
  • TensorRT: NVIDIA-specific, incompatible with Sophgo hardware

Prerequisites

Required Knowledge

  • Basic Linux command line operations
  • Understanding of Docker containers
  • Familiarity with YOLO model architecture
  • Basic networking concepts for cloud deployment

Required Software

  • Docker Desktop (for local development)
  • SSH client (Terminal on macOS, PuTTY on Windows)
  • Web browser for cloud provider management
  • Text editor for configuration files

Required Files

  • Trained YOLO11n model in ONNX format
  • 100 calibration images (representative of your dataset)
  • 1 test image for validation

Cloud Provider Setup Options

Since the conversion process requires Linux and specific toolchains, cloud providers offer the most reliable environment. Here are setup guides for major providers:

Advantages: Simple interface, predictable pricing, good documentation

Setup Steps:

  1. Create DigitalOcean account at digitalocean.com

  2. Create new Droplet with these specifications:

    • Image: Ubuntu 22.04 LTS
    • Plan: Basic, 4GB RAM, 2 vCPUs ($24/month, can delete after use)
    • Region: Choose closest to your location
    • Authentication: SSH Key (recommended) or Password
  3. SSH Connection:

    ssh root@your_droplet_ip
  4. Install Dependencies:

    apt update && apt upgrade -y
    apt install -y docker.io git wget
    systemctl start docker
    systemctl enable docker

Estimated Cost: $0.50-2.00 for conversion process (if deleted immediately after)

Option 2: AWS EC2

Advantages: Most comprehensive cloud platform, free tier available

Setup Steps:

  1. Create AWS account at aws.amazon.com

  2. Launch EC2 instance:

    • AMI: Ubuntu Server 22.04 LTS
    • Instance Type: t3.medium (2 vCPU, 4GB RAM)
    • Security Group: Allow SSH (port 22) from your IP
  3. SSH Connection:

    ssh -i your-key.pem ubuntu@your-instance-ip
  4. Install Dependencies:

    sudo apt update && sudo apt upgrade -y
    sudo apt install -y docker.io git wget
    sudo systemctl start docker
    sudo systemctl enable docker
    sudo usermod -aG docker ubuntu

Estimated Cost: $0.10-0.50 for conversion process (t3.medium pricing)

Option 3: Google Cloud Platform

Advantages: $300 free credits for new users, excellent performance

Setup Steps:

  1. Create GCP account at cloud.google.com

  2. Create Compute Engine instance:

    • Machine Type: e2-standard-2 (2 vCPU, 8GB RAM)
    • Boot Disk: Ubuntu 22.04 LTS, 20GB
    • Firewall: Allow HTTP/HTTPS traffic
  3. SSH via Browser (built-in terminal) or use gcloud CLI

  4. Install Dependencies:

    sudo apt update && sudo apt upgrade -y
    sudo apt install -y docker.io git wget
    sudo systemctl start docker
    sudo systemctl enable docker
    sudo usermod -aG docker $USER

Estimated Cost: Free with credits, otherwise ~$0.20-0.60 for conversion

Option 4: Microsoft Azure

Advantages: Good integration with Windows ecosystem, student discounts

Setup Steps:

  1. Create Azure account at azure.microsoft.com

  2. Create Virtual Machine:

    • Image: Ubuntu Server 22.04 LTS
    • Size: Standard_B2s (2 vCPUs, 4GB RAM)
    • Authentication: SSH public key
  3. SSH Connection:

    ssh azureuser@your-vm-ip
  4. Install Dependencies:

    sudo apt update && sudo apt upgrade -y
    sudo apt install -y docker.io git wget
    sudo systemctl start docker
    sudo systemctl enable docker
    sudo usermod -aG docker azureuser

Estimated Cost: ~$0.30-0.80 for conversion process

Option 5: Alibaba Cloud

Advantages: Strong presence in Asia, competitive pricing

Setup Steps:

  1. Create account at alibabacloud.com

  2. Create ECS instance:

    • Image: Ubuntu 22.04 64-bit
    • Instance Type: ecs.t6-c1m2.large (2 vCPU, 4GB RAM)
    • Security Group: Allow SSH (22/22)
  3. SSH Connection:

    ssh root@your-ecs-ip
  4. Install Dependencies:

    apt update && apt upgrade -y
    apt install -y docker.io git wget
    systemctl start docker
    systemctl enable docker

Estimated Cost: ~$0.20-0.50 for conversion process

Option 6: Tencent Cloud

Advantages: Good for users in China, affordable pricing

Setup Steps:

  1. Create account at intl.cloud.tencent.com

  2. Create CVM instance:

    • Image: Ubuntu Server 22.04 LTS 64-bit
    • Model: S5.MEDIUM4 (2 vCPU, 4GB RAM)
    • Security Group: Allow SSH (port 22)
  3. SSH Connection:

    ssh ubuntu@your-cvm-ip
  4. Install Dependencies:

    sudo apt update && sudo apt upgrade -y
    sudo apt install -y docker.io git wget
    sudo systemctl start docker
    sudo systemctl enable docker
    sudo usermod -aG docker ubuntu

Estimated Cost: ~$0.15-0.40 for conversion process

Step-by-Step Conversion Process

Step 1: Prepare Your Environment

  1. Connect to your cloud instance via SSH

  2. Set up TPU-MLIR environment:

    # Pull the official TPU-MLIR Docker image
    docker pull sophgo/tpuc_dev:v3.1

    # Create working directory
    mkdir ~/yolo_conversion && cd ~/yolo_conversion

    # Start Docker container
    docker run --privileged --name tpu_converter -v $PWD:/workspace -it sophgo/tpuc_dev:v3.1
  3. Install TPU-MLIR tools inside container:

    pip install tpu_mlir[all]==1.7

    # Clone and build TPU-MLIR
    git clone -b v1.7 --depth 1 https://github.com/sophgo/tpu-mlir.git
    cd tpu-mlir
    source ./envsetup.sh
    ./build.sh

Step 2: Upload Your Model Files

From your local machine, upload files to cloud instance:

# Upload ONNX model
scp your_model.onnx user@your-cloud-ip:~/yolo_conversion/

# Upload calibration images (create zip first)
zip -r calibration_images.zip /path/to/calibration/images/
scp calibration_images.zip user@your-cloud-ip:~/yolo_conversion/

# Upload test image
scp test_image.jpg user@your-cloud-ip:~/yolo_conversion/

Step 3: Prepare Directory Structure

Inside your cloud instance:

# Create required directory structure
mkdir -p model_yolo11n/{COCO2017,image,Workspace}

# Extract and organize files
unzip calibration_images.zip
mv calibration_images/* model_yolo11n/COCO2017/
mv test_image.jpg model_yolo11n/image/test.jpg
mv your_model.onnx model_yolo11n/Workspace/yolo11n.onnx

# Rename calibration images to expected format
cd model_yolo11n/COCO2017/
count=1
for file in *.jpg *.png *.jpeg; do
if [ -f "$file" ]; then
mv "$file" "Calibration${count}.jpg"
((count++))
if [ $count -gt 100 ]; then break; fi
fi
done
cd ../..

Step 4: Enter Docker Container and Begin Conversion

# Copy model folder into Docker container
docker cp model_yolo11n tpu_converter:/workspace/tpu-mlir/

# Enter Docker container
docker exec -it tpu_converter /bin/bash

# Navigate to workspace
cd /workspace/tpu-mlir/model_yolo11n/Workspace

Step 5: Model Conversion Pipeline

5.1: ONNX Version Downgrade

python /workspace/tpu-mlir/downgrade_onnx.py yolo11n.onnx yolo11n_v8.onnx

5.2: Convert ONNX to MLIR

model_transform \
--model_name yolo11n \
--model_def yolo11n_v8.onnx \
--input_shapes "[[1,3,640,640]]" \
--mean "0.0,0.0,0.0" \
--scale "0.0039216,0.0039216,0.0039216" \
--keep_aspect_ratio \
--pixel_format rgb \
--output_names "/model.23/cv2.0/cv2.0.2/Conv_output_0,/model.23/cv3.0/cv3.0.2/Conv_output_0,/model.23/cv2.1/cv2.1.2/Conv_output_0,/model.23/cv3.1/cv3.1.2/Conv_output_0,/model.23/cv2.2/cv2.2.2/Conv_output_0,/model.23/cv3.2/cv3.2.2/Conv_output_0" \
--test_input ../image/test.jpg \
--test_result yolo11n_top_outputs.npz \
--mlir yolo11n.mlir

Parameter Explanations:

  • --model_name: Identifier for your model in the conversion pipeline

    • Purpose: Creates consistent naming throughout the process
    • Can be changed: Yes, use descriptive names like "traffic_detection" or "person_counter"
    • Effect: Only affects internal naming, no impact on performance
  • --model_def: Path to your ONNX model file

    • Purpose: Specifies which model to convert
    • Can be changed: Yes, must match your actual ONNX file name
    • Effect: Different models will produce different results
  • --input_shapes: Defines input tensor dimensions [batch, channels, height, width]

    • Purpose: Tells the converter the expected input image format
    • Standard value: [[1,3,640,640]] for YOLO11n
    • Can be changed: ⚠️ Caution - Must match your training resolution
    • Effects of changes:
      • Smaller (e.g., 320x320): Faster inference, lower accuracy
      • Larger (e.g., 1280x1280): Higher accuracy, much slower, may exceed memory limits
      • Different aspect ratio: Will distort images, poor results
  • --mean: Pixel normalization mean values for RGB channels

    • Purpose: Centers pixel values around zero (standard preprocessing)
    • Standard value: "0.0,0.0,0.0" (no mean subtraction)
    • Can be changed: Only if your model was trained with different normalization
    • Common alternatives:
      • ImageNet: "123.675,116.28,103.53" (if model uses ImageNet preprocessing)
      • Custom: Match your training preprocessing exactly
  • --scale: Pixel normalization scale factors

    • Purpose: Scales pixel values from 0-255 range to 0-1 range
    • Standard value: "0.0039216,0.0039216,0.0039216" (equivalent to 1/255)
    • Can be changed: Only if your model expects different input range
    • Effects of changes:
      • Wrong scale values will cause complete model failure
      • Must match exactly what your model was trained with
  • --keep_aspect_ratio: Maintains image proportions during resize

    • Purpose: Prevents image distortion by padding instead of stretching
    • Can be changed: Yes, use --no_keep_aspect_ratio to disable
    • Effects:
      • Enabled (default): Better accuracy, black padding on images
      • Disabled: Slightly faster, but images may be distorted
  • --pixel_format: Color channel ordering

    • Purpose: Specifies whether input uses RGB or BGR color order
    • Standard value: rgb for most modern models
    • Can be changed: Yes, to bgr if your model expects it
    • Effects of wrong setting: Colors will be swapped (red appears blue, etc.)
  • --output_names: Specifies which model layers to use as outputs

    • Purpose: Tells converter which layers contain detection results
    • Standard for YOLO11n: The 6 output layers shown (3 scales × 2 heads each)
    • Can be changed: ⚠️ Advanced users only - requires deep model knowledge
    • Effects: Wrong outputs will prevent detection from working
  • --test_input: Path to validation image

    • Purpose: Tests conversion accuracy by comparing before/after results
    • Can be changed: Yes, use any representative image from your dataset
    • Recommended: Use image similar to your deployment scenario
  • --test_result: Output file for validation data

    • Purpose: Stores reference results for later comparison
    • Can be changed: Yes, any filename ending in .npz
    • Effect: Only affects file naming
  • --mlir: Output MLIR file name

    • Purpose: Intermediate representation for next conversion step
    • Can be changed: Yes, but keep .mlir extension
    • Effect: Only affects file naming

5.3: Generate Calibration Table

run_calibration \
yolo11n.mlir \
--dataset ../COCO2017 \
--input_num 100 \
-o yolo11n_calib_table

Parameter Explanations:

  • yolo11n.mlir: Input MLIR model from previous step

    • Purpose: The model file that needs calibration data
    • Can be changed: Must match the output filename from step 5.2
    • Effect: Different models will produce different calibration tables
  • --dataset: Path to calibration images directory

    • Purpose: Provides representative images for analyzing activation ranges
    • Can be changed: Yes, but must contain images similar to deployment scenario
    • Requirements: Images should be .jpg, .png, or .bmp format
    • Quality impact: More diverse, representative images = better calibration
  • --input_num: Number of calibration images to use

    • Purpose: Determines how many images are processed for statistical analysis
    • Standard value: 100 (good balance of accuracy vs. processing time)
    • Can be changed: Yes, within practical limits
    • Effects of changes:
      • Fewer images (25-50): Faster calibration, potentially less accurate quantization
      • More images (200-500): Better calibration accuracy, much longer processing time
      • Too few (<10): Poor quantization, significant accuracy loss
      • Too many (>1000): Diminishing returns, very long processing time
  • -o (output file): Name for the calibration table file

    • Purpose: Stores statistical data about layer activations for quantization
    • Can be changed: Yes, any filename (no extension needed)
    • Effect: Only affects filename, content is the same

What Happens During Calibration:

  1. Statistical Analysis: Each calibration image is processed through the model
  2. Activation Mapping: The tool records the range of values each layer produces
  3. Quantization Planning: Determines how to map FP32 values to INT8 efficiently
  4. Accuracy Preservation: Finds optimal scaling factors to minimize precision loss

Expected Output: This process will take 5-15 minutes and should show progress like:

input_num = 100, ref = 100
real input_num = 100
activation_collect_and_calc_th for op: /model.23/cv3.2/cv3.2.2/Conv_output_0_Conv
[Progress bar showing completion]
auto tune end, run time: XXX seconds

5.4: Compile Final INT8 Model

model_deploy \
--mlir yolo11n.mlir \
--quantize INT8 \
--quant_input \
--processor cv181x \
--calibration_table yolo11n_calib_table \
--test_input ../image/test.jpg \
--test_reference yolo11n_top_outputs.npz \
--customization_format RGB_PACKED \
--fuse_preprocess \
--aligned_input \
--model yolo11n_sym_int8.cvimodel

Parameter Explanations:

  • --mlir: Input MLIR model file

    • Purpose: The model representation to be compiled for TPU
    • Can be changed: Must match output from step 5.2
    • Effect: Different MLIR files will produce different final models
  • --quantize: Quantization precision level

    • Purpose: Determines numerical precision for model weights and activations
    • Standard value: INT8 for reCamera (required for CV181x TPU)
    • Can be changed: Limited options on CV181x
    • Available options:
      • INT8: Required for reCamera, 4x smaller, 4-8x faster
      • F16: Higher precision, larger size, may not fit in memory
      • F32: Original precision, too large for reCamera deployment
  • --quant_input: Quantizes input preprocessing

    • Purpose: Moves input scaling/normalization to TPU for efficiency
    • Can be changed: Yes, omit this flag to keep input processing on CPU
    • Effects:
      • Enabled (recommended): Faster inference, better TPU utilization
      • Disabled: Slightly slower, but more flexible input formats
  • --processor: Target hardware specification

    • Purpose: Optimizes code generation for specific chip architecture
    • Standard value: cv181x for all reCamera models
    • Can be changed: ⚠️ Never change - other values won't work on reCamera
    • Effect: Wrong processor setting will cause deployment failure
  • --calibration_table: Quantization reference data

    • Purpose: Provides statistical data for optimal INT8 conversion
    • Can be changed: Must match output filename from step 5.3
    • Effect: Different calibration data affects model accuracy
  • --test_input: Validation image for accuracy testing

    • Purpose: Verifies model accuracy after quantization
    • Can be changed: Yes, should represent typical use case
    • Recommendation: Use same image as in step 5.2 for consistency
  • --test_reference: Reference output for comparison

    • Purpose: Compares quantized model output to original FP32 results
    • Can be changed: Must match output filename from step 5.2
    • Effect: Used only for validation, doesn't affect final model
  • --customization_format: Input data layout optimization

    • Purpose: Optimizes memory layout for TPU processing
    • Standard value: RGB_PACKED for image data
    • Can be changed: Advanced users only
    • Effects:
      • RGB_PACKED: Optimized for RGB images (recommended)
      • NCHW: Standard tensor format, may be slower
  • --fuse_preprocess: Integrates preprocessing into model

    • Purpose: Combines image resizing/normalization with inference
    • Can be changed: Yes, omit flag to handle preprocessing separately
    • Effects:
      • Enabled (recommended): Single-step deployment, better performance
      • Disabled: More flexibility, but requires external preprocessing
  • --aligned_input: Memory alignment optimization

    • Purpose: Ensures optimal memory access patterns for TPU
    • Can be changed: Yes, but recommended to keep for performance
    • Effects:
      • Enabled: Better memory bandwidth utilization
      • Disabled: May be slightly slower
  • --model: Output filename for final converted model

    • Purpose: Creates the .cvimodel file for reCamera deployment
    • Can be changed: Yes, use descriptive names like person_detection.cvimodel
    • Requirement: Must end with .cvimodel extension
    • Effect: Only affects filename

What Happens During Compilation:

  1. Layer Conversion: Each neural network layer is converted to TPU instructions
  2. Memory Optimization: Model weights are arranged for efficient TPU access
  3. Quantization Application: FP32 weights are converted to INT8 using calibration data
  4. Hardware Mapping: Operations are mapped to specific TPU functional units
  5. Validation: Final model is tested against reference outputs

Expected Output: The conversion should complete with validation results showing similarity scores >99%:

npz compare PASSED
230 compared
230 passed
min_similarity = (0.9999997615814209, 0.9999984392787142, 116.13544464111328)

Performance Expectations After Conversion:

  • Model Size: 3-8MB (compared to 20-40MB original ONNX)
  • Inference Speed: 15-30 FPS on reCamera
  • Accuracy: 97-99% of original model performance
  • Memory Usage: ~10-20MB RAM during inference

Step 6: Download Converted Model

6.1: Exit Docker and copy file to host

# Exit Docker container
exit

# Copy converted model from container to host
docker cp tpu_converter:/workspace/tpu-mlir/model_yolo11n/Workspace/yolo11n_sym_int8.cvimodel ./

# Verify file exists and check size (should be 2-10MB)
ls -lh yolo11n_sym_int8.cvimodel

6.2: Download to your local machine

# From your local machine
scp user@your-cloud-ip:~/yolo_conversion/yolo11n_sym_int8.cvimodel ~/Downloads/

Step 7: Clean Up Cloud Resources

Don't forget to terminate your cloud instance to avoid ongoing charges!

  • DigitalOcean: Destroy Droplet from control panel
  • AWS: Terminate EC2 instance
  • GCP: Delete Compute Engine instance
  • Azure: Delete Virtual Machine
  • Alibaba/Tencent: Release ECS/CVM instance

Common Issues and Troubleshooting

Issue 1: "File not found" errors during conversion

Symptoms:

../image/test.jpg doesn't existed !!!

Solution:

# Check if file exists and has correct extension
ls -la ../image/
# If file has .img extension, rename it
mv ../image/test.img ../image/test.jpg

Issue 2: "Directory not empty" when moving files

Symptoms:

mv: cannot move 'Download/model_yolo11n' to 'tpu-mlir/model_yolo11n': Directory not empty

Solution:

# Remove existing directory and replace
rm -rf tpu-mlir/model_yolo11n
mv Download/model_yolo11n tpu-mlir/

Issue 3: Calibration fails with "There is no inputs"

Symptoms:

RuntimeError: There is no inputs

Solution:

# Ensure calibration images are in correct format (.jpg, .png)
cd ../COCO2017/
for file in *.img; do
mv "$file" "${file%.img}.jpg"
done

Issue 4: Docker permission errors

Symptoms:

permission denied while trying to connect to the Docker daemon socket

Solution:

# Add user to docker group
sudo usermod -aG docker $USER
# Log out and log back in, or run:
newgrp docker

Issue 5: Out of memory errors

Symptoms:

CUDA out of memory

Solution:

  • Upgrade to larger cloud instance (8GB+ RAM)
  • Reduce batch size in conversion commands
  • Use fewer calibration images (minimum 50)

Issue 6: Model validation fails

Symptoms:

npz compare FAILED

Solution:

  • Check if test image is representative of training data
  • Verify ONNX model is correct version
  • Try different test image

Issue 7: SSH connection issues

Symptoms:

Connection refused
ssh: connect to host [IP] port 22: Connection refused

Solution:

  • Check cloud provider security groups allow SSH (port 22)
  • Verify instance is running
  • Try different SSH key or password authentication

Deployment to reCamera

Step 1: Connect reCamera

  1. Connect reCamera to your computer via USB-C cable
  2. Access web interface at http://192.168.42.1
  3. Login with username: root, password: recamera.1

Step 2: Upload Model

  1. Navigate to Workspace section
  2. Click on model node in the flow editor
  3. Click "Upload" button
  4. Select your .cvimodel file
  5. Configure model parameters:
    • Model Name: yolo11n_detection
    • Classes: Enter your class names (comma-separated)
    • Confidence Threshold: 0.5 (adjust as needed)
    • IoU Threshold: 0.45

Step 3: Deploy and Test

  1. Click "Deploy" button
  2. Wait for "Successfully deployed" message
  3. Navigate to Dashboard for live preview
  4. Adjust confidence/IoU thresholds as needed

Frequently Asked Questions

Q: How long does the conversion process take?

A: Typically 20-45 minutes depending on model complexity and cloud instance performance. The calibration step is usually the longest.

Q: Can I use a different YOLO version?

A: This guide is specific to YOLO11n. Other versions (YOLOv8, YOLOv9) require different output layer names and may have compatibility issues.

Q: What if my model accuracy drops significantly after conversion?

A: Some accuracy loss (1-3%) is normal due to INT8 quantization. If loss is >5%, try:

  • Using more representative calibration images
  • Increasing calibration image count to 200-500
  • Adjusting confidence thresholds during deployment

Q: Can I convert models trained on custom datasets?

A: Yes, but ensure your calibration images are representative of your custom dataset. The 100 calibration images should cover the variety of scenarios your model will encounter.

Q: What's the maximum model size supported?

A: The reCamera's memory limits practical model size to ~8-16MB. YOLO11n typically produces 3-8MB models after conversion.

Q: Do I need to keep the cloud instance running?

A: No, you can terminate the instance immediately after downloading your converted model. The conversion is a one-time process.

Q: Can I batch convert multiple models?

A: Yes, you can keep the same environment and convert multiple models by repeating steps 5-6 with different model files.

Q: What if I encounter an error not covered here?

A:

  1. Check the Docker container logs: docker logs tpu_converter
  2. Verify your ONNX model loads correctly in a Python environment first
  3. Try with a simpler test model to isolate the issue
  4. Contact Seeed Studio support with specific error messages

Q: Are there alternatives to cloud deployment?

A: Yes, you can:

  • Use Docker Desktop locally on Mac/Windows (requires significant RAM)
  • Set up WSL2 on Windows with Docker
  • Use a local Linux machine or VM

However, cloud deployment is recommended for reliability and performance.


Conclusion

Converting YOLO11n models for reCamera deployment requires understanding both the hardware constraints and the TPU-MLIR toolchain. While the process has several steps, following this guide should result in a successfully converted model ready for edge AI deployment.

The key to success is:

  1. Preparation: Having all files in the correct format and structure
  2. Environment: Using a properly configured Linux environment (cloud recommended)
  3. Patience: Allowing sufficient time for the calibration and conversion steps
  4. Validation: Testing your converted model thoroughly before deployment

For additional support, consult the SeeedStudio ReCamera wiki or the TPU-MLIR documentation.

Loading Comments...