Grove - 8 Channel I2C Multiplexer/I2C Hub (TCA9548A)

We've already released the Grove - I2C Hub (4 Port) and the Grove - I2C Hub (6 Port). Wait, still not enough? Well well, we know you are seeking more. Here you are, we present you the Grove - 8 Channel I2C Hub.
More importantly, this is more than just a superposition of port quantities. As we all know, I2C devices must use different addresses in the same bus system, even use the Grove I2C Hub (4 or 6 port), the rule is still the rule. However, with the help of Grove - 8 Channel I2C Hub, you can plug up to 8 same-address I2C devices to the same Grove I2C system. All thanks to the TCA9548A I2C Multiplexer Chip. It adopts time-division multiplexing technology so that the same controller can control 8 I2C devices with the same address. No more worrying about address conflicts.
Features
- 8 Grove I2C Port
- Support multiple devices with the same I2C address
- Support 3.3V/5V System
Platform Supported
| Arduino | Raspberry Pi | |||
|---|---|---|---|---|
![]() | ![]() | ![]() | ![]() | ![]() |
Getting Started
Read the I2C address of devices connecting on the Grove - 8 Channel I2C Hub
Materials Required
| Seeeduino XIAO | Grove Breadboard | Grove - 8 Channel I2C Multiplexer/I2C Hub (TCA9548A) |
|---|---|---|
| Get one now | Get one now | Get one now |
We also require up to 8 I2C devices, please click here to find the Grove I2C devices you like. At these example, we use three I2C devices.
Hardware connection

Connect the I2C Hub with Seeeduino XIAO's I2C interface, and connect each I2C device with each hub.
Software code
#include "TCA9548A.h"
// if you use the software I2C to drive, you can uncommnet the define SOFTWAREWIRE which in TCA9548A.h.
#ifdef SOFTWAREWIRE
#include <SoftwareWIRE.h>
SoftwareWire myWIRE(3, 2);
TCA9548A<SoftwareWire> TCA;
#define WIRE myWIRE
#else
#include <Wire.h>
TCA9548A<TwoWire> TCA;
#define WIRE Wire
#endif
#define SERIAL Serial
void setup()
{
SERIAL.begin(115200);
while(!SERIAL){};
//WIRE.begin();
TCA.begin(WIRE);
//defaut all channel was closed
//TCA.openAll();
//TCA.closeAll();
// Select the channels you want to open. You can open as many channels as you want
TCA.openChannel(TCA_CHANNEL_0); //TCA.closeChannel(TCA_CHANNEL_0);
TCA.openChannel(TCA_CHANNEL_1); //TCA.closeChannel(TCA_CHANNEL_1);
TCA.openChannel(TCA_CHANNEL_2); //TCA.closeChannel(TCA_CHANNEL_2);
TCA.openChannel(TCA_CHANNEL_3); //TCA.closeChannel(TCA_CHANNEL_3);
TCA.openChannel(TCA_CHANNEL_4); //TCA.closeChannel(TCA_CHANNEL_4);
TCA.openChannel(TCA_CHANNEL_5); //TCA.closeChannel(TCA_CHANNEL_5);
TCA.openChannel(TCA_CHANNEL_6); //TCA.closeChannel(TCA_CHANNEL_6);
TCA.openChannel(TCA_CHANNEL_7); //TCA.closeChannel(TCA_CHANNEL_7);
}
void loop()
{
uint8_t error, i2cAddress, devCount, unCount;
SERIAL.println("Scanning...");
devCount = 0;
unCount = 0;
for(i2cAddress = 1; i2cAddress < 127; i2cAddress++ )
{
WIRE.beginTransmission(i2cAddress);
error = WIRE.endTransmission();
if (error == 0)
{
SERIAL.print("I2C device found at 0x");
if (i2cAddress<16) SERIAL.print("0");
SERIAL.println(i2cAddress,HEX);
devCount++;
}
else if (error==4)
{
SERIAL.print("Unknow error at 0x");
if (i2cAddress<16) SERIAL.print("0");
SERIAL.println(i2cAddress,HEX);
unCount++;
}
}
if (devCount + unCount == 0)
SERIAL.println("No I2C devices found\n");
else {
SERIAL.print(devCount);
SERIAL.print(" device(s) found");
if (unCount > 0) {
SERIAL.print(", and unknown error in ");
SERIAL.print(unCount);
SERIAL.print(" address");
}
SERIAL.println();
}
SERIAL.println();
delay(1000);
}
-
Step 1 Download the library from the resource and add the "zip" library to your Arduino IDE. Please refer to How to install an Arduino Library.
-
Step 2 Find the example code and upload it to your board. Please refer to How to upload code.
-
Step 3 After uploading the code, you will see the I2C adress of each device from the serial monitor. The adress 0x70 is the I2C adress of I2C Hub.

Schematic Online Viewer
Resource
- [PDF] TCA9548A_DATASHEET
- [PDF] Hardware schematic
- [ZiP] Grove 8 Channel I2C Hub Library
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.