edit

Grove - I2C High Accuracy Temp&Humi Sensor(SHT35)

Grove - I2C High Accuracy Temp&Humi Sensor(SHT35) is based on SHT3x-DIS, which is the next generation of Sensirion’s temperature and humidity sensors. It builds on a new CMOSens® sensor chip that is at the heart of Sensirion’s new humidity and temperature platform. The SHT3x-DIS has increased intelligence, reliability and improved accuracy specifications compared to its predecessor. Its functionality includes enhanced signal processing, two distinctive and user selectable I2C addresses and communication speeds of up to 1 MHz.

Features

  • High accuracy of ±1.5 %RH and ±0.1 °C
  • Fully calibrated, linearized, and temperature compensated digital output
  • I2C Interface with communication speeds up to 1MHz and two user selectable addresses
  • Very fast start-up and measurement time

Specification

Item Value
Operating Voltage 3.3V / 5V
Specified Temperature Range -40°C to +125°C
Temperature Resolution 0.01°C
Temperature Accuracy Tolerance ±0.1 °C
Specified Humidity Range 0%RH to +100%RH
Humidity Resolution 0.01%RH
Humidity Accuracy Tolerance ±1.5 %RH
Interface I2C
I2C Address 0x45(default) / 0x44(optional)

Applications

  • Industrial Freezers and Refrigerators
  • Food Processing
  • Personal Computers and Servers
  • PC Peripherals
  • Consumer Electronics
  • Handheld/Portable Devices

Hardware Overview

Pin Out

Schemaitc

Power

This module is based on SHT35, the input voltage of this chip range from 2.15v-5.5v, so you can use both 3.3v and 5v pin of Arduino to supply for this module.

Platforms Supported

Arduino Raspberry Pi

Caution

The platforms mentioned above as supported is/are an indication of the module's software or theoritical compatibility. We only provide software library or code examples for Arduino platform in most cases. It is not possible to provide software library / demo code for all possible MCU platforms. Hence, users have to write their own software library.

Getting Started

Play With Arduino

Hardware

Materials required

Seeeduino V4.2 Base Shield Grove-SHT35 Sensor
enter image description here enter image description here enter image description here
Get One Now Get One Now Get One Now

Note

1 Please plug the USB cable gently, otherwise you may damage the port. Please use the USB cable with 4 wires inside, the 2 wires cable can't transfer data. If you are not sure about the wire you have, you can click here to buy

2 Each Grove module comes with a Grove cable when you buy. In case you lose the Grove cable, you can click here to buy.

  • Step 1. Connect the Grove - I2C High Accuracy Temp&Humi Sensor(SHT35) to port I2C of Grove-Base Shield.

  • Step 2. Plug Grove - Base Shield into Seeeduino.

  • Step 3. Connect Seeeduino to PC via a USB cable.

Note

If we don't have Grove Base Shield, We also can directly connect this module to Seeeduino as below.

Seeeduino Grove Cable Grove - I2C High Accuracy Temp&Humi Sensor(SHT35)
GND Black GND
5V or 3.3V Red VCC
SDA White SDA
SCL Yellow SCL

Software

Attention

If this is the first time you work with Arduino, we strongly recommend you to see Getting Started with Arduino before the start.

  • Step 1. Download the Grove-SHT35 Sensor Library from Github.

  • Step 2. Refer to How to install library to install library for Arduino.

  • Step 3. Restart the Arduino IDE. Open the example, you can open it in the following three ways:

    1. Open it directly in the Arduino IDE via the path: File → Examples → Grove Temperature sensor SHT35 → basic_demo.

    2. Open it in your computer by click the basic_demo.ino which you can find in the folder XXXX\Arduino\libraries\Seeed_SHT35-master\examples\basic_demo, XXXX is the location you installed the Arduino IDE.

    3. Or, you can just click the icon in upper right corner of the code block to copy the following code into a new sketch in the Arduino IDE.

#include "Seeed_SHT35.h"


/*SAMD core*/
#ifdef ARDUINO_SAMD_VARIANT_COMPLIANCE
  #define SDAPIN  20
  #define SCLPIN  21
  #define RSTPIN  7
  #define SERIAL SerialUSB
#else
  #define SDAPIN  A4
  #define SCLPIN  A5
  #define RSTPIN  2
  #define SERIAL Serial
#endif

SHT35 sensor(SCLPIN);


void setup()
{
    SERIAL.begin(115200);
    delay(10);
    SERIAL.println("serial start!!");
    if(sensor.init())
    {
      SERIAL.println("sensor init failed!!!");
    }
    delay(1000);
}


void loop()
{
     u16 value=0;
    u8 data[6]={0};
    float temp,hum;
    if(NO_ERROR!=sensor.read_meas_data_single_shot(HIGH_REP_WITH_STRCH,&temp,&hum))
    {
      SERIAL.println("read temp failed!!");
      SERIAL.println("   ");
      SERIAL.println("   ");
      SERIAL.println("   ");
    }
    else
    {
      SERIAL.println("result======>");
      SERIAL.print("temperature =");
      SERIAL.println(temp);

      SERIAL.print("humidity =");
      SERIAL.println(hum);

      SERIAL.println("   ");
      SERIAL.println("   ");
      SERIAL.println("   ");
    }
    delay(1000);
}

Attention

The library file may be updated. This code may not be applicable to the updated library file, so we recommend that you use the first two methods.

  • Step 4. Upload the demo. If you do not know how to upload the code, please check How to upload code.

  • Step 5. Open the Serial Monitor of Arduino IDE by click Tool-> Serial Monitor. Or tap the Ctrl+Shift+M key at the same time. Set the baud rate to 115200.

Success

If every thing goes well, when you open the Serial Monitor , it may show as below:

serial start!!
=>
temperature =24.10
humidity =51.09


result======>
temperature =24.10
humidity =50.96


result======>
temperature =24.10
humidity =51.04


result======>
temperature =24.11
humidity =51.09

Play With Raspberry Pi (With Grove Base Hat for Raspberry Pi)

Hardware

  • Step 1. Things used in this project:
Raspberry pi Grove Base Hat for RasPi Grove - SHT35 Sensor
enter image description here enter image description here enter image description here
Get ONE Now Get ONE Now Get ONE Now
  • Step 2. Plug the Grove Base Hat into Raspberry.
  • Step 3. Connect the Grove - I2C High Accuracy Temp&Humi Sensor(SHT35) to I2C port of the Base Hat.
  • Step 4. Connect the Raspberry Pi to PC through USB cable.

Software

  • Step 1. Follow Setting Software to configure the development environment.
  • Step 2. Download the source file by cloning the grove.py library.
cd ~
git clone https://github.com/Seeed-Studio/grove.py
  • Step 3. Excute below commands to run the code.
cd grove.py/grove
python grove_I2C_High_Accuracy_tem_hum_SHT35_sensor.py 

Following is the grove_I2C_High_Accuracy_tem_hum_SHT35_sensor.py code.

import time
from grove.i2c import Bus

def CRC(data):
  crc = 0xff
  for s in data:
    crc ^= s
    for i in range(8):
      if crc & 0x80:
        crc <<= 1
        crc ^= 0x131
      else:
        crc <<= 1
  return crc

class GroveTemperatureHumiditySensorSHT3x(object):

    def __init__(self, address=0x45, bus=None):
        self.address = address

        # I2C bus
        self.bus = Bus(bus)

    def read(self):
        # high repeatability, clock stretching disabled
        self.bus.write_i2c_block_data(self.address, 0x24, [0x00])

        # measurement duration < 16 ms
        time.sleep(0.016)

        # read 6 bytes back
        # Temp MSB, Temp LSB, Temp CRC, Humididty MSB, Humidity LSB, Humidity CRC
        data = self.bus.read_i2c_block_data(0x45, 0x00, 6)
        temperature = data[0] * 256 + data[1]
        celsius = -45 + (175 * temperature / 65535.0)
        humidity = 100 * (data[3] * 256 + data[4]) / 65535.0
        if data[2] != CRC(data[:2]):
            raise RuntimeError("temperature CRC mismatch")
        if data[5] != CRC(data[3:5]):
            raise RuntimeError("humidity CRC mismatch")
        return celsius, humidity


def main():
    sensor = GroveTemperatureHumiditySensorSHT3x()
    while True:
        temperature, humidity = sensor.read()

        print('Temperature in Celsius is {:.2f} C'.format(temperature))
        print('Relative Humidity is {:.2f} %'.format(humidity))

        time.sleep(1)

if __name__ == "__main__":
  main()

Success

If everything goes well, you will be able to see the following result

pi@raspberrypi:~/grove.py/grove $ python grove_I2C_High_Accuracy_tem_hum_SHT35_sensor.py 
Temperature in Celsius is 20.47 C
Relative Humidity is 40.28 %
Temperature in Celsius is 20.47 C
Relative Humidity is 40.47 %
Temperature in Celsius is 20.47 C
Relative Humidity is 40.70 %
Temperature in Celsius is 20.43 C
Relative Humidity is 40.70 %
Temperature in Celsius is 20.41 C
Relative Humidity is 40.60 %
^CTraceback (most recent call last):
  File "grove_I2C_High_Accuracy_tem_hum_SHT35_sensor.py", line 89, in <module>
    main()
  File "grove_I2C_High_Accuracy_tem_hum_SHT35_sensor.py", line 86, in main
    time.sleep(1)
KeyboardInterrupt

You can quit this program by simply press Ctrl+C.

Schematic Online Viewer

Resources

Projects

Transportation data visualization with Google Map:We use the Wio LTE cat.1 to monitor transportation GPS and other info. For cold chain, we can monitor the GPS location together with temperature and humidity. For the bicycling, we can monitor the GPS location together with the hear rate.

Tech Support

Please do not hesitate to submit the issue into our forum