Grove - Passive Buzzer

This is a 3-5V passive buzzer. You can change the PMW frequency to award different beep sound to get a "buzzer music". Also, the buzzer can be set as an alarm for security applications. So get one and start your own project!
Features
- Passive: Tunable passive buzzer
- Interface: Grove
Specification
| Item | Value |
|---|---|
| Voltage range | 3V–5V |
| Resonant Frequency | 2700 Hz |
| sound output | > 80dB |
| Working temperature | -20-70 °C |
| Dimensions | 20mm 20mm 10mm |
| Weight | 3g |
| Battery | Exclude |
Platform Supported
| Arduino | Raspberry Pi | |||
|---|---|---|---|---|
![]() | ![]() | ![]() | ![]() | ![]() |
Getting Started
Play with Arduino
Materials Required
| Seeeduino XIAO | Grove Breadboard | Grove Passive Buzzer |
|---|---|---|
![]() | ||
| Get one now | Get one now | Get one now |
Hardware Connection

The Grove interface on the breadboard and on the Grove Passive Buzzer are connected by the Grove cable.
Software
- Step1 Copy the code below to the Arduino IDE and upload. If you do not know how to update the code, please check How to upload code.
Code example1 - simply get the beep sound
int buzzer = 5; // Buzzer connect with Pin 5
int frequency = 2700; //reach the Resonant Frequency
int cycle = 1000000/frequency;
void setup()
{
Serial.begin(9600); // set the baud rate
pinMode(buzzer,OUTPUT); // set buzzer as output
}
void loop()
{
digitalWrite(buzzer,HIGH);
delayMicroseconds(cycle/2);
digitalWrite(buzzer,LOW);
delayMicroseconds(cycle/2); // run the PMW cycle
}
- Step2 After uploading the code tp the board, you will hear thr buzzer beep.
Code example2 - Use buzzer to play music
//set the corresponding notes with frequency
#define NOTE_D0 0
#define NOTE_D1 294
#define NOTE_D2 330
#define NOTE_D3 350
#define NOTE_D4 393
#define NOTE_D5 441
#define NOTE_D6 495
#define NOTE_D7 556
#define NOTE_DL1 147
#define NOTE_DL2 165
#define NOTE_DL3 175
#define NOTE_DL4 196
#define NOTE_DL5 221
#define NOTE_DL6 248
#define NOTE_DL7 278
#define NOTE_DH1 589
#define NOTE_DH2 661
#define NOTE_DH3 700
#define NOTE_DH4 786
#define NOTE_DH5 882
#define NOTE_DH6 990
#define NOTE_DH7 112
#define WHOLE 1
#define HALF 0.5
#define QUARTER 0.25
#define EIGHTH 0.25
#define SIXTEENTH 0.625
//the note part of the whole song
int tune[] =
{
NOTE_DH1, NOTE_D6, NOTE_D5, NOTE_D6, NOTE_D0,
NOTE_DH1, NOTE_D6, NOTE_D5, NOTE_DH1, NOTE_D6, NOTE_D0, NOTE_D6,
NOTE_D6, NOTE_D6, NOTE_D5, NOTE_D6, NOTE_D0, NOTE_D6,
NOTE_DH1, NOTE_D6, NOTE_D5, NOTE_DH1, NOTE_D6, NOTE_D0,
NOTE_D1, NOTE_D1, NOTE_D3,
NOTE_D1, NOTE_D1, NOTE_D3, NOTE_D0,
NOTE_D6, NOTE_D6, NOTE_D6, NOTE_D5, NOTE_D6,
NOTE_D5, NOTE_D1, NOTE_D3, NOTE_D0,
NOTE_DH1, NOTE_D6, NOTE_D6, NOTE_D5, NOTE_D6,
NOTE_D5, NOTE_D1, NOTE_D2, NOTE_D0,
NOTE_D7, NOTE_D7, NOTE_D5, NOTE_D3,
NOTE_D5,
NOTE_DH1, NOTE_D0, NOTE_D6, NOTE_D6, NOTE_D5, NOTE_D5, NOTE_D6, NOTE_D6,
NOTE_D0, NOTE_D5, NOTE_D1, NOTE_D3, NOTE_D0,
NOTE_DH1, NOTE_D0, NOTE_D6, NOTE_D6, NOTE_D5, NOTE_D5, NOTE_D6, NOTE_D6,
NOTE_D0, NOTE_D5, NOTE_D1, NOTE_D2, NOTE_D0,
NOTE_D3, NOTE_D3, NOTE_D1, NOTE_DL6,
NOTE_D1,
NOTE_D3, NOTE_D5, NOTE_D6, NOTE_D6,
NOTE_D3, NOTE_D5, NOTE_D6, NOTE_D6,
NOTE_DH1, NOTE_D0, NOTE_D7, NOTE_D5,
NOTE_D6,
};
//the duration time of each note
float duration[] =
{
1, 1, 0.5, 0.5, 1,
0.5, 0.5, 0.5, 0.5, 1, 0.5, 0.5,
0.5, 1, 0.5, 1, 0.5, 0.5,
0.5, 0.5, 0.5, 0.5, 1, 1,
1, 1, 1 + 1,
0.5, 1, 1 + 0.5, 1,
1, 1, 0.5, 0.5, 1,
0.5, 1, 1 + 0.5, 1,
0.5, 0.5, 0.5, 0.5, 1 + 1,
0.5, 1, 1 + 0.5, 1,
1 + 1, 0.5, 0.5, 1,
1 + 1 + 1 + 1,
0.5, 0.5, 0.5 + 0.25, 0.25, 0.5 + 0.25, 0.25, 0.5 + 0.25, 0.25,
0.5, 1, 0.5, 1, 1,
0.5, 0.5, 0.5 + 0.25, 0.25, 0.5 + 0.25, 0.25, 0.5 + 0.25, 0.25,
0.5, 1, 0.5, 1, 1,
1 + 1, 0.5, 0.5, 1,
1 + 1 + 1 + 1,
0.5, 1, 0.5, 1 + 1,
0.5, 1, 0.5, 1 + 1,
1 + 1, 0.5, 0.5, 1,
1 + 1 + 1 + 1
};
int length;//define the number of notes
int buzzer = 5; //set the buzzer Pin
void setup()
{
pinMode(buzzer, OUTPUT); // set the buzzer as output mode
length = sizeof(tune) / sizeof(tune[0]); //count the number of note
}
void loop()
{
for (int x = 0; x < length; x++) //"sing" the note one by one
{
tone(buzzer, tune[x]); //output the "x" note
delay(400 * duration[x]); //rythem of the music,it can be tuned fast and slow by change the number"400"
noTone(buzzer);//stop the current note and go to the next note
}
delay(5000);//after playing the whole song, delay for 5 sec
}
- Step3 After uploading the code to the board, you can hear a music from the buzzer.
Play with Raspberry Pi
Materials Requied
| Raspberry Pi 4B(4GB) | Grove Base Hat for Raspberry Pi | Grove Digital PIR Motion Sensor |
|---|---|---|
![]() | ||
| Get one now | Get one now | Get one now |
Hardware Connection

Connect the Buzzer with "PWM" on the Grove Base Hat.
Software Code
- Step 1 Install Grove.py on your Raspberry.
One-click installation, quick start, what ever you call, with the single command below, we can install/update all dependencies and latest grove.py.
If you are using Raspberry Pi with Raspberrypi OS >= Bullseye, you cannot use this command line.
curl -sL https://github.com/Seeed-Studio/grove.py/raw/master/install.sh | sudo bash -s -
if everything goes well, you will see the following notice.
Successfully installed grove.py-0.5
#######################################################
Lastest Grove.py from github install complete !!!!!
#######################################################
``` -
Besides the one-click installation, you can also install all the dependencies and latest grove.py step by step.
If you are using Raspberry Pi with Raspberrypi OS >= Bullseye, you have to use this command line only with Python3.
git clone https://github.com/Seeed-Studio/grove.py
cd grove.py
# Python2
sudo pip install .
# Python3
sudo pip3 install .
- Step 2 Create a python file for the code.
cd grove.py
nano example.py
- Step 3 Copy the following code to the python file
#!/usr/bin/env python
import time
from mraa import getGpioLookup
from upm import pyupm_buzzer as upmBuzzer
def main():
# Grove - Buzzer connected to PWM port
buzzer = upmBuzzer.Buzzer(getGpioLookup('GPIO12'))
CHORDS = [upmBuzzer.BUZZER_DO, upmBuzzer.BUZZER_RE, upmBuzzer.BUZZER_MI,
upmBuzzer.BUZZER_FA, upmBuzzer.BUZZER_SOL, upmBuzzer.BUZZER_LA,
upmBuzzer.BUZZER_SI]
for i in range(0, len(CHORDS)):
buzzer.playSound(CHORDS[i], 500000)
time.sleep(0.1)
del buzzer
print('application exiting...')
if __name__ == '__main__':
main()
- Step 4 Run the program
sudo chmod +x example.py
sudo ./example.py
If everything goes well, you can hear"do,re,mi,fa,so.la.xi".
Schematic Online Viewer
Resource
- [PDF] MLT_8530_DATASHEET
- [PDF] Hardware schematic
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.