Skip to main content

Grove - Wio-E5 LoRa P2P Example

Are you looking for a simple, flexible, and cost-effective solution for your IoT project? Consider trying LoRa P2P.

LoRa is a low-power wireless modulation technology that enables devices to communicate over long distances with minimal energy consumption. "P2P" stands for "point-to-point," meaning devices can communicate directly with each other without the need for intermediate network infrastructure such as base stations or routers.

By leveraging LoRa P2P, IoT devices can communicate directly with each other in environments requiring long-distance communication and low power consumption.

Here's an example of how to build a LoRa point-to-point transmission application using Grove Wio-E5 and Seeed Studio XIAO SAMD21.

Preparations​

If this is your first time using Seeed Studio XIAO SAMD21, please refer to this wiki.

If this is your first time using Arduino, Please put your hand on here to start your Arduino journey.

Connecting hardware​

We can connect the Wio-E5 module to the UART socket directly as the below picture shows.

point to point transmission with grove wio e5

Download Library​

The u8g2 library must be installed for this demo. Click to download the library and install it (How to install an Arduino Library).

Download the example​

Copy the code stick on the Aruino IDE then upload it. One of them is used as a master, and the NODE_SLAVE macro definition in the code needs to be commented out, and the other is used as a slave, and the NODE_SLAVE macro definition in the code needs to be turned on.

# include <Arduino.h>
# include <U8x8lib.h>

// #define NODE_SLAVE

U8X8_SSD1306_128X64_NONAME_HW_I2C u8x8(/*reset=*/U8X8_PIN_NONE);
// U8X8_SSD1306_128X64_NONAME_SW_I2C u8x8(/*clock=*/ SCL, /*data=*/ SDA, /*reset=*/ U8X8_PIN_NONE); // OLEDs without Reset of the Display

static char recv_buf[512];
static bool is_exist = false;

static int at_send_check_response(char *p_ack, int timeout_ms, char*p_cmd, ...)
{
int ch = 0;
int index = 0;
int startMillis = 0;
va_list args;
memset(recv_buf, 0, sizeof(recv_buf));
va_start(args, p_cmd);
Serial1.printf(p_cmd, args);
Serial.printf(p_cmd, args);
va_end(args);
delay(200);
startMillis = millis();

if (p_ack == NULL)
{
return 0;
}

do
{
while (Serial1.available() > 0)
{
ch = Serial1.read();
recv_buf[index++] = ch;
Serial.print((char)ch);
delay(2);
}

if (strstr(recv_buf, p_ack) != NULL)
{
return 1;
}

} while (millis() - startMillis < timeout_ms);
return 0;
}

static int recv_prase(void)
{
char ch;
int index = 0;
memset(recv_buf, 0, sizeof(recv_buf));
while (Serial1.available() > 0)
{
ch = Serial1.read();
recv_buf[index++] = ch;
Serial.print((char)ch);
delay(2);
}

if (index)
{
char *p_start = NULL;
char data[32] = {
0,
};
int rssi = 0;
int snr = 0;

p_start = strstr(recv_buf, "+TEST: RX \"5345454544");
if (p_start)
{
p_start = strstr(recv_buf, "5345454544");
if (p_start && (1 == sscanf(p_start, "5345454544%s", data)))
{
data[4] = 0;
u8x8.setCursor(0, 4);
u8x8.print(" ");
u8x8.setCursor(2, 4);
u8x8.print("RX: 0x");
u8x8.print(data);
Serial.print(data);
Serial.print("\r\n");
}

p_start = strstr(recv_buf, "RSSI:");
if (p_start && (1 == sscanf(p_start, "RSSI:%d,", &rssi)))
{
u8x8.setCursor(0, 6);
u8x8.print(" ");
u8x8.setCursor(2, 6);
u8x8.print("rssi:");
u8x8.print(rssi);
}
p_start = strstr(recv_buf, "SNR:");
if (p_start && (1 == sscanf(p_start, "SNR:%d", &snr)))
{
u8x8.setCursor(0, 7);
u8x8.print(" ");
u8x8.setCursor(2, 7);
u8x8.print("snr :");
u8x8.print(snr);
}
return 1;
}
}
return 0;
}

static int node_recv(uint32_t timeout_ms)
{
at_send_check_response("+TEST: RXLRPKT", 1000, "AT+TEST=RXLRPKT\r\n");
int startMillis = millis();
do
{
if (recv_prase())
{
return 1;
}
} while (millis() - startMillis < timeout_ms);
return 0;
}

static int node_send(void)
{
static uint16_t count = 0;
int ret = 0;
char data[32];
char cmd[128];

memset(data, 0, sizeof(data));
sprintf(data, "%04X", count);
sprintf(cmd, "AT+TEST=TXLRPKT,\"5345454544%s\"\r\n", data);

u8x8.setCursor(0, 3);
u8x8.print(" ");
u8x8.setCursor(2, 3);
u8x8.print("TX: 0x");
u8x8.print(data);

ret = at_send_check_response("TX DONE", 2000, cmd);
if (ret == 1)
{

count++;
Serial.print("Sent successfully!\r\n");
}
else
{
Serial.print("Send failed!\r\n");
}
return ret;
}

static void node_recv_then_send(uint32_t timeout)
{
int ret = 0;
ret = node_recv(timeout);
delay(100);
if (!ret)
{
Serial.print("\r\n");
return;
}
node_send();
Serial.print("\r\n");
}

static void node_send_then_recv(uint32_t timeout)
{
int ret = 0;
ret = node_send();
if (!ret)
{
Serial.print("\r\n");
return;
}
if (!node_recv(timeout))
{
Serial.print("recv timeout!\r\n");
}
Serial.print("\r\n");
}

void setup(void)
{

u8x8.begin();
u8x8.setFlipMode(1);
u8x8.setFont(u8x8_font_chroma48medium8_r);

Serial.begin(115200);
// while (!Serial);

Serial1.begin(9600);
Serial.print("ping pong communication!\r\n");
u8x8.setCursor(0, 0);

if (at_send_check_response("+AT: OK", 100, "AT\r\n"))
{
is_exist = true;
at_send_check_response("+MODE: TEST", 1000, "AT+MODE=TEST\r\n");
at_send_check_response("+TEST: RFCFG", 1000, "AT+TEST=RFCFG,866,SF12,125,12,15,14,ON,OFF,OFF\r\n");
delay(200);
# ifdef NODE_SLAVE
u8x8.setCursor(5, 0);
u8x8.print("slave");
# else
u8x8.setCursor(5, 0);
u8x8.print("master");
# endif
}
else
{
is_exist = false;
Serial.print("No E5 module found.\r\n");
u8x8.setCursor(0, 1);
u8x8.print("unfound E5 !");
}
}

void loop(void)
{
if (is_exist)
{
# ifdef NODE_SLAVE
node_recv_then_send(2000);
# else
node_send_then_recv(2000);
delay(3000);
# endif
}
}

Review Results​

Resources​

Datasheet:

Certifications:

Relevant SDK:

Tech Support & Product Discussion​

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...