Skip to main content

How to Use XIAO ESP32S3 with LoRa Module via Arduino

The integration of Wio-E5 with XIAO-ESP32-S3 through Arduino presents a robust platform for IoT project development. This guide is designed to assist you in establishing a seamless connection between Wio-E5 and XIAO-ESP32-S3, enabling a wide range of applications and functionalities.

I will lead you through the process of utilizing XIAO-ESP32-S3, Grove-Wio-E5, and Grove-Temperature & Humidity Sensor for LoRa communication. Tailored for both beginners and intermediate enthusiasts, this tutorial offers step-by-step instructions for the setup and implementation of wireless communication using LoRa technology. The goal is to empower you with the skills to effectively employ XIAO-ESP32-S3 for LoRa communication. In the final stages, we will utilize ChirpStack to display the collected data in Home Assistant.

Implementation​

Arduino Program Code​

Software​

Make certain modifications to the following code, such as modifying the AppKEY and other essential information of LoRa communication module, so as to be able to access LoRaWAN, and then modify the data we want to send by command: AT+CMSGHEX. For example, I send data by simulating temp and humi here.

#include <Arduino.h>
#include <Wire.h>
#include <DHT.h>

// Buffer to receive data
static char recv_buf[512];
static bool is_exist = false;
static bool is_join = false;
static int led = 0;

int sensorPin = A1; // Define the sensor pin
#define DHTTYPE DHT20 // Use DHT 20 type
DHT dht(DHTTYPE); // Initialize DHT sensor for temperature and humidity

// Function to send AT commands and check for expected response within a timeout
static int at_send_check_response(char *expected_ack, int timeout_ms, char *command_format, ...) {
int character;
int num = 0;
int index = 0;
int startMillis = 0;
va_list args;
memset(recv_buf, 0, sizeof(recv_buf));
va_start(args, command_format);
Serial1.printf(command_format, args);
Serial.printf(command_format, args);
va_end(args);
delay(200);
startMillis = millis();

if (expected_ack == NULL) {
return 0;
}

do {
while (Serial1.available() > 0) {
character = Serial1.read();
recv_buf[index++] = character;
Serial.print((char)character);
delay(2);
}

if (strstr(recv_buf, expected_ack) != NULL) {
return 1;
}
} while (millis() - startMillis < timeout_ms);
return 0;
}

// Function to parse received messages
static void recv_parse(char *message) {
if (message == NULL) {
return;
}
char *start = NULL;
int data = 0;
int rssi = 0;
int snr = 0;

start = strstr(message, "RX");
if (start && (1 == sscanf(start, "RX: \"%d\"\r\n", &data))) {
Serial.println(data);
Serial.print("led :");
led = !!data;
Serial.println(led);
digitalWrite(LED_BUILTIN, led ? LOW : HIGH);
}

start = strstr(message, "RSSI");
if (start && (1 == sscanf(start, "RSSI %d,", &rssi))) {
Serial.print("RSSI:");
Serial.println(rssi);
}

start = strstr(message, "SNR");
if (start && (1 == sscanf(start, "SNR %d", &snr))) {
Serial.print("SNR :");
Serial.println(snr);
}
}

void setup() {
Serial.begin(115200); // Initialize serial communication
Serial1.begin(9600, SERIAL_8N1, 44, 43);
Wire.begin();
dht.begin();

// Basic AT command to check module presence
if (at_send_check_response("+AT: OK", 100, "AT\r\n")) {
is_exist = true;

// Send AT+ID command to get the device ID
if (at_send_check_response("+ID:", 1000, "AT+ID\r\n")) {
Serial.print("Received ID data: ");
Serial.println(recv_buf);
} else {
Serial.println("Failed to get ID data.");
}

// Other configuration commands
at_send_check_response("+MODE: LWOTAA", 1000, "AT+MODE=LWOTAA\r\n");
at_send_check_response("+DR: EU868", 1000, "AT+DR=EU868\r\n");
at_send_check_response("+CH: NUM", 1000, "AT+CH=NUM,0-2\r\n");
at_send_check_response("+KEY: APPKEY", 1000, "AT+KEY=APPKEY,\"2B7E151628AED2A6ABF7158809CF4F3D\"\r\n");
at_send_check_response("+CLASS: C", 1000, "AT+CLASS=A\r\n");
at_send_check_response("+PORT: 8", 1000, "AT+PORT=8\r\n");

delay(200);
is_join = true;
} else {
is_exist = false;
Serial.println("No E5 module found.");
}
}

void loop() {
float temp_hum_val[2] = {0};
if (is_exist) {
int ret = 0;
if (is_join) {
ret = at_send_check_response("+JOIN: Network joined", 12000, "AT+JOIN\r\n");
if (ret) {
is_join = false;
} else {
at_send_check_response("+ID: AppEui", 1000, "AT+ID\r\n");
Serial.println("JOIN failed!");
delay(5000);
}
} else {
if (!dht.readTempAndHumidity(temp_hum_val)) {
char cmd[128];
sprintf(cmd, "AT+CMSGHEX=\"%04X%04X%04X\"\r\n", int(temp_hum_val[1] * 100), int(temp_hum_val[0] * 100), analogRead(sensorPin));
ret = at_send_check_response("Done", 5000, cmd);
if (ret) {
recv_parse(recv_buf);
} else {
Serial.println("Send failed!");
}
}
delay(30000);
}
} else {
delay(1000);
}
}

ChirpStack Configuration​

ChirpStack is an open-source Internet of Things (IoT) solution designed for building and managing LoRaWAN networks. It provides a comprehensive set of tools and services to assist users in deploying, managing, and monitoring LoRaWAN networks, including gateways, network servers, application servers, and devices. For information on how to connect to ChirpStack, please refer to this link.

After creating a new device profile in ChirpStack, fill in the payload codec with the following code:

function decodeUplink(input) {
var decoded = {
temp: 0,
humi: 0,
moisture: 0,
};
var bytes = input["bytes"];
bytes = bytes2HexString(bytes);

// Assuming the data is encoded at a ratio of 100 times
decoded.temp = parseInt(bytes.slice(0, 4), 16) / 100;
decoded.humi = parseInt(bytes.slice(4, 8), 16) / 100;
decoded.moisture = parseInt(bytes.slice(-4), 16);

let messages = [
{
type: "temp",
measurementId: 4097,
measurementValue: decoded.temp,
},
{
type: "humi",
measurementId: 4098,
measurementValue: decoded.humi,
},
{
type: "moisture",
measurementId: 4103,
measurementValue: decoded.moisture,
},
];

var result = {};
result.messages = messages;
return { data: result };
}

/**
* Convert to an 8-digit binary number with 0s in front of the number
* @param arr
* @returns {string}
*/
function toBinary(arr) {
let binaryData = arr.map((item) => {
let data = parseInt(item, 16).toString(2);
let dataLength = data.length;
if (data.length !== 8) {
for (let i = 0; i < 8 - dataLength; i++) {
data = `0` + data;
}
}
return data;
});
let ret = binaryData.toString().replace(/,/g, "");
return ret;
}

function bytes2HexString(arrBytes) {
var str = "";
for (var i = 0; i < arrBytes.length; i++) {
var tmp;
var num = arrBytes[i];
if (num < 0) {
tmp = (255 + num + 1).toString(16);
} else {
tmp = num.toString(16);
}
if (tmp.length === 1) {
tmp = "0" + tmp;
}
str += tmp;
}
return str;
}

Click Submit.​

As shown in the following figure, the relevant data is received, indicating that the data is successfully sent.

Decoding alone may not provide a visually intuitive representation of sensor data. In such cases, we can utilize user-friendly platforms, with Home Assistant being a prime example.

Application: Integrate with Home Assistant​

Home Assistant is an open-source smart home automation platform designed to enable users to integrate, control, and automate various smart devices and services. It supports interoperability with a wide range of smart home devices, allowing users to create customized automation scenarios and smart home control systems. If we can integrate XIAO-ESP32-S3 with Home Assistant, it will diversify the development possibilities for XIAO-ESP32-S3.

Both ChirpStack and Home Assistant have built-in MQTT plugin integration. This allows them to communicate data through the MQTT protocol, facilitating the transmission of sensor data from the gateway (equipped with an MQTT plugin) to Home Assistant.

You can also integrate Wio-E5 with XIAO-ESP32-S3 into Home Assistant. Please refer to this tutorial.

  • Step 3: Click Send and Test the sensor by clicking Measure

Tech Support & Product Discussion​

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...