Skip to main content

Wio-E5 mini

pir

LoRaWAN® is a mark used under license from the LoRa Alliance®. The LoRa® Mark is a trademark of Semtech Corporation or its subsidiaries.

Wio-E5 mini is a compacted-sized development board suitable for the rapid testing and building of small-size prototyping and helps you design your ideal LoRaWAN® wireless IoT device with a long-distance transmission range.

Wio-E5 mini is embedded with Wio-E5 STM32WLE5JC Module, which delivers the world-first combo of LoRa® RF and MCU chip into one single tiny chip and is FCC and CE certified. It is powered by ARM Cortex-M4 core and Semtech SX126X LoRa® chip and supports LoRaWAN® protocol on the worldwide frequency and (G)FSK, BPSK, (G)MSK, and LoRa® modulations.

Learn more about Wio-E5 here.

More comparison between the Wio-E5 and LoRa® RFM95 chip:

pir

Wio-E5 mini leads out all GPIOs of Wio-E5, including UART, ADC, SPI, IIC, and etc. It contains RESET and BOOT buttons and is use-friendly. Supporting LoRaWAN® protocol, Wio-E5 mini features ultra-long-range transmission and ultra-low power consumption: it is able to achieve a transmission range of up to 10 km, and the sleep current of Wio-E5 modules on board is as low as 2.1 uA(WOR mode). It is designed with industrial standards with a wide working temperature at -40 ℃ ~ 85℃, high sensitivity between -116.5dBm ~ -136 dBm, and RF output power up to +20.8 dBm at 3.3V.

Other than the Wio-E5 mini, we also provide other choices including the Wio-E5 Development Board carrying more complex interfaces and features to unlock the more powerful performance of the Wio-E5 module. It provides a broader range of access protocols and superabundant types of interfaces. Thus you are able to test and prototype the module rapidly with RS-485, Grove interfaces, and rich GPIOs. (Learn more about Wio-E5 Development Board)

Since Wio-E5 is a LoRaWAN® chip with an MCU, there are three main ways to utilize the Wio-E5 mini:

1. Connect Wio-E5 mini to PC and control by AT commands

There is a built-in USB to UART function on board, you could connect the Wio-E5 mini to your PC with a USB type C cable, and use serial communication software to send AT commands and read data from the board.

2. Connect Wio-E5 mini to another mainboard via UART and control by AT commands

For example, connect Wio-E5 mini to Seeeduino XIAO and the Expansion Board via UART, and send AT commands and read data from Seeeduino XIAO through Arduino IDE serial monitor.

3. User Application Development by using SDK

Develop your own LoRa® development board with MCU function by using STM32Cube Programmer, which is the SDK officially provided by STMicroelectronics. To download this SDK resource, please find the resources in learning and document down below.

With all the outstanding features listed above, the Wio-E5 mini will be a superior choice for IoT device development, testing, prototyping, and applications in long-distance, ultra-low power consumption IoT scenarios like smart agriculture, smart office, and smart industry.

If you are unfamiliar with LoRa® and LoRaWAN® technology, please check out this blog LoRa®pedia in detail.

Features

  • Full GPIOs led out from the Wio-E5 STM32WLE5JC

  • Global LoRaWAN® and LoRa® frequency plan supported

  • Long-distance transmission range to 10km (ideal value in open area)

  • Mini and compact size, suitable for rapid testing and building small size prototype

  • Convenient RESET and BOOT buttons on board

Hardware Overview

pir

pir

Specifications

ParametersSpecifications
size50*23mm
voltage - supply3.7V - 5V
power - outputup to +20.8 dBm at 3.3V
working frequency868/915MHz
protocolLoRaWAN®
sensitivity-116.5 dBm ~ -136 dBm
interfacesUSB Type C / 2P-2.54mm Hole / 112P-2.54mm Header2 / SMA-K / IPEX
modulationLoRa®, (G)FSK, (G)MSK, BPSK
working temperature-40℃ ~ 85℃
currentWio-E5 module sleep current as low as 2.1uA (WOR mode)
Part List:
Wio-E5 mini *1
Antenna(EU868/US915)*1
USB TypeC (20cm) *1
Sticker*1 
1X12pin male pin headers *2

Applications

  • Wio-E5 module Easy testing
  • Rapid small-dimension prototyping of LoRa® devices with Wio-E5
  • Any long-distance wireless communication application development
  • LoRa® and LoRaWAN® application learn and research

pir

Application Notes

1. Factory AT Firmare

wio-E5 series has a built-in AT command firmware, which supports LoRaWAN® Class A/B/C protocol and a wide frequency plan: EU868/US915/AU915/AS923/KR920/IN865. With this AT command firmware, developers can easily and quickly build their prototype or application.

The AT command firmware contains a bootloader for DFU and the AT application. The "PB13/SPI_SCK/BOOT" pin is used to control Wio-E5 to stay in the bootloader or jump to the AT application. When PB13 is HIGH, the module will jump to AT application after reset, with a default baud rate of 9600. When PB13 is LOW (press the "Boot" button on Wio-E5 mini), the module will stay in the bootloader, and keep transmitting "C" character every 1S at baud rate 115200.

tip
  • Factory AT Firmware is programmed with RDP(Read Protection) Level 1, developers need to remove RDP first with STM32Cube Programmer. Note that regression RDP to level 0 will cause a flash memory mass to erase and the Factory AT Firmware can't be restored again.
  • The "PB13/SPI_SCK/BOOT" pin on the Wio-E5 module is just a normal GPIO, not the "BOOT0" pin of the MCU. This "PB13/SPI_SCK/BOOT" pin is used in the bootloader of the Factory AT firmware, to decide to jump to APP or stay in bootloader(for DFU). The real "BOOT0" pin doesn't pinout to the module, so users need to be careful when developing the low-power applications

2. Clock Configuration

2.1 HSE

  • 32MHz TCXO

  • TCXO power supply: PB0-VDD_TCXO

2.2 LSE

  • 32.768KHz crystal oscillator

3. RF Switch

Wio-E5 module ONLY transmits through RFO_HP:

  • Receive: PA4=1, PA5=0

  • Transmit(high output power, SMPS mode): PA4=0, PA5=1

Getting Started

Quick start of AT Commands

Preparation

  • Step 1. Connect Wio-E5 mini to PC via a Type-C cable

  • Step 2. Open a serial tool(eg. Arudino Serial Monitor), select the right COM port, set baudrate to 9600 and select Both NL & CR

  • Step 3. Try to send "AT" and you will see the response.

pir

Basic AT Commands

Command FormatReturnDescription
AT+AT: OKTest command
AT+VER+VER: $MAJOR.$MINOR.$PATCH
+VER: 4.0.11
Check Firmware version
AT+ID // Read all, DevAddr( ABP), DevEui( OTAA), AppEui( OTAA)
AT+ID = DevAddr // Read Device Address
AT+ID = DevEui // Read DevEui
AT+ID = AppEui // Read AppEui
+ID: DevAddr, xx: xx: xx:xx
+ID: DevEui, xx:xx:xx:xx:xx:xx:xx:xx
+ID: AppEui13, xx:xx:xx:xx:xx:xx:xx
Use to check the ID of the LoRaWAN module. ID is treated as big endian numbers.
AT+ID = DevAddr, “01234567” // Set new DevAddr
AT+ID = DevEui, “0123456789ABCDEF” // Set new DevEui
AT+ID = AppEui, “0123456789ABCDEF” // Set new AppEui
+ID: DevAddr, 01:23:45:67
+ID: DevEui, 01:23:45:67:89:AB:CD:EF
+ID: AppEui, 01:23:45:67:89:AB:CD:EF
Change the ID
AT+RESET+RESET: OKReset the module
AT+MSG=”Data to send”+MSG: Start
+MSG: FPENDING // Downlink frame FPENDING flag is set
+MSG: Link 20, 1
+MSG: ACK Received // LinkCheckAns received
+ MSG: MULTICAST // Downlink frame is multi cast message
+MSG: PORT: 8; RX: "12345678" //Downlink message is received
+MSG: RXWIN2, RSSI -106, SNR 4 //Downlink frame signal strength
+MSG: Done
send string format frame which is no need to be confirmed by the server
AT+PORT = “port”
eg: AT+PORT = 8 //Set port to 8
+ PORT: 8Set port number which will be used by MSG/CMSG/MSGHEX/CMSGHEX command to send message, port number should range from 1 to 255.
AT+ADR=" state"
eg: AT+ADR=ON // Enable ADR function
AT+ ADR= OFF // Disable ADR function
AT+ADR=? // Check current ADR configuration
+ADR: ON // ADR query/ set returnSet ADR function of LoRaWAN module
AT+DR // Check current selected DataRate
AT+DR=drx // "drx" should range 0~15
+DR: DR0
+DR: US915 DR0 SF10 BW12
Use LoRaWAN defined DRx to set datarate of LoRaWAN AT modem.
AT+ DR= band //" band" could be band names defined in Chapter3 Band Plans
AT+ DR= SCHEME // Check current band
(EU868) +DR: EU868
+DR: EU868 DR0 SF12 BW125K
+DR: EU868 DR1 SF11 BW125K
+DR: EU868 DR2 SF10 BW125K
+DR: EU868 DR3 SF9 BW125K
+DR: EU868 DR4 SF8 BW125K
+DR: EU868 DR5 SF7 BW125K
+DR: EU868 DR6 SF7 BW125K
+DR: EU868 DR7 FSK
+DR: EU868 DR8 RFU
+DR: EU868 DR9 RFU
+DR: EU868 DR10 RFU
+DR: EU868 DR11 RFU
+DR: EU868 DR12 RFU
+DR: EU868 DR13 RFU
+DR: EU868 DR14 RFU
+DR: EU868 DR15 RFU
Data rate scheme
AT + CH // query all channels
AT + CH = ch // check single channel frequency
Query Channel Configuration
AT+CH="chn", ["freq"], ["drmin"], ["drmax"]
// Change the chn channel frequency to "Freq"
// "freq" is in MHz.
// Available "drmin"/"drmax" range DR0 ~ DR15
+CH: 3,433700000,DR0:DR5
+CH: 3,433700000,DR
Set channel parameter of LoRaWAN modem, Set frequency zero to delete one channel.
AT+CH=chn,ON
AT+CH=chn, OFF
Enable or Disable Channel
AT+ KEY= NWKSKEY, “ 16 bytes length key”
eg: AT+KEY=NWKSKEY, "2B7E151628AED2A6ABF7158809CF4F3C"
eg: AT+KEY=NWKSKEY, "2B 7E 15 16 28 AE D2 A6 AB F7 15 88 09 CF 4F 3C”
+ KEY: NWKSKEY 2B7E151628AED2A6ABF7158809CF4F3CChange network session key (NWKSKEY)
AT+ KEY= APPSKEY, “ 16 bytes length key”
eg: AT+KEY=APPSKEY, "2B7E151628AED2A6ABF7158809CF4F3C"
eg: AT+KEY= APPSKEY, "2B 7E 15 16 28 AE D2 A6 AB F7 15 88 09
+ KEY: APPSKEY 2B7E151628AED2A6ABF7158809CF4F3CChange application session key (APPSKEY)
AT+ FDEFAULT
AT+ FDEFAULT= Seeed
+FDEFAULT: OKReset LoRaWAN AT modem to factory default configuration
T+ DFU=" New state"
eg: AT+DFU=ON // Enable DFU function
eg: AT+DFU=OFF //Disable DFU function
AT+DFU=? // Check if DFU is enabled configuration
+DFU: ON
+DFU: OFF
Use to enter DFU mode
T+MODE="mode"
eg: AT+MODE=TEST // Enter TEST mode
eg: AT+MODE= LWOTAA // Enter LWOTAA mode
eg: AT+MODE= LWABP // Enter LWABP mode
+MODE: LWABP // Enter TEST mode successfully
+MODE: LWOTAA // Enter LWOTAA mode successfully
+MODE: TEST // Enter TEST mode successfully
Use to select work mode
AT + JOIN
AT + JOIN = FORCE
a) Join successfully +JOIN: Starting
+ JOIN: NORMAL
+JOIN: NetID 000024 DevAddr 48:00:00:01
+JOIN: Done
b) Join failed
+JOIN: Join failed
c) Join process is ongoing
+ JOIN: LoRaWAN modem is busy
When OTAA mode is enabled, JOIN command could use to join a known network

For more information, refer to the Command Specification.

Connect and send data to The Things Network

  • Step 1. Visit The Things Network website and sign up for a new account

  • Step 2. After logging in, click your profile and select Console

pir

  • Step 3. Select a cluster to start adding devices and gateways

pir

  • Step 4. Click Go to applications

pir

  • Step 5. Click + Add application

pir

  • Step 6. Fill Application ID and click Create application

pir

Note: Here Application name and Description are not compulsory fields. If Application name is left blank, it will use the same name as Application ID by default

The following is the newly created application

pir

  • Step 7. Click + Add end device

pir

  • Step 8. Click Manually, to enter the registration credentials manually

pir

  • Step 9. Select the Frequency plan according to your region. Also make sure you use the same frequency as the gateway in which you will connect this device to. Select MAC V1.0.2 as the LoRaWAN® version and PHY V1.0.2 REV B as the Regional Parameters version. These settings are according to the LoraWAN® stack of Wio-E5.

pir

  • Step 10. While the Wio-E5 module is still accessible over the serial console, send the following AT commands on the serial monitor:

    • AT+ID=DevEui to get your Device EUI
    • AT+ID=AppEui, to get your App EUI
    • AT+KEY=APPKEY,"2B7E151628AED2A6ABF7158809CF4F3C" to set the App Key

The output will be as follows:

Tx: AT+ID=DevEui
Rx: +ID: DevEui, 2C:F7:F1:20:24:90:03:63
Tx: AT+ID=AppEui
Rx: +ID: AppEui, 80:00:00:00:00:00:00:07
Tx: AT+KEY=APPKEY,"2B7E151628AED2A6ABF7158809CF4F3C"
Rx: +KEY: APPKEY 2B7E151628AED2A6ABF7158809CF4F3C
  • Step 11. Copy and paste the above information into DevEUI, AppEUI and AppKey fields. End device ID field will be automatically filled when we fill DevEUI. Finally click Register end device

pir

  • Step 12. Register your LoRaWAN® Gateway with TTN Console. Please refer to the instructions shown here

  • Step 13. Type the following AT commmands to connect to TTN

// If you are using US915
AT+DR=US915
AT+CH=NUM,8-15

// If you are using EU868
AT+DR=EU868
AT+CH=NUM,0-2

AT+MODE=LWOTAA
AT+JOIN

The output on serial monitor will be as follows:

Tx: AT+DR=US915
Rx: +DR: US915
Tx: AT+CH=NUM,8-15
Rx: +CH: NUM, 8-15

Tx: AT+MODE=LWOTAA
Rx: +MODE: LWOTAA

Tx: AT+JOIN
Rx: +JOIN: Start
+JOIN: NORMAL
+JOIN: Network joined
+JOIN: NetID 000013 DevAddr 26:01:5F:66
+JOIN: Done

If you see +JOIN: Network joined on your serial console, that means your device has successfully connected to TTN!

You can also check your device status on the End devices page

pir

  • Step 14. Type the following AT commands to send data to TTN
// send string "HELLO" to TTN 
Tx: AT+MSG=HELLO
Rx: +MSG: Start
+MSG: FPENDING
+MSG: RXWIN2, RSSI -112, SNR -1.0
+MSG: Done
// send hex "00 11 22 33 44"
Tx: AT+MSGHEX="00 11 22 33 44"
Rx: +MSGHEX: Start
+MSGHEX: Done

For more information about AT Commands, please refer to Wio-E5 AT Command Specification

Develop with STM32Cube MCU Package

This section is for Wio-E5 mini, aiming at building several applications with STM32Cube MCU Package for STM32WL series(SDK).

Note: We have now updated the library to support v1.1.0 which is the latest version of STM32Cube MCU Package for STM32WL series.

note

Please read Erase Factory AT Firmware section first, as if we need to erase the Factory AT Firmware before we program with SDK. After erasing the Factory AT Firmware it CANNOT be recovered.

Preparations

Software:

Hardware:

  • LoRaWAN® Gateway connected to LoRaWAN® Network Server (e.g. TTN)

  • A USB Type-C cable and a ST-LINK. Connect the Type-C cable to the Type-C port of the board for power and serial communication. Connect the ST-LINK to the SWD pins as follows

connection

GPIO Configuration Overview

  • As the hardware design of Wio-E5 series is a bit different with NUCLEO-WL55JC, the official STM32WL55JC development board from ST, developers need to reconfigure some gpios, to adapt the SDK example to Wio-E5 series. We have already reconfigured GPIOs, but we think it is nessary to point out the difference.
SDK Example LabelGPIO of NUCLEO-WL55JCGPIO of Wio-E5 mini
RF_CTRL1PC4PA4
RF_CTRL2PC5PA5
RF_CTRL3PC3None
BUT1PA0PB13 (Boot Button)
BUT2PA1None
BUT3PC6None
LED1PB15None
LED2PB9PB5
LED3PB11None
PROB1PB12PA0 (D0 Button)
PROB2PB13PB10
PROB3PB14PB3
PROB4PB10PB4
UsartUsart2(PA2/PA3)Usart1(PB6/PB7)
note

The label PROB refers to the pin of Probe Line. These pins are able to set as the CM4_EVENTOUT additional function. As part of the CoreSight debugging components of Arm Cortex-M4 kernel, this feature enables non-intrusive debugging and hardware-level event tagging. It monitors CPU internal activities in real time without pausing the CPU or occupying communication interfaces (such as UART), converting “events” that are difficult to observe directly in software into measurable electrical signals.

Applications

Now we will explore several applications for Wio-E5 mini with STM32Cube MCU Package for STM32WL series(SDK).

LoRaWAN® End Node

This application will connect Wio-E5 mini with TTN (The Things Network) and send data after connecting with a LoRaWAN® gateway.

  • Step 1. Click here to visit Seeed-Studio/LoRaWan-E5-Node repository and download it as a ZIP file

pir

  • Step 2. Extract the ZIP file and navigate to LoRaWan-E5-Node > Projects > Applications > LoRaWAN > LoRaWAN_End_Node > STM32CubeIDE

  • Step 3. Double click the .project file

    Note: For MAC, it should take one of the options below to open the project:

    • 1. Navigate to Wio-E5-Node > Projects > Applications > LoRaWAN > LoRaWAN_End_Node. Doulble click file "LoRaWAN_End_Node.ioc".

    • 2. Use "Import Projects from File System or Archieve" like below images.

pir

  • Step 4. Right click on the project and click Properties

pir

  • Step 5. Navigate to C/C++ Build > Settings > MCU Post build outputs, tick Convert to Intel Hex file (-O ihex) and click Apply and Close

pir

  • Step 6. Click Build 'Debug', and it should compile without any errors

build

pir

Now we will modify our Device EUI, Application EUI, Application KEY and LoRawan® Region

  • Step 7. Please follow the guide here to setup your TTN application, get your Application EUI and copy it to the macro definition LORAWAN_JOIN_EUI in LoRaWAN/App/se-identity.h , for example, the Application EUI here is 80 00 00 00 00 00 00 0x07 :
// LoRaWAN/App/se-identity.h

/*!
* App/Join server IEEE EUI (big endian)
*/
#define LORAWAN_JOIN_EUI { 0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x07 }
  • Step 8. Also, you can modify your Device EUI and Application Key, by setting the macro definition LORAWAN_DEVICE_EUI and LORAWAN_NWK_KEY in LoRaWAN/App/se-identity.h. Make sure LORAWAN_DEVICE_EUI and LORAWAN_NWK_KEY are the same as the Device EUI and App Key in TTN console.
// LoRaWAN/App/se-identity.h

/*!
* end-device IEEE EUI (big endian)
*/
#define LORAWAN_DEVICE_EUI { 0x2C, 0xF7, 0xF1, 0x20, 0x24, 0x90, 0x03, 0x63 }

/*!
* Network root key
*/
#define LORAWAN_NWK_KEY 2B,7E,15,16,28,AE,D2,A6,AB,F7,15,88,09,CF,4F,3C

pir

  • Step 9. The default LoRaWAN Region is EU868, you can modify it, by setting the macro definition ACTIVE_REGION in LoRaWAN/App/lora_app.h
// LoRaWAN/App/lora_app.h

/* LoraWAN application configuration (Mw is configured by lorawan_conf.h) */
/* Available: LORAMAC_REGION_AS923, LORAMAC_REGION_AU915, LORAMAC_REGION_EU868, LORAMAC_REGION_KR920, LORAMAC_REGION_IN865, LORAMAC_REGION_US915, LORAMAC_REGION_RU864 */
#define ACTIVE_REGION LORAMAC_REGION_US915

pir

  • Step 10. After the above modifications, rebuild the example and program to your Wio-E5. Open STM32CubeProgrammer, connect ST-LINK to your PC, hold RESET Button of your Device, then click Connect and release RESET Button:

pir

  • Step 11. Make sure the Read Out Protection is AA, if it is shown as BB, select AA and click Apply:

pir

  • Step 12. Now, go to the Erasing & Programming page, select your hex file path(for example: C:\Users\user\Downloads\LoRaWan-E5-Node\Projects\Applications\LoRaWAN\LoRaWAN_End_Node\STM32CubeIDE\Debug\LoRaWAN_End_Node.hex ), select the programming options as the following picture, then click Start Programming!

pir

You will see the message Download verified successfully, once programming is finished.

  • Step 13. If your LoRaWAN® Gateway and TTN are setup, Wio-E5 will join successfully after reset! A confirm LoRaWAN® package will be sent to TTN every 30 seconds. The following log will be printed on the serial monitor (Arduino Serial Monitor is used here) if the join is successful:

pir

  • Cheers! Now you have connected Wio-E5 to LoRaWAN® Network! You can now proceed to develop more exciting LoRaWAN® End Node applications!

Note: Wio-E5 only supports high power output mode, so you can't use these macro definitions in radio_board_if.h :

#define RBI_CONF_RFO     RBI_CONF_RFO_LP_HP
// or
#define RBI_CONF_RFO RBI_CONF_RFO_LP

Eventhough RBI_CONF_RFO is defined as RBI_CONF_RFO_LP_HP in radio_board_if.h, it will not be used because USE_BSP_DRIVER is defined and BSP_RADIO_GetTxConfig() function returns RADIO_CONF_RFO_HP

FreeRTOS LoRaWAN®

This application will also connect Wio-E5 mini with TTN (The Things Network) and send data after connecting with a LoRaWAN® gateway. The difference between previous LoRaWAN® End Node application and this FreeRTOS LoRaWAN® application is that, the previous one runs on bare metal whereas this runs under FreeRTOS.

  • Step 1. Click here to visit Seeed-Studio/LoRaWan-E5-Node repository and download it as a ZIP file

pir

  • Step 2. Extract the ZIP file and navigate to LoRaWan-E5-Node > Projects > Applications > FreeRTOS > FreeRTOS_LoRaWAN

  • Step 3. Double click the .project file

  • Step 4. Refer to step 4 - step 13 from the previous LoRaWAN® End Node application to connect Wio-E5 mini with TTN!

FreeRTOS LoRaWAN® AT

This application will also connect Wio-E5 mini with TTN (The Things Network) and send data after connecting with a LoRaWAN® gateway. The difference between previous FreeRTOS LoRaWAN application and this application is that, you can use AT commands.

  • Step 1. Click here to visit Seeed-Studio/LoRaWan-E5-Node repository and download it as a ZIP file

pir

  • Step 2. Extract the ZIP file and navigate to LoRaWan-E5-Node > Projects > Applications > FreeRTOS > FreeRTOS_LoRaWAN_AT

  • Step 3. Double click the .project file

  • Step 4. Refer to step 4 - step 12 from the previous LoRaWAN End Node application

  • Step 5. Open a serial monitor such as Arduino Serial Monitor and you will see the following output

pir

  • Step 6. Type AT? and press ENTER to view all the available AT commands

pir

  • Step 7. If you still want to change Device EUI, Application EUI, Application KEY and LoRawan® Region, you can change using AT commands. However, these parameters are already set in se-identity.h and lora_app.h in this example

  • Step 8. Type AT+JOIN=1 and you will see the following output once the join is successful!

pir

Note: Here AT+JOIN=(Mode) format should be used. Mode corresponds to either 0 for ABP or 1 for OTAA

FreeRTOS LowPower

This application will enable low-power mode on Wio-E5 mini. Once the application is flashed, the board will consume power as normal for 2 seconds and enter low-power mode for 2 seconds and so on.

  • Step 1. Click here to visit Seeed-Studio/LoRaWan-E5-Node repository and download it as a ZIP file

pir

  • Step 2. Extract the ZIP file and navigate to LoRaWan-E5-Node > Projects > Applications > FreeRTOS > FreeRTOS_LowPower

  • Step 3. Double click the .project file

  • Step 4. Right click on the project and click Properties

pir

  • Step 5. Navigate to C/C++ Build > Settings > MCU Post build outputs, tick Convert to Intel Hex file (-O ihex) and click Apply and Close

pir

  • Step 6. Click Build 'Debug', and it should compile without any errors

pir

pir

  • Step 7. Open STM32CubeProgrammer, connect ST-LINK to your PC, hold RESET Button of your Device, then click Connect and release RESET Button:

pir

  • Step 8. Make sure the Read Out Protection is AA, if it is shown as BB, select AA and click Apply:

pir

  • Step 9. Now, go to the Erasing & Programming page, select your hex file path(for example: C:\Users\user\Downloads\LoRaWan-E5-Node\Projects\Applications\FreeRTOS\FreeRTOS_LowPower\Debug\FreeRTOS_LowPower.hex ), select the programming options as the following picture, then click Start Programming!

pir

You will see the message Download verified successfully, once programming is finished.

  • Step 10. Connect the Wio-E5 mini to a PC by attaching a power meter. You will notice the red LED on the board blinks every second and the board switches between normal and low power states (The current on the power meter comes down for 1 second for lower power state and comes back up for 1 second for normal working state)

pir

Low Power

This application will also enable low-power mode on Wio-E5 mini. The difference between previous FreeRTOS LowPower application and this Low Power application is that, the previous one runs under FreeRTOS whereas this runs on bare metal.

  • Step 1. Click here to visit Seeed-Studio/LoRaWan-E5-Node repository and download it as a ZIP file

pir

  • Step 2. Extract the ZIP file and navigate to LoRaWan-E5-Node > Projects > Applications > LowPower

  • Step 3. Double click the .project file

  • Step 4. Refer to step 4 - step 10 from the previous FreeRTOS LowPower application and you will see the same output at the end on the power meter!

Resources

Wio-E5 mini Datasheet:

Wio-E5 Datasheet:

Wio-E5 Certifications:

Relevant SDK:

Tech Support & Product Discussion

Please submit any technical issue into our forum.

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...