Keypoint Detection - PFLD
This section describes how to train the PFLD model on the PFLD meter dataset. The PFLD model is presented in the paper PFLD: A Practical Facial Landmark Detector.
Prepare Datasets
SSCMA uses Custom Meter Datasets by default to train the PFLD model, please refer to the following steps to complete the preparation of datasets.
-
Please refer to Internet Datasets - SSCMA - Custom Meter Dataset to download and unpack the dataset.
-
Remember its folder path (e.g.
datasets\meter) of the unpacked datasets, you may need to use this folder path later.
Choose a Configuration
We will choose a appropriate configuration file depending on the type of training task we need to perform, which we have already introduced in Config, for a brief description of the functions, structure, and principles of the configuration file.
For the meter PFLD model example, we use pfld_mbv2n_112.py as the configuration file, which is located in the folder under the SSCMA root directory configs/pfld and its additionally inherits the default_runtime_pose.py configuration file.
For beginners, we recommend to pay attention to the data_root and epochs parameters in this configuration file at first.
pfld_mbv2n_112.py
_base_='../_base_/default_runtime_pose.py'
num_classes=1
model=dict(type='PFLD',
backbone=dict(type='PfldMobileNetV2',
inchannel=3,
layer1=[16, 16, 16, 16, 16],
layer2=[32, 32, 32, 32, 32, 32],
out_channel=16),
head=dict(type='PFLDhead',
num_point=num_classes,
input_channel=16,
loss_cfg=dict(type='L1Loss')))
# dataset settings
dataset_type='MeterData'
data_root=''
height=112
width=112
batch_size=32
workers=4
train_pipeline=[
dict(type="Resize", height=height, width=width, interpolation=0),
dict(type='ColorJitter', brightness=0.3, p=0.5),
dict(type='GaussNoise'),
dict(type='MedianBlur', blur_limit=3, p=0.3),
dict(type='HorizontalFlip'),
dict(type='VerticalFlip'),
dict(type='Rotate'),
dict(type='Affine', translate_percent=[0.05, 0.1], p=0.6)
]
val_pipeline=[dict(type="Resize", height=height, width=width)]
train_dataloader=dict(
batch_size=32,
num_workers=2,
persistent_workers=True,
drop_last=False,
collate_fn=dict(type='default_collate'),
sampler=dict(type='DefaultSampler', shuffle=True, round_up=False),
dataset=dict(type=dataset_type,
data_root=data_root,
index_file=r'train/annotations.txt',
pipeline=train_pipeline,
test_mode=False),
)
val_dataloader=dict(
batch_size=1,
num_workers=1,
persistent_workers=True,
drop_last=False,
collate_fn=dict(type='default_collate'),
sampler=dict(type='DefaultSampler', shuffle=False, round_up=False),
dataset=dict(type=dataset_type,
data_root=data_root,
index_file=r'val/annotations.txt',
pipeline=val_pipeline,
test_mode=True),
)
test_dataloader=val_dataloader
lr=0.0001
epochs=300
evaluation=dict(save_best='loss')
optim_wrapper=dict(
optimizer=dict(type='Adam', lr=lr, betas=(0.9, 0.99), weight_decay=1e-6))
optimizer_config=dict(grad_clip=dict(max_norm=35, norm_type=2))
val_evaluator=dict(type='PointMetric')
test_evaluator=val_evaluator
find_unused_parameters=True
train_cfg=dict(by_epoch=True, max_epochs=500)
# learning policy
param_scheduler=[
dict(type='LinearLR', begin=0, end=500, start_factor=0.001,
by_epoch=False), # warm-up
dict(type='MultiStepLR',
begin=1,
end=500,
milestones=[350, 400, 450, 490],
gamma=0.1,
by_epoch=True)
]
Training Model
Training the model requires using our previously configured SSCMA working environment, if you follow our Installation guide using Conda to install SSCMA in a virtual environment named sscma, please first make sure that you are currently in the virtual environment.
Then, in the SSCMA project root directory, we execute the following command to train an end-to-end meter PFLD model.
python3 tools/train.py \
configs/pfld/pfld_mbv2n_112.py \
--cfg-options \
data_root='datasets/meter' \
epochs=50
During training, the model weights and related log information are saved to the path work_dirs/pfld_mbv2n_112 by default, and you can use tools such as TensorBoard to monitor for training.
tensorboard --logdir work_dirs/pfld_mbv2n_112
After the training is completed, the path of the latest FOMO model weights file is saved in the work_dirs/pfld_mbv2n_112/last_checkpoint file. Please take care of the path of the weight file, as it is needed when converting the model to other formats.
If you have a virtual environment configured but not activated, you can activate it with the following command.
conda activate sscma
Testing and Evaluation
Testing
After have finished training the PFLD model, you can specify specific weights and test the model using the following command.
python3 tools/inference.py \
configs/pfld/pfld_mbv2n_112.py \
"$(cat work_dirs/pfld_mbv2n_112/last_checkpoint)" \
--cfg-options \
data_root='datasets/meter'
If you want a real-time preview while testing, you can append a parameter --show to the test command to show the predicted results. For more optional parameters, please refer to the source code tools/test.py.
Evaluation
In order to further test and evaluate the model on a realistic edge computing device, you need to export the model. In the process of exporting the model, SSCMA will do some optimization on the model, such as model pruning, distillation, etc. You can refer to the Export section to learn more about how to export models.
Deployment
After exporting the model, you can deploy the model to the edge computing device for testing and evaluation. You can refer to the Deploy section to learn more about how to deploy models.