Skip to main content

ODYSSEY Getting Started

Please check with the latest version: https://wiki.seeedstudio.com/ODYSSEY-X86J4105/

The ODYSSEY - X86J4105, is based on Intel Celeron J4105, a Quad-Core 1.5GHz CPU that bursts up to 2.5GHz. It has all the great features that a standard Computer needs, including an 8GB LPDDR4 RAM, 64GB eMMC Storage(optional), onboard Wi-Fi/BLE, Dual Gigabit Ethernet Ports, Audio Input and Output, USB Ports, HDMI, SATA Connectors, PCIe, etc.

Key Features

  • Intel® Celeron® J4105, Quad-Core 1.5-2.5GHZ
  • Dual-Band Frequency 2.5GHz/5GHz WiFi/ Bluetooth 5.0
  • Intel® UHD Graphics 600
  • Dual Gigabit Ethernet
  • Integrated Arduino Coprocessor ATSAMD21 ARM® Cortex®-M0+
  • Raspberry Pi 40-Pin Compatible
  • 2 x M.2 PCIe (B Key and M Key)
  • Pre-installed with Windows 10 Enterprise
  • Compatible with Grove Ecosystem

Hardware Specifications

ComponentsODYSSEY - X86J4105
ProcessorIntel® Celeron® J4105 (Frequency: 1.5 - 2.5GHz)
CoprocessorMicrochip® ATSAMD21G18 32-Bit ARM® Cortex® M0+
GraphicsIntel® UHD Graphics 600 (Frequency: 250 – 750MHz)
MemoryLPDDR4 8GB
Storage64GB eMMC V5.1
WirelessWi-Fi 802.11 a/b/g/n/ac @ 2.4/5 GHz HT160 & Bluetooth® 5.0
NetworkingIntel® I211AT PCIe Gigabit LAN
AudioMicrophone + headphone Combo Connector
Headers28-pin header from SAMD21G18 & 40-pin header compatible with Raspberry Pi
USBUSB 2.0 Type-A x2, USB 3.1 Type-A x1, USB 3.1 Type-C x1
Video InterfacesHDMI2.0a: Up to 4096x2160 @ 60Hz 24bpp / DP1.2a: Up to 4096x2160 @60Hz 24bpp
Expansion SlotsM.2(Key B, 2242/2280): SATA III, USB2.0, UIM; M.2 (Key M, 2242/2280): PCIe 2.0 ×4; Micro SD card Socket; SIM Card Socket; SATA III
RTCJST 1.0 CR2032 3V
TPMBuilt-in TPM (2.0)
Power ConnectorDC Jack 5.5/2.1mm or Type-C PD
Power Supply (for bare board)
DC Jack Input: Min:12V @ 300mA - 1.2A, Max:19V @ 200mA - 0.7A
Type-C Input: Min: 15V @ 0.27A, Max:15V @ 0.93A
Dimensions110x110mm
CertificationsFCC, CE

!!!Note If you are using 3.5inch HDD drives with the ODYSSEY – X86J4105, make sure to use a DC power supply of 12V@2A or Type-C power supply of 15V@2A.

!!!Note You can power the X86 using a power bank, but you need to make sure to use a power bank with USB PD protocol and connect via USB C. Also, you can seamlessly switch between USB C power and DC power with no issue.

Hardware Overview

Pinout Diagram

Quick Start with ODYSSEY - X86J4105

Hardware Required

  1. ODYSSEY - X86J4105

  2. Power Adapter(provided)

  3. External monitor

  4. HDMI cable

  5. Keyboard and Mouse

Attaching External Storage

For 64 GB EMMC storage version of the ODYSSEY - X86J4105, you can skip this step. However, if you need more storage for your needs, feel free to follow this step.

There are 4 methods of adding storage for ODYSSEY - X86J4105, but only 3 methods support installing the operating system(M.2 SATA, M.2 PCIE and SATA), and the Micro SD card slot can only be used as external storage.

  • Method 1 - M.2 PCIE Connector

  • Method 2 - M.2 SATA Connector

  • Method 3 - SATA Connector

  • Method 4 - Micro SD Card Slot

Installing the Operating System

ODYSSEY - X86J4105 supports both Windows and Linux operating system.

  • For Non-EMMC version, attach extenal storage following previous steps, and install your desired operating system through a bootable USB drive.

  • For EMMC version, Windows 10 Enterprise is pre-installed.

Step 1

Connect bootable USB drive into one of the USB ports on ODYSSEY - X86J4105.

Note: please visit Creating Bootable USB and Installing OS for more information about creating a bootable USB Drive.

Step 2

Press the power button and keep pressing the F7 key on the keyboard until the Boot Manager screen appears.

Step 3

Select the connected USB Drive as the 1st boot drive and press Enter.

Step 4

Follow the instructions on the installation to complete installing the operating system.

Note: To access the BIOS setup, keep pressing DEL key when booting up.

Connecting Antennas

Connect two antennas into the two sockets on the board.

Note: One Antenna is for Wi-Fi and Bluetooth, and the other is for strong 5G Connectivity.

Adding 4G Cellular Connectivity

For 4G Cellular connectivity, insert a standard SIM card into the SIM card slot of the board.

Insert a PCIE 4G Module

Note: This module is a must have if you want to use the connected SIM Card.

Connecting to Display

There are 2 methods for display:

Method 1 - HDMI Port

Method 2 - DP over USB-C Port

Connecting to Keyboard and Mouse

Connect Keyboard and Mouse through USB ports

Powering up

There are two ways to power up the ODYSSEY - X86J4105:

Method 1

The simplest way is to use the 12V/2A power adaptor included in the package, and connect to the DC jack of ODYSSEY - X86J4105.

Method 2

You can also power the ODYSSEY - X86J4105 through the USB-C port with 12V input. Furthermore, if your Monitor supports USB-PD, you are able to power and display ODYSSEY - X86J4105 using only 1 cable!

Performance Stats

Wi-Fi Connecitivity

Bluetooth Connecitivity

Operating as Computer

  • Browsing and watch videos on Youtube

  • Playing Google T-Rex!

Using the Arduino Core (ATSAMD21G18) in Windows

The ODYSSEY - X86J4105 is built with Arduino Core(ATSAMD21G18) which provides more functionality to the board, and to use it, simply download the Arduino IDE, and Install the Windows version.

  1. Click File->Preferences->Additional Boards Manager URL: and Copy the following link into it https://files.seeedstudio.com/arduino/package_seeeduino_boards_index.json.

  2. Click Tools->Board:->Boards Manager..., and Boards Manager will appear. Search and install the Seeeduino Zero board library.

  1. Select the right Port and Board before uploading.
  • Port -> COMxx(Seeeduno Zero)

  • Board -> Seeeduino Zero

Feel free to explore your creativity with ODYSSEY - X86J4105!

Using the Arduino Core (ATSAMD21G18) in Linux OS

If you have installed Linux OS, Download the Linux version of Arduino IDE and install the IDE as follow:

Installing Arduino IDE

  1. Open terminal and goto Downloads
cd ~/Downloads
  1. Use tar command to unzip the downloaded file
tar -xvf arduino -1.8.10-linux64.tar.xz
  1. Move the file to opt
sudo mv arduino-1.8.10 /opt
  1. Install Arduino IDE and make a Desktop shortcut
cd /opt/arduino-1.8.10/ && chmod +x install.sh && ./install.sh
  1. Allow permissions for Arduino to upload
cd /opt/arduino-1.8.10 && ./arduino-linux-setup.sh

Installing Board Libraries

  1. Click File->Preferences->Additional Boards Manager URL: and Copy the following link into it https://files.seeedstudio.com/arduino/package_seeeduino_boards_index.json.

  2. Click Tools->Board:->Boards Manager..., and Boards Manager will appear. Search and install the Seeeduino Zero board library.

  1. Select the right Port and Board before uploading.
  • Port -> ttyACM0(Seeeduno Zero)

  • Board -> Seeeduino Zero

FAQs

How can I access the BIOS setup

Press the Power Button and keep pressing DEL key until you see the BIOS Setup.

Arduino IDE doesn't recognize the onboard microcontroller

Add a jumper wire between RST Pin and GND Pin on the 4-Pin header (to the left of SAMD21's 28 pins) to reset the AMSAMDG21.

I cannot connect Wi-Fi and Bluetooth

Check BIOS settings and enable Wi-Fi and Bluetooth from BIOS

ODYSSEY - X86J4105 doesn't power up

Maker sure you use the 12V/2A power adapter provided in the box and check connection.

Different status of Power button of ODYSSEY - X86J4105

It has the same power button state as other computers:

  • Short Press(While it's off) -> Turn on

  • Short Press(While it's on) -> Sleep

  • Long Press(While it's on) -> Force shutdown

Is the built-in fan controllable

Currently the fan is controlled by BIOS, and not controlled by user. The fan speed is set according to the CPU temperature. Check Chipset -> FAN Contorl in the BIOS setup screen for more information.

How to upgrade BIOS

For the instructions of upgrading BIOS, please check the Installing OS section.

How to set the ODYSSEY - X86J4105 to auto power on when power plugged in

This also need to be configured in the BIOS. Enter BIOS settings by pressing DEL key. Navigate to Chipset -> Restore on AC Power Loss and change settings to Last State.

Fan is not turning on

Odyssey fan is controlled by Embedded controller (EC) which role as initialize the device before system is up. The temperature in BIOS is detected by EC and the temperature sensor place close to the intel CPU which do not have the sensor pin. In another word, the temperature is not the CPU's direct value, maybe 5 degrees centigrade error. What you saw the temperature value in system is feedback by CPU internal, temperature in BIOS screen feedback by EC, fan run or stop according the EC value.

  • EC detect value (BIOS screen) and fan speed table like this:

Disable fan state: stop

Normal fan state: less than 40°C–stop,45-50°C–50%,50-60℃–60%,above 60℃–80%

Positive fan state: less than 40°C–stop,45-50°C–70%,50-60℃–80%,above 60℃–100%

Fan Pinout

Some of you may need to know the 5V PWM fan pinout in order to DIY/replace to your own fans. Odyssey has a 5V PWM pin for the fan with a smaller header than the usual 5V pin header. You may need to replace the header in order to fit in.

Re-Installing the Original Windows

The eMMC versions of ODYSSEY-X86 will have Windows 10 pre-installed into the device. If you install another OS and wanting to go back to the original Windows 10 please check here:

  • Original Windows 10 Image

    • This image supports Auto Flash. Simply download the above image and unzip the files and place in the root location of a USB drive.

    • Plug in the USB drive to ODYSSEY-X86 and boot up from the USB Drive. This will auto flash the Original Windows 10 Image back in the eMMC.

Does Odyssey have TPM?

Odyssey has FTPM integrated in the processor.

Does Odyssey board have Boot Guard for Secure Boot?

Yes, you can enable the "Security Boot" option in the BIOS. When this is enabled, the BIOS will disable booting from unauthenticated devices.

Why is GPIO still working after Odyssey is Shut down?

To set this up, you need to update to the latest BIOS we provide. In the latest BIOS, you can change enable to disable here to turn off both GPIO and ODYSSEY.

Resources

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...