Skip to main content

Weekly Wiki

Greetings​

This is Seraphina in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is December 11th and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

LinkStar H28K​

The LinkStar H28K is equipped with a quad-core Cortex-A53 RK3528 chip with two gigabit Ethernet ports, using PCIE/RGMII gigabit, and non-relay network ports for more stable speeds.It's a real pocket design, just 5.5x6.5cm.

In this wiki, we will show you the hardware overview.
H28K Introduction

In this wiki we will show you how to install operating system with TF card or eMMC.
Install Operating System - H28K

mmWave for XIAO to Home Assistant via Bluetooth​

24GHz mmWave Sensor for XIAO - Human Static Presence is a expansion board for Seeed Studio XIAO series. It is an antenna-integrated, high-sensitivity mmwave sensor that is based on the FMCW principle. Combined with sensor signal processing and accurate human body sensing algorithms, it can identify human bodies in motion and stationary states.

This chapter primarily introduces how the 24GHz mmWave Sensor for XIAO connects to the HA via Bluetooth. For detailed functional features of the 24GHz mmWave Sensor for XIAO, you can refer to here.

Existed Wiki Updated​

How to batch configure - SenseCAP T1000 FAQ​

We have updated the method about how to batch configure for SenseCAP T1000

Run the code of Object Detection with reTerminal and Pi camera in BookWorm OS​

We have updated the method about how to run the code of the Object Detection with reTerminal and Pi camera in BookWorm OS.

The Efforts of Contributor✨​

Past Weekly wiki​

Loading Comments...