Skip to main content

Weekly Wiki

Greetings!​

This is Matthew in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

Today is May 22nd and a brand new week has begun! Check out what Seeed did last week!

Latest Wiki Launched​

Seeed Studio XIAO nRF52840 on Sidewalk​

Amazon Sidewalk is a wireless network protocol developed by Amazon that allows compatible devices to share a small portion of their internet bandwidth with nearby devices. The goal of Sidewalk is to create a larger, more resilient network that can extend the range of smart home devices and improve their connectivity.

reTerminal DM Getting Started​

reTerminal DM is A 10.1" open-source industrial HMI - an Integrated Device Master to unify data flow and manage the onsite device.

SenseCAP Indicator Native Firmware​

The SenseCAP Indicator D1S and D1Pro version has the built-in tVOC and CO2 sensors, and an external Grove TH sensor for accurate data reading. The SenseCAP native firmware provides air quality detector UI to show the sensor data.

OpenAI x SenseCAP Indicator​

Sensecap Indicator integrates two popular models ChatGPT and DALL·E via API, empowering users to quickly experience and enjoy the charm of AI!

You can refer to the links below for more help:

SenseCAP Indicator - Dive into the Hardware​

This chapter will provide detailed information about ESP32 and RP2040 of SenseCAP Indicator, including their functions and usage. It covers include programming, interfacing with sensors, and communicating with other devices,etc.

SenseCAP Indicator - How to Create your own UI​

LvGL is an open-source graphics library providing everything you need to create an embedded GUI with easy-to-use graphical elements, beautiful visual effects, and a low memory footprint.

SenseCAP Indicator - Develop with ESP32-S3​

SenseCAP Indicator - Develop with RP2040​

Grove - NFC (ST25DV64)​

Grove - NFC (ST25DV64) is an innovative and versatile NFC/RFID tag board based on the advanced ST25DV64K chip from STMicroelectronics. This dynamic chip supports ISO/IEC 15693 and NFC Forum Type 5 tag standards, making it compatible with a wide array of NFC-enabled devices.

reTerminal and Pi camera modules​

This is the wiki that helps you to install the necessary drivers and related components to ensure proper functionality of the PiCam on the fresh Raspberry Pi OS installation.

Existed Wiki Updated​

BootLoader Mode on Seeed Studio XIAO ESP32S3​

We have upgraded the bootloader mode for XIAO ESP32S3.

Past Weekly wiki​

Loading Comments...