Skip to main content

Weekly Wiki

Greetings​

This is Matthew in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

Today is July 24th and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Deploy YOLOv8 on NVIDIA Jetson using TensorRT​

This wiki guide explains how to deploy a YOLOv8 model into NVIDIA Jetson Platform and perform inference using TensorRT. Here we use TensorRT to maximize the inference performance on the Jetson platform.

Different computer vision tasks will be introduced here such as:

  • Object Detection
  • Image Segmentation
  • Image Classification
  • Pose Estimation
  • Object Tracking

EdgeBox RPi 200 Balena OS Setup​

Balena is an Internet of Things (IoT) platform designed to help developers build, deploy, and manage IoT applications across a fleet of devices. It supports a wide range of device architectures and includes features for containerized application deployment, making it possible to easily update your IoT software and HostOS, fix bugs and introduce new features on your IoT applications.

TinyML Topic Page​

TinyML is a field of study in Machine Learning and Embedded Systems that explores machine learning on small, low-powered microcontrollers, enabling secure, low-latency, low-power and low-bandwidth machine learning inferencing on edge devices. If you're excited about TinyML but not sure where to start, our one-stop guide is perfect for you. This guide provides an overview of what TinyML is, the opportunities it offers, and step-by-step instructions on how to get started. Join this exciting field and start your TinyML journey today!

Existed Wiki Updated​

Add IMX219 and IMX477 camera usages to reComputer Industrial J20 Series​

Add IMX219 and IMX477 camera usages to reComputer Industrial J20 Series

Add IMX219 and IMX477 camera usages to reComputer Industrial J40, J30 Series​

Add IMX219 and IMX477 camera usages to reComputer Industrial J40, J30 Series

Add 4G module usage on reterminal DM​

Add 4G module usage on reterminal DM

pir

Update sensecraft edge OS download link and add tips about 32-bit driver

XIAO Canbus Expansion board​

Thanks for the notices, we have changed pin promopt to the correct ones:

pir

  1. GND
  2. CAN-H
  3. CAN-L
  4. LED Indicators for RX/TX
  5. SN65NVD230

Add reTerminal DM DI/DO wiring samples​

Upload PCB Source file for reTermianl Bridge​

Add Wio 1110 libraries Installation steps​

The Efforts of Contributor​

Past Weekly wiki​

Loading Comments...