Skip to main content

Weekly Wiki ✨

Greetings​

This is Matthew in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is August 21st and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

SenseCAP T1000 Tracker​

SenseCAP T1000 is a compact LoRaWAN® tracker that utilizes GNSS/Wi-Fi/Bluetooth for precise indoor & outdoor location tracking. It boasts self-geo-adaptive capabilities, local data storage, and an impressive months of battery life. Additionally, it is equipped with temperature, light, and motion sensors, making it ideal for a variety of location-based applications.

SenseCAP Indicator x LoRa Application Development​

We have published a wiki about using SenseCAP Indicator for peer-to-peer data transfer under the LoRa network.

This demonstration showcases how to establish a basic LoRa communication between the SenseCAP Indicator and the XIAO board using the Wio-E5 as an intermediary. The SenseCAP Indicator retrieves sensor data from the XIAO, which is then transmitted via Wio-E5. The transmitted payload is subsequently received by the SenseCAP Indicator, which deciphers and outputs. the result and displays the data on its screen.

Existed Wiki Updated​

Andanced OV5640 camera Sensor for XIAO ESP32S3 Sense​

We now have a new fully XIAO ESP32S3 Sense-compatible powerful camera, the OV5640, on our shelves, and if you purchase it, you can replace the camera to use it.

Update Indicator flash firmware​

We have updated the firmware for SenseCAP Indicator(both ESP32S3 and RP2040 chip)

Flash TinyML model on XIAO ESP32S3 Sense using SenseCraft Model Assistant function​

We flash the SenseCraft Model Assistant program in advance for all XIAO ESP32S3 Sense participating in the Workshop, and pre-set the model for face recognition. Simply connect the XIAO ESP32S3 Sense to your PC via a data cable to instantly display face recognition.

The Efforts of Contributor✨​

MicroPython for ESP32C3​

Thanks our contributor - Zachary for adding a wiki page about connecting XIAO ESP32C3 and Seeed Studio Expansion Board to build a Wi-Fi signal strength tracker, which proves invaluable when establishing a high-speed, high-quality family network, programming with MicroPython.

Thanks our contributor for organizing tinyML workshop page​

Thanks our contributor - Salman for organizing tinyML workshop page to make the course more logical.

Past Weekly wiki​

Loading Comments...