Skip to main content

Weekly Wiki

Greetings​

This is Matthew in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is September 25th and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Object detection on reTerminal DM using Edge Impulse​

In today's digital landscape, the integration of edge AI and IoT (Internet of Things) technologies has opened up exciting possibilities for developers and enthusiasts. One such powerful platform that simplifies the creation of machine learning models for edge devices is Edge Impulse. In this step-by-step guide, we will walk you through the process of installing Edge Impulse on your reTerminal DM device and creating a local object detection solution.

SenseCAP Hotspot APP​

SenseCAP Hotspot APP is a powerful APP mainly used for data visualization and remote device management for SenseCAP MX Hotspot.

Setup Your Toolchain(Arduino on Wio Tracker)​

The Wio Tracker 1110 Dev Board leverages Arduino to enhance your coding experience, before you start development, need to set up your toolchain first.

reServer Industrial​

reServer Industrial features 2x 2.5" SATA HDD/ SSD drive bays to easily store hundreds of local video footages in a video analytics application. Also it enables multiple connectivity options including 5 RJ-45 Ethernet ports, 1 RS232/422/485, 4x Isolated DI/DO, 1x CAN, 4* USB3.1. Fanless design with versatile mounting options allows deployment from -20 to 60 ℃, which is ideal for more harsh environments and heavier loads.

IO Expander for XIAO​

The Wio Tracker 1110 Dev Board is based on Wio-WM1110 Wireless Module and integrates Semtech's LR1110 LoRa® transceiver and a multi-purpose radio front-end for geolocation, it's a user-friendly, LoRa-based tracking development platform.

FAQ for SenseCAP Tracker​

These are the general questions for SenseCAP Tracker.

Existed Wiki Updated​

Seeed Studio XIAO nRF52840 on Amazon Sidewalk​

We have updated the contents regarding Sidewalk on Seeed Studio XIAO nRF52840, certificated by AWS official.

The Efforts of Contributor✨​

Past Weekly wiki​

Loading Comments...