Skip to main content

Weekly Wiki

Greetings​

This is Seraphina in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is January 15th and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Which LoRaWAN Network Should I Select​

In the rapidly expanding realm of IoT (Internet of Things), LoRaWAN networks have surged in popularity, offering extended range and low-power communication capabilities for diverse IoT applications. Lately, we've been inundated with inquiries: "Which LoRaWAN network should I choose for my specific project?"

In this article, we’ll take you through the components of a LoRaWAN network, explore the differences between public and private LoRaWAN networks, and offer references to help you make an informed decision.

pir

Use Infineon Wi-Fi Module on reComputer​

In this document, you will learn how to use Infineon’s Wi-Fi 6/6E module on reComputer J4012.

Extend Home Assistant with LoRaWAN device (XIAO-ESP32-S3)​

Home Assistant is an open source smart home platform system, and user can easily connect their own Internet of Things devices to the system for unified management. However, the main special point of the Home Assistant is not just to realize the view of various sensing devices, but to realize the automatic linkage of cross-platform device, only such a smart home platform is enough to have vitality.

pir

Connect Grove Vision AI V2 to Home Assistant​

Integrating Grove Vision AI V2 into Home Assistant can elevate your smart home setup by adding advanced visual sensing capabilities. This integration allows for real-time environmental analysis and customized automation, making your home environment more intelligent and responsive.

External Camera supported Overview​

Grove Vision AI V2 features a standard CSI interface and is compatible with Raspberry Pi cameras. To explore the full potential of the Grove Vision AI V2 you may want a CSI camera separately, we recommend the OV5647-62 FOV Camera Module for Raspberry Pi.

Local Voice Chatbot​

As artificial intelligence technology rapidly evolves, voice interaction has become an increasingly important mode of human-computer interaction. Especially in fields like smart homes, personal assistants, and customer service support, the demand for voice chatbots is growing significantly. However, most existing voice chatbots rely on cloud computing services, which raises concerns about data privacy and network latency to some extent.

This project aims to address these issues by building a locally-operated voice chatbot. Utilizing Nvidia Riva and Meta Llama2, we have developed a secure, private, and fast-responding voice interaction system.

Grove Offline Voice Recognition sensor​

Grove - Offline Voice recognition Module is apt for low power pure-offline voice recognition, based on VC-02 module. It has up to 150 pre-programmed commands that can be used to control your smart appliances. It features an identification time less than 100ms, in a compact form factor of 18mm * 17mm. The module can communicate through the UART peripheral and provide unique Hex Code to each recognised command.

Existed Wiki Updated​

Run R23.5 OpenWrt​

We updated the latest version of OpenWrt for Rerouter, the R23.5 version. If you want to use the latest version of OpenWrt, you can follow this wiki.

Getting Started with MediaPipe on reTerminal​

We've updated the Grove MediaPipe usage on reTerminal.

Seeed Studio XIAO Series Compatible Accessories​

We've added the XIAO Series Compatible Accessories to our Seeed Studio XIAO INTRODUCION.

The Efforts of Contributor​

Past Weekly wiki​

Loading Comments...