Skip to main content

Weekly Wiki

Greetings​

This is Seraphina in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is May 27th and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Matter Development Framework Overview​

Embark on an illuminating journey into the world of Matter development with our comprehensive tutorial. Through the lens of the quintessential light example, we'll shed light on the fundamental concepts and knowledge that form the bedrock of Matter development. From clusters and attributes to commands and beyond, this tutorial will equip you with the tools to navigate the Matter framework with confidence. Get ready to flip the switch on your Matter development skills and let's dive into the brilliant world of connected devices!

Grove - MP3 v4.0​

This MP3 module with an Arduino can be turned into your multi-format music player! It's a Music module based on WT2605CX high-quality audio chip, which has better performance then MP3 V3 and supports Grove interface, Speaker JST interface, 3.5mm audio jack and SD card, supporting SPI-Flash, TF card, and USB flash disk.

Building a crowd density based on Grove Vision AI V2 and Home Assistant​

Throughout this tutorial, we will guide you through the step-by-step process of setting up the hardware, configuring the software, and integrating the system with Home Assistant. Whether you are a beginner or an experienced user, this tutorial aims to provide you with the knowledge and tools necessary to create a sophisticated environment detection system that enhances your smart home experience.

Real-time IoT Data Processing Node Powered By Apache Kafka​

Our cutting-edge processing node, Kafka-ESP32, combines the power of Apache Kafka and ESP32C6 microcontrollers to deliver an efficient solution for handling IoT data streams. By using the XIAO ESP32C6 with the DHT20 environmental sensor, data is collected and seamlessly sent to Apache Kafka via the ESP32C6. Kafka's high-throughput, low-latency messaging capabilities enable real-time data processing and analysis, while its distributed architecture allows for effortless scalability. Kafka-ESP32 empowers you to develop custom applications and integrations, revolutionizing the way you manage and utilize your IoT assets in today's data-driven landscape.

Existed Wiki Updated​

Flash JetPack OS to A603 Carrier Board​

We have updated the method for flashing Jetpack 6 on the A603 carrier board.

At the same time, we have added a driver package for the A603 based on JP5.1.2, adapted to the IMX477 camera: Use IMX477 Camera with A603 Jetson Carrier Board

The Efforts of Contributor​

Past Weekly wiki​

Loading Comments...