Skip to main content

Weekly Wiki

Greetings​

This is Seraphina in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is June 3rd and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

[Grove - ADC for Load Cell (HX711)](https://wiki.seeedstudio.com/grove_adc_for_load_cell_hx711 /)​

The Grove - ADC for Load Cell (HX711) is a 24-bit A/D converter designed specifically for the load cell. It contains an on-chip low noise programmable amplifier with an optional gain of 32, 64 and 128. The HX711 chip integrates a regulated power supply, an on-chip clock oscillator, and other peripheral circuits, which have the advantages of high integration, fast response, and strong anti-interference.

Grove Vision AI V2 Notifies You Via Telegram​

This project combines the XIAO ESP32S3 and Grove Vision AI V2 to create a compact person detection device. The V2 module, equipped with a person detection model, identifies human presence and sends the results to the ESP32S3. The microcontroller then processes the information and forwards the detection alerts to a designated Telegram account, providing real-time notifications whenever a person is detected in the monitored area.

Quick start with Zigbee on XIAO ESP32C6​

In this tutorial, we will embark on a journey to explore Zigbee application development using the XIAO ESP32C6 development board. The XIAO ESP32C6 is a compact yet powerful board that features the ESP32-C6 chip, which offers integrated Wi-Fi and Bluetooth Low Energy (BLE) connectivity. By leveraging the ESP Zigbee SDK, we can harness the full potential of the XIAO ESP32C6 and extend its capabilities to include Zigbee functionality.

The Efforts of Contributor​

Past Weekly wiki​

Loading Comments...