Skip to main content

Weekly Wiki

Greetings​

This is Seraphina in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is June 10th and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

EdgeEdge Box RPi 200 with Node Red and BACnet TCP​

BACnet IP (Building Automation and Control Network over IP) is a communication protocol designed for managing and automating building systems. It enables devices from different manufacturers to interoperate seamlessly over standard IP networks, enhancing system integration and flexibility. The primary advantages of BACnet IP in Building Management Systems (BMS) include improved scalability, easier installation and maintenance, and the ability to leverage existing network infrastructure. BACnet IP also supports real-time data exchange, facilitating better monitoring and control of building systems. This results in increased energy efficiency, reduced operational costs, and enhanced occupant comfort and safety.

Edge Box RPi 200 with Node Red and Modbus RS485​

Modbus RTU (Remote Terminal Unit) is a popular protocol in industrial automation for connecting devices like sensors and controllers over serial communication lines. Known for its simplicity and reliability, it is widely used in monitoring and controlling industrial processes. The Edge Box RPi 200, an industrial IoT gateway based on the Raspberry Pi, enables integration of Modbus RTU devices with modern networks. Using Node-RED, a flow-based development tool, this wiki guides users in setting up Modbus RTU communication with the Edge Box RPi 200. It highlights applications such as energy management, environmental monitoring, and process control. This resource offers a quick and practical approach to leveraging Modbus RTU in various industrial scenarios.

The Efforts of Contributor✨​

XIAO nRF52840(Sense) Zephyr Application​

Thanks our contributor Tim to create the tutorial for XIAO nRF52840(Sense) With Zephyr(RTOS)

This wiki covers Zephyr support for the Seeed Studio XIAO nRF52840(Sense). With the assistance of this guide you will be able to utilize the feature set available to the board.

Past Weekly wiki​

Click here
Loading Comments...