Skip to main content

Weekly Wiki

Greetings​

This is Seraphina in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is June 17th and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

SenseCAP T1000 tracker - Wialon Integrated​

Wialon is the fleet management software platform for GPS monitoring and IoT which tracks over 3,7 million mobile and stationary units in 150+ countries of the world and consists of more than 2,500 partner companies, 700 hardware manufacturers, hundreds of Wialon-based solution developers.

The content of this chapter will guide users how to connect the SenseCAP T1000 Tracker to Wialon platform.

pir

Edge Box RPi 200 with Node Red and InfluxDB​

Deploying InfluxDB on an Edgebox RPi 200, a Raspberry Pi-powered edge controller, enables robust time-series data collection and analysis at the edge of your network. This setup is ideal for IoT applications, providing real-time insights and monitoring capabilities. By leveraging the lightweight yet powerful InfluxDB database, you can efficiently manage and analyze sensor data directly on the Edgebox. The following guide outlines the steps to install, configure, and use InfluxDB on your Edgebox RPi 200, ensuring a seamless integration into your data infrastructure

reComputer R1000 with Balena​

balena is an Internet of Things (IoT) platform designed to help developers build, deploy, and manage IoT applications across a fleet of devices. It supports a wide range of device architectures and includes features for containerized application deployment, making it possible to easily update your IoT software and HostOS, fix bugs and introduce new features on your IoT applications. balena provides a unified way to push code updates, manage device configurations and ensure devices run reliably and securely in the field, regardless of their location or network conditions.

pir

Existed Wiki Updated​

J401 carrier board Hardware and Interfaces Usage​

We have updated the tutorial on how to use M.2 Key M, M.2 Key E slot on J401 carrier board.

M.2 Key M

M.2 Key E

Flash JetPack OS to J401 Carrier Board - Updated JetPack 6.0 ​

We have added the JetPack 6.0 image package and updated on how to flash JetPack6.0 on a J401 carrier board.

The Efforts of Contributor✨​

Train and deploy a custom classification model with YOLOv8​

Thanks our contributor Bruno to create the application tutorial for reComputer.

On this guide we will explain how to train and deploy a custom classification model with YOLOv8

Past Weekly wiki​

Click here
Loading Comments...