Skip to main content

Weekly Wiki

Greetings​

This is Seraphina in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is June 24th and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Getting Started with SenseCAP Watcher​

SenseCAP Watcher is an AI watcher to help you monitor anomalies within a space and then take actions. Simply speak to Watcher to give commands, and it will execute your desired tasks when the event occurs.

As a new comer for smart building / smart home system, SenseCAP Watcher is far more intelligent compared to current sensors and actuators. It understands what is happening within the space and then takes actions accordingly.

Meshtastic® Network Introduction​

Meshtastic® is an open source, off-grid, decentralized, mesh network built to run on affordable, low-power devices, it enables you to use inexpensive LoRa radios as a long range off-grid communication platform in areas without existing or reliable communications infrastructure.

pir

recomputer R1000 with Node-Red and BACnet IP​

This tutorial shows the process of using node-red to read BACnet device data on Recomputer R1000 and perform real-time visual display.We used a BACnet device simulator on the W10 PC to simulate the real BACnet device. The recomputer R1000 and the W10 PC were connected to the same router to ensure that they were on the same network segment, and then the data was read and displayed.

Connect N3uron with BACnet on Edgebox RPi 200​

BACnet is a widely adopted protocol in Building Management Systems (BMS) due to its open standard, which allows seamless integration and communication between devices from different manufacturers. Its popularity is also driven by its flexibility, supporting various network configurations and providing robust interoperability. N3uron, a powerful and versatile platform, enhances the capabilities of BACnet by enabling efficient data acquisition and management. Using BACnet TCP with the YABE Room Simulator, users can simulate and visualize BACnet devices, facilitating testing and development. This combination ensures a comprehensive and effective approach to BMS solutions, leveraging the strengths of each technology.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...