Skip to main content

Weekly Wiki

Greetings​

This is Seraphina in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is July 1st and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

reTerminal DM with Node Red and Modbus TCP​

Modbus is a widely used communication protocol in industrial environments, known for its simplicity and robustness. Modbus RTU (Remote Terminal Unit) is a serial communication protocol that operates over RS-232 or RS-485 physical layers. It uses a compact, binary representation of the data, making it efficient for transmission over long distances and in noisy environments. Modbus TCP, on the other hand, extends the protocol to Ethernet networks, encapsulating Modbus frames within TCP/IP packets. This allows for faster communication speeds and the integration of Modbus with modern IT infrastructure. Both versions are favored in industrial settings due to their reliability, ease of implementation, and ability to facilitate communication between a wide variety of devices and systems, such as PLCs, sensors, and SCADA systems.

reTerminal DM with Node Red and BACnet TCP​

BACnet IP (Building Automation and Control Network over IP) is a communication protocol designed for managing and automating building systems. It enables devices from different manufacturers to interoperate seamlessly over standard IP networks, enhancing system integration and flexibility. The primary advantages of BACnet IP in Building Management Systems (BMS) include improved scalability, easier installation and maintenance, and the ability to leverage existing network infrastructure. BACnet IP also supports real-time data exchange, facilitating better monitoring and control of building systems. This results in increased energy efficiency, reduced operational costs, and enhanced occupant comfort and safety.

reTerminal DM with Node Red and InfluxDB​

Deploying InfluxDB on an reTerminal DM, a Raspberry Pi-powered HMI, enables robust time-series data collection and analysis at the edge of your network. This setup is ideal for IoT applications, providing real-time insights and monitoring capabilities. By leveraging the lightweight yet powerful InfluxDB database, you can efficiently manage and analyze sensor data directly on the reTerminal DM. The following guide outlines the steps to install, configure, and use InfluxDB on your reTerminal DM, ensuring a seamless integration into your data infrastructure.

reTerminal DM with Grafana for IoT Dash Board​

Grafana is an open-source visualization and analytics software that enables you to query, visualize, alert on, and explore your metrics, logs, and traces from any storage location. It offers tools to transform your time-series database (TSDB) data into insightful graphs and visualizations. As a powerful monitoring solution, Grafana helps in making informed decisions, enhancing system performance, and streamlining troubleshooting. In this wiki, we will guide you through the installation of Grafana on a Raspberry Pi-powered reTerminal DM, connect it to an existing InfluxDB database, and create an illustrative dashboard.

reComputer R1000 with fuxa to use modbus RTU/TCP​

FUXA is a web-based Process Visualization (SCADA/HMI/Dashboard) software. With FUXA you can create modern process visualizations with individual designs for your machines and real-time data display.It supports Modbus RTU/TCP, Siemens S7 Protocol, OPC-UA, BACnet IP, MQTT, and other protocols.

This article mainly introduces how to use fuxa for ModbusRTU/TCP communication.

pir

Existed Wiki Updated​

A607 JetPack 6 Compatibility​

We've now updated the method for flashing Jetpack 6 on A607.

NVIDIA® Jetson AGX Orin 32GB H01 JetPack 6 Compatibility​

We've now updated the method for flashing Jetpack 6 on Jetson AGX Orin 32GB H01.

Installation to reTerminal DM Lorawan Module​

We have updated packages installation to reterminal dm lorawan module.

Using Grove Vision AI V2 with AT Commands - Compatibility of different XIAO​

We've added a table of how the Grove Vision AI V2 pairs with the XIAO

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...