Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is August 26th and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Getting Started with reServer J501​

The J501 carrier board is a powerful extension board that supports NVIDIA Jetson AGX Orin modules. It features rich data ports and extension interfaces, completely unleashed the full performance of the AGX Orin module. Also it supports adding GMSL extension to connect up to 8 GMSL cameras.

Getting started with 60GHz mmWave Fall Detection Sensor Kit with XIAO ESP32C6 (MR60FDA2)​

Introducing our advanced mmWave Sensor Modules for XIAO, designed to provide cutting-edge monitoring solutions for both fall detection and heartbeat monitoring. Powered by the robust XIAO ESP32 microcontroller with built-in Wi-Fi and Bluetooth connectivity, these modules offer precise and reliable detection capabilities. Whether you need to monitor falls in real-time or track heartbeats with sensitive accuracy, our modules are equipped with state-of-the-art technology, including customizable RGB LEDs and ambient light sensing. With easy expansion options through Grove GPIO ports, these versatile modules are perfect for a wide range of applications, from smart home integration to healthcare monitoring.

Getting started with 60GHz mmWave Breathing and Heartbeat Detection Sensor Kit with XIAO ESP32C6 (MR60BHA2)​

Introducing our advanced mmWave Sensor Modules for XIAO, designed to provide cutting-edge monitoring solutions for both fall detection and heartbeat monitoring. Powered by the robust XIAO ESP32 microcontroller with built-in Wi-Fi and Bluetooth connectivity, these modules offer precise and reliable detection capabilities. Whether you need to monitor falls in real-time or track heartbeats with sensitive accuracy, our modules are equipped with state-of-the-art technology, including customizable RGB LEDs and ambient light sensing. With easy expansion options through Grove GPIO ports, these versatile modules are perfect for a wide range of applications, from smart home integration to healthcare monitoring.

Send message from Watcher & Node-RED to Open Interpreter​

Open Interpreter is an open-source tool that facilitates interaction between users and their computers by enabling natural language commands to execute code in various programming languages. It acts as a bridge, allowing users to write instructions in plain language, which the interpreter then translates into executable code. This enhances productivity and makes programming more accessible, especially for those who may not be familiar with coding syntax. We will show you how to configure it in following steps.

Build balenaOS for reComputer R1000​

balena is an Internet of Things (IoT) platform designed to help developers build, deploy, and manage IoT applications across a fleet of devices. It supports a wide range of device architectures and includes features for containerized application deployment, making it possible to easily update your IoT software and HostOS, fix bugs and introduce new features on your IoT applications. balena provides a unified way to push code updates, manage device configurations and ensure devices run reliably and securely in the field, regardless of their location or network conditions.

pir

This tutorial will show you how to compile, configure and burn balenaOS for R1000.

SenseCAP T1000 tracker and Thingsboard Integrated​

ThingsBoard is an open-source IoT platform that enables rapid development, management, and scaling of IoT projects. Our goal is to provide the out-of-the-box IoT cloud or on-premises solution that will enable server-side infrastructure for your IoT applications.

The content of this chapter will guide users how to connect the SenseCAP T1000 Tracker to ThingsBoard through TTN.

SenseCraft AI for Watcher Plans and Benefits​

At Watcher, we believe in providing developers with a clear and transparent pricing structure for integrating artificial intelligence into their projects. We understand that every developer has unique requirements, which is why we offer a range of pricing plans designed to cater to various needs and budgets. To help you make an informed decision, we've outlined the key aspects of our pricing model and the specific features included in each plan.

SenseCAP Watcher, is now pre-launched on Kickstarter proudly with the official KS badge of "Project We Love"!

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...