Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is September 2nd and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Connecting Siemens PLCs Using the S7 Protocol with reComputer R1000​

In this article, we'll explore how to use Node-RED, a popular flow-based development tool, on a Raspberry Pi-powered reComputer to interface with Siemens PLCs using the S7 Protocol. This setup allows for efficient and flexible integration of industrial automation systems with modern IoT platforms.

Deploy Frigate On Jetson​

image1

Frigate is an open-source NVR (Network Video Recorder) with Realtime Object Detection for IP cameras. In this guide, we'll walk through the steps to deploy Frigate on an NVIDIA Jetson device. NVIDIA Jetson is an edge AI platform that enables efficient deployment of AI workloads. Combining Frigate with Jetson leverages hardware-accelerated machine learning to efficiently process video streams and detect objects.

XIAO ESP32S3 Sense Sleep Modes​

ESP32 supports two major power saving modes: Light-sleep and Deep-sleep. According to the features used by an application, there are some sub sleep modes. See Sleep Modes for these sleep modes and sub sleep modes. Additionally, there are some power-down options that can be configured to further reduce the power consumption. See Power-down Options for more details.

Raspberry Pi 5 uses PCIe hat/dual hat​

This tutorial mainly introduces the hardware connection configuration of M.2 Hat/dual Hat and how to make the Raspberry Pi boot from the SSD.And introduces two installation methods, with and without casing.

XIAO ESP32C6 with PlatformIO​

PlatformIO is a development platform that integrates many types of development boards and has good scalability. If the platform does not have the type you need, you can manually add the type of development board yourself. The code you write on Arduino can use it, just add the corresponding library

In this wiki , we wiil introduce how to install and run the sample code in PlatformIO

We also created a tutorial for using the XIAO nRF52840 with PlatformIO.

Github Contribution(Pull Request) Guide​

We provide two tutorial documents: Full Steps Pull Request and Quick Pull Request. You can follow the steps in these documents to upload your innovative solution. Thank you for considering contributing to our seeed-studio files!

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...