Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is December 9th, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Configuring Model Output on SenseCraft AI for Grove Vision AI V2​

This wiki article provides a comprehensive guide on how to configure model output settings for the Grove Vision AI V2 device using the SenseCraft AI platform. By following these step-by-step instructions, you will learn how to set up trigger conditions and actions based on the output of your trained model running on the Grove Vision AI V2.

Configuring Model Output and GPIO on SenseCraft AI for XIAO ESP32S3 Sense​

This wiki article provides a step-by-step guide on how to configure model output and GPIO settings for the XIAO ESP32S3 Sense board using the SenseCraft AI platform. By following these instructions, you will learn how to trigger GPIO level changes based on specific event conditions detected by your trained model.

Using a model for Grove Vision AI V2​

SenseCraft AI is a powerful platform that offers a wide range of AI models compatible with various devices, including the Grove Vision AI V2. The Grove Vision AI V2 is a comprehensive AI vision module that combines a camera, processor, and AI capabilities, making it easy to integrate computer vision applications into your projects.

In this tutorial, we will guide you through the process of using a SenseCraft AI model on the Grove Vision AI V2 and previewing the model's output. We will also explore some key concepts and settings to help you understand and optimize the model's performance.

Using a model for XIAO ESP32S3 Sense​

SenseCraft AI is a powerful platform that provides a vast repository of AI models compatible with various devices. It allows developers and enthusiasts to easily deploy and experiment with different AI models on their hardware.

In this comprehensive tutorial, we will guide you through the process of using a SenseCraft AI model on the XIAO ESP32S3 Sense board and previewing the model's output. We will also delve into some key concepts and settings to help you understand and optimize the model's performance.

SenseCraft AI for SenseCAP Watcher​

SenseCAP Watcher is a powerful monitoring device that can be configured to recognize specific objects and trigger alarms based on user-defined tasks. To enhance Watcher's object recognition capabilities, users can leverage custom models from the SenseCraft AI model repository. This wiki article will guide you through the process of using these custom models in your Watcher monitoring tasks.

Relay Add On Module For XIAO​

The Relay Add On Module For XIAO is a smart module from Seeed Studio designed to control AC-powered appliances. It is characterized by the combination of XIAO, through the ESPHome access Home Assistant to control a variety of appliances, so that your home smarter!

RTL8822CE Wireless Module for Jetson​

The RTL8822CE is a compact Dual-band WLAN+Bluetooth Combo M.2 Card that integrates a 2T2R Dual-band WLAN subsystem with PCI Express controllers and a Bluetooth v5.0 subsystem with USB support. Compatible with IEEE 802.11 a/b/g/n/ac standards, it delivers a maximum PHY rate of up to 867 Mbps and supports Bluetooth dual mode (v5.0/v4.2/v2.1). Ideal for high-performance wireless and Bluetooth connectivity for using with embedded devices such as reComputer J4012.

Configuring Wio-SX1262 with XIAO ESP32S3 kit as Meshtastic device​

Meshtastic is an open source, off-grid, decentralized, mesh network built to run on affordable, low-power devices. Seeed Studio provides a comprehensive range of ready-to-go Meshtastic devices for hobbyists and industrial users. XIAO ESP32S3 & Wio-SX1262 Kit is flexible solution for meshtastic developer and maker.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...