Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is February 17th, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Deploy DeepSeek on reComputer Jetson with MLC​

This wiki provides a step-by-step guide to deploying DeepSeek on reComputer Jetson devices with MLC for efficient AI inference on the edge.

OS Update/Upgrade Guideline with Web​

This document outlines the reCamera OS upgrade and rollback process. Users can update via the web interface or command line, supporting OTA updates, specific version installations, or local package upgrades. It also includes commands for restoring factory settings and provides contact details for technical support.

Existing Wiki Updated​

Flashing JP6.2 on A603 and A608 Boards for Jetson Update​

We have updated the flashing procedure for flashing JP6.2 on the A603 and A608 carrier boards.

Single Channel LoRaWAN Gateway - SenseCAP Indicator​

We have added the SenseCAP Indicator Connect to ChirpStack example.

Getting started with 60GHz mmWave Fall Detection Sensor Kit with XIAO ESP32C6 (MR60FDA2)​

We have added the Module firmware upgrade example.

Voice Assistant System for Home Assitant​

We have added the XMOS Firmware update example and optimized the Add XIAO ESP32S3 to ESPHome example.

reCamera Quick Start Guide​

We have added the OTA Upgrade from 0.1.3 to latest version example.

Getting Started with ReSpeaker 2-Mics Pi HAT v2 on Raspberry Pi​

We have fixed and optimized the Setup the driver on Raspberry Pi example.

Getting Started with Seeed Studio XIAO-RS485-Expansion-Board​

We have added the schematic files for Seeed Studio XIAO RS485 Expansion Board.

The Efforts of Contributor​

Seeed Studio XIAO nRF52840 with NuttX(RTOS)​

This wiki introduces setting up NuttX RTOS on the Seeed Studio XIAO nRF52840 board. NuttX is a lightweight, scalable real-time operating system known for its small footprint and broad hardware support. The guide walks through installing necessary tools, configuring the board, building the system, and flashing firmware. It includes examples for using NuttShell (NSH), USBNSH, and JUMBO applications, with a focus on practical tasks like GPIO and LED control.

Past Weekly wiki​

Click here
Loading Comments...