Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is February 24th, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Getting Started with Wi-Fi HaLow Mini PCIe Module​

This guide will walk you through setting up and using the Wi-Fi HaLow Mini PCIe Module to build a Wi-Fi HaLow gateway. The Mini PCIe form factor makes it easy to integrate Wi-Fi HaLow connectivity into existing systems and create IoT gateways that can connect numerous low-power devices over long distances.

Getting Started with Wi-Fi HaLow Module for XIAO​

This tutorial will guide you through setting up and using the Wio-WM6180 Wi-Fi HaLow Module with a XIAO ESP32S3 to build a Wi-Fi HaLow client. Wi-Fi HaLow (IEEE 802.11ah) is designed for long-range, low-power IoT applications, operating in the sub-1 GHz frequency band. We'll walk through the hardware setup, software configuration, and demonstrate how to establish Wi-Fi HaLow connectivity for your IoT projects.

reServer Industrial Hardware Interface Usage​

This guide covers the key features and setup of the reServer Industrial board, which offers versatile connectivity options, including 5 RJ-45 Ethernet ports (4 PoE PSE), and supports 2.5" SATA HDD/SSD storage. With its fanless design and passive heatsink, it’s built for harsh environments, offering efficient cooling and low power consumption, making it ideal for demanding, noise-sensitive applications.

reCamera Software Structure​

The software comes with a stable reCamera OS that supports firmware OTA updates. Additionally, Node-RED and Sensecraft AI platform is integrated in the device for easier deployment experience. This integration offers novice developers a modular programming experience based on Node-RED nodes. For advanced developers, the in-depth Linux-based development and python are also there for twist and play.

We warmly welcome developers proficient in JavaScript, C/C++, Python, Linux OS, buildroot, as well as geeks, students, and beginners, to engage in further development and explore applications.

Develop reCamera with Node-RED​

Node-RED's goal is to enable anyone to build applications that collect, transform and visualize their data; building flows that can automate their world. Its low-code nature makes it accessible to users of any background, whether for home automation, industrial control systems or anything in between. By integrated Node-RED with reCamera, it provides a beginner-friendly development method that can let users drag and play with the device right the way. You can learn the Node-RED Concept here or start with a video tutorial.

Develop reCamera with c&cpp​

reCamera has limited resources and no compilation environment for C code is configured. If you want to use C&CPP to develop applications on the reCamera, you need to configure the cross-compilation environment on a linux machine. This wiki provides a simple example for configuring the compilation environment to help you get started quickly.

Existing Wiki Updated​

LoRaWAN® Gateway Module WM1302​

We have added the Run Semtech SX1302 packet forwarder example.

reComputer Mini Hardware and Interfaces Usage​

We have added the Ethernet, USB, UART, and other examples for reComputer Mini hardware and interface usage.

Flash JetPack OS to J401 Carrier Board​

We have added the flashing JP6.2 example.

Getting Started with Seeed Studio XIAO MG24​

We have added the Preventing XIAO MG24 from Bricking During Deep Sleep and Unbricking example.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...