Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is March 3rd, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Getting Started with reCamera Gimbal​

The reCamera gimbal 2002 series is the first open-source camera control system, composed of one tiny AI camera - reCamera 2002w 8GB/64GB, and one compatible 2-Axis gimbal basement with 2 brushless motors. It is powered by an RISC-V SoC, providing 1 TOPS AI performance with video encoding at 5MP @ 30 FPS. It offers a Lego-like self-assembly package and integrates the Sensecraft AI platform and Node-RED platform for smooth graphical programming and pipeline construction, enabling rapid self-training, model conversion, and deployment of AI models such as Yolo v5/v8/11.

reComputer R1100 Getting Started​

The reComputer R1100, powered by the Raspberry Pi CM4, is a versatile edge IoT gateway with AI capabilities. It features a comprehensive range of industrial interfaces, including 2x Ethernet, 2x USB, 2x RS485, 2x RS232, 2x DI, and 2x DO, along with flexible wireless connectivity options such as 4G, LoRa®, and Wi-Fi/BLE. These features make it an ideal choice for various industrial applications.

reComputer R1100 Assembly Guide​

This Wiki will show you how to Assemble and Disassemble the unit to install peripherals components, as well as the option for mounting.

Configure reComputer R1100​

Learn how to configure and test hardware components on the reComputer R1100 series after installing devices. This wiki covers GPIO mapping, USER LED testing, SPI communication, Wi-Fi and Bluetooth scanning, LoRa®, 4G, Zigbee over Mini-PCIe, RS485, RS232, DI/DO testing,UPS for safe shutdown and more.

Existing Wiki Updated​

XIAO ESP32S3 Sense Sleep Modes​

We have updated the example code for the Deep-Sleep, Light-Sleep, and Modem-Sleep modes of the XIAO ESP32S3 Sense.

reComputer R1000 Raspbian OS to eMMC​

We have added an operation example for Boot from NVME.

Flash JetPack OS to A603 Carrier Board​

We have added an example for using CAN Interfaces.

NVIDIA® Jetson AGX Orin 32GB H01 Kit​

We have added relevant information about Developer Tools.

The Efforts of Contributor​

Develop both chips with Arduino​

This tutorial will guide you to develop your own custom project/firmware for the Sensecap Indicator using the simplicity and Flexibility of the Arduino Framework.

Past Weekly wiki​

Click here
Loading Comments...