Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is April 28th, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Getting start with reComputer J401B​

pir

The reComputer J401B series is an iteration on reComputer Classic series. The reComputer J4011B with NVIDIA Jetson Orin NX 8GB modules is a powerful and compact edge AI device with rich interfaces: 2x USB 3.2, HDMI, Ethernet, M.2 Key E for Wi-Fi module, M.2 Key M for SSD, mini-PCIe for LTE module, CAN, 40-pin and more.

J401B Interfaces​

pir

This wiki introduces the various different hardware and interfaces on the reComputer J401B and how to use them to expand your project ideas.

Total Solar Radiation Sensor​

pir

The IP68 RS485 Total Solar Radiation Sensor measures real-time solar total radiation from 300 to 1100 nanometers. It's ideal for environmental monitoring and agriculture. Pair it with the SenseCAP Sensor Hub 4G Data Logger or SenseCAP S2100 LoRaWAN® Data Logger for seamless data collection and management. On this page, we'll guide you through the process of connecting the S2100 LoRaWAN Data Logger with a Total Solar Radiation Sensor, enabling you to create a robust, industrial-grade LoRaWAN wireless sensor that can be used commercially in just five minutes.

Existing Wiki Updated​

Connect Seeed Studio IoT Button To ESPHome​

We have modified the configuration code in the 'Adding the ESPHome Configuration' section.

Grove - Barometer (High-Accuracy)​

We have corrected the example steps related to 'Play With Raspberry Pi' and adjusted the sample code.

Flash Opensource Firmware to M2 Gateway​

We have added a sample reference for flashing firmware via Luci.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...