Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is July 21st, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

reSpeaker XVF3800 USB 4 Microphone Array with XIAO ESP32S3​

pir

The ReSpeaker XVF3800 USB 4-Mic Array is a professional circular 4-microphone array based on the XMOS XVF3800. It features AEC, AGC, DoA, beamforming, VAD, noise suppression, de-reverberation, and 360° voice capture (up to 5 meters). It also supports dual operation modes, making it ideal for advanced voice applications. When combined with the Xiao ESP32S3, controlling the ReSpeaker XVF3800 USB becomes even more powerful, unlocking endless possibilities.

We also provide several practical guides to help you explore the capabilities of the reSpeaker XVF3800 USB 4 Microphone Array with XIAO ESP32S3:

These tutorials cover various features including I2S audio input/output, I2C control, RGB lighting, and GPIO handling, providing a complete understanding of the XVF3800's functionality in real-world scenarios.

reCamera connects to XIAO via HTTP​

pir

This document demonstrates how to enable communication between the reCamera and XIAO via HTTP, transmitting data to XIAO so that you can integrate the reCamera into your own projects.

TRMNL 7.5" (OG) DIY Kit​

pir

The TRMNL 7.5" (OG) DIY Kit, co-developed by Seeed Studio and TRMNL, is a versatile e-ink development solution. It combines a 7.5-inch 800×480 monochrome e-ink display, XIAO ESP32-S3 PLUS driver board, 2000 mAh rechargeable battery, and 10cm FPC extension cable. Fully compatible with the TRMNL BYOD ecosystem, this kit enables no-code dashboard building with over 375 plugins and 8 layouts, ideal for DIY enthusiasts, smart home interfaces, and creative digital signage.

Getting Started with XIAO IR Mate Smart IR Remote (For Home Assistant)​

pir

This device is specially designed for Home Assistant users, aiming to provide a seamless, efficient, and integrated smart infrared remote control solution. Through this guide, you will learn how to set up the device, connect it to your home network, integrate it into Home Assistant, and unlock its full potential, from basic signal learning to advanced smart air conditioner control.

Existing Wiki Updated​

Get Started with Indicator for Meshtastic​

We have added instructions on how to use the Keyboard.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...