Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is October 13th, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

XIAO ePaper Display Board EE04 with PlatfromIO​

pir

This document provides a guide on how to use the XIAO ePaper Display Board EE04 with PlatformIO, including hardware setup, project creation, code uploading, button control, and battery voltage detection examples.

PyCuVSLAM with reComputer​

pir

PyCuVSLAM is NVIDIA's GPU-accelerated visual odometry and SLAM library cuVSLAM's Python wrapper. It supports monocular, stereo, RGB-D, multi-camera, and visual-inertial (IMU) modes, providing a simple Python API that can directly interface with camera streams and output real-time camera poses, map points, and loop closure information. The underlying CUDA optimization enables high-precision, low-latency SLAM inference on both PC and Jetson devices, making it suitable for robotic navigation, drone positioning, and 3D perception applications.This wiki will provide instructions on how to deploy pycuvslam on reComputer.

How to use LLaVa on the reComputer Industrial J4012 to monitor your warehouse​

This wiki describes deploying a VLM (Visual Learning Model) on the reComputer Industrial J4012, using a USB camera as the input for the VLM. When the system detects a safe situation, the signal light will turn green via RS485 control. In dangerous situations, such as a fire or the presence of someone with a weapon, the signal light will turn yellow. When the light sensor detects the signal from the warehouse light being turned off via RS485, the signal light will turn red.

Existing Wiki Updated​

Deploying OpenRemote on reComputer R1x Manage IoT Devices at the Edge​

We have added an operation example of MQTT Agent with ChirpStack LoRaWAN Gateway Integration.

Seeed Studio XIAO nRF54L15 Matter​

We have added an operation example of Matter Hub Config.

Getting Started with TRMNL 7.5" (OG) DIY Kit in Arduino​

We have added an operation demo of Equipment Installatio.

Getting started with SO-ARM100 and SO-ARM101 robotic arm with LeRobot​

We have provided a tutorial on how to use the device with the Orbbec Gemini2 Depth Camera.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...