Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is October 20th, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Efficient Multi-Task Vision Inference Engine Deployment on Jetson​

pir

Visual Perception Engine is a cutting-edge framework that revolutionizes robotic perception by eliminating redundant computations through shared backbone networks. Unlike traditional approaches where each visual task runs independently, VPEngine uses a unified base model backbone (e.g., DINOv2) to extract image features only once, which are then reused by multiple task heads. This approach significantly reduces memory overhead and CPU-GPU data transfer while supporting dynamic task scheduling and seamless ROS2 integration.This wiki will show you how to use reComputer Robotics in conjunction with GMSL cameras to deploy the Visual Perception Engine to the edge.

Flashing AI Models on the SenseCAP Watcher​

pir

This guide focuses on how to flash the SenseCAP Watcher with the Visual Recognition Triggered Conversation firmware and how to replace or update the AI model on the device. It is intended as a hands-on instructional guide for these operations.

EE04 ePaper Display Work with ESPHome for Home Assistant​

pir

This document is a detailed tutorial on integrating the EE04 ePaper Display with ESPHome to create a smart home control panel in Home Assistant. It covers hardware preparation, firmware setup, and data display such as weather information. The guide also provides examples of configuring the SPI interface, fonts, graphics, and data retrieval from Home Assistant using YAML files.

Existing Wiki Updated​

Getting Started with reTerminal E Series ePaper Display and EEZ Studio​

We have added an example showing how to configure the Project Settings.

NVIDIA® Jetson AGX Orin 32GB H01 Kit​

We have added a tutorial on how to flash JP5.1.4 onto the NVIDIA® Jetson AGX Orin 32GB H01 Kit.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...