Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is November 3rd, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

reCamera HQ POE Getting Started Guide​

pir

Welcome to reCamera HQ PoE! Featuring an advanced CMOS sensor and an M12 lens mount for flexible lens replacement, reCamera 2002 HQ PoE delivers sharp, clear images. With PoE support, power and data run through a single Ethernet cable. This guide helps you set up and start using its powerful AI Vision features quickly.

YOLO11n Model Conversion for reCamera: Complete Guide​

pir

In this tutorial, you’ll convert a YOLO11n ONNX model into an INT8 CV181x .cvimodel and deploy it on reCamera. We cover setup (cloud or local), calibration with 100 images, TPU-MLIR conversion, validation, deployment, and troubleshooting.

EE04 ePaper Display with EEZ Studio​

pir

This tutorial uses the XIAO ePaper Display Board EE04, based on EEZ Studio and by compiling and uploading the program using the Arduino IDE.

XIAO ePaper Display Board EE04 with the SenseCraft HMI​

pir

SenseCraft HMI lets you create professional, no-code visual interfaces through an intuitive cloud editor. Paired with the XIAO ePaper Display Board (ESP32-S3) – EE04, it brings seamless integration for low-power ePaper dashboards and smart displays. This tutorial walks you through a hands-on example using a 7.3" Spectra™ 6 E-Ink display.

pir

OpenEPaperLink (OEPL) is an open-source firmware and communication protocol for electronic shelf labels, supporting multiple displays via ESP32 or nRF52840 access points with 802.15.4 radio. In this tutorial, we use OPEL Config Builder to adjust e-paper parameters and OEPL Image Uploader to upload images.

Existing Wiki Updated​

Getting Started with XIAO ePaper Display EE04​

We have added instructions for using the User Buttons on the XIAO ePaper Display Board (ESP32-S3) - EE04.

The Efforts of Contributor​

Building a Voice-Interactive Chatbot with Local LLMs, STT, and TTS​

This project brings the dream of a fully voice-interactive AI assistant to life — running entirely on local hardware, without reliance on cloud services.
By combining Speech-to-Text (STT), Text-to-Speech (TTS), and Local Large Language Models (LLMs) using Ollama, the system enables natural, private, and real-time conversations between humans and machines. The entire setup runs inside Docker containers and can be deployed on NVIDIA Jetson devices, edge computers, or any Linux-based system with GPU acceleration.

Past Weekly wiki​

Click here
Loading Comments...